MCUXpresso SDK Documentation

lpc_i2c_dma_b2b_transfer_master

lpc_i2c_dma_b2b_transfer_master#

Overview#

The i2c_dma_b2b_transfer_master example shows how to use i2c driver as master to do board to board transfer with DMA:

In this example, one i2c instance as master and another i2c instance on the other board as slave. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct.

Supported Boards#