MCUXpresso SDK Documentation

i3c_interrupt_b2b_slave

i3c_interrupt_b2b_slave#

Overview#

The example shows how to use i3c driver as slave to do board to board transfer with a interrupt master, slave application is implemented with functional API instead of transactional API to reduce code size and improve performance on low frequency MCU.

In this example, one i3c instance as slave and another i3c instance on the other board as master. Master will enter dynamic address cycle to assign address to the connected slave, after success, will use I3C SDR mode to transfer data, then receive data from the connected I3C slave and check the data consistency.

Supported Boards#

LPCXpresso860MAX
Hardware requirements
  • Micro USB cable

  • LPCXpresso860max board

  • Personal Computer

Board settings

I3C one board:

  • Transfer data from MASTER_BOARD to SLAVE_BOARD of I3C interface, I3C0 pins of MASTER_BOARD are connected with I3C0 pins of SLAVE_BOARD

MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name   Board Location     Pin Name   Board Location
P0_26       J1-2               P0_26       J1-2
P1_14       J1-4               P1_14       J1-4
GND         J1-14              GND         J1-14
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J4) on the board

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Press reset button to begin running the demo.

Running the demo

The following message shows in the terminal if the example runs successfully.

I3C board2board Interrupt example -- Slave.


Check I3C master I3C SDR transfer.


I3C slave request IBI event with one mandatory data byte 0x20.

I3C slave request IBI event sent.
Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7  
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f  
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17  
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f  


 I3C Slave I3C SDR transfer finished .