flexspi_octal_edma_transfer#
Overview#
The flexspi_octal_edma_transfer example shows how to use flexspi driver with dma:
In this example, flexspi will send data and operate the external octal flash connected with FLEXSPI. Some simple flash command will be executed, such as Write Enable, Erase sector, Program page. Example will first erase the sector and program a page into the flash, at last check if the data in flash is correct.
Supported Boards#
MIMXRT1180-EVK
Hardware requirements
Mini/micro USB cable
MIMXRT1180-EVK board
Personal Computer
Board settings
In order to interface the on-board octal FLASH it is necessary to populate with 0R or short circuit following positions: R293, R296, R297, R298 and set jumper J75 to position 1-2. Jumper J59 should remain in the default 2-3 position.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
FLEXSPI edma example started!
Vendor ID: 0x2c
Erasing Serial NOR over FlexSPI...
Erase data - successfully.
Program data - successfully.