flexio_spi_int_spi_transfer_slave#
Overview#
The flexio_spi_slave_interrupt_spi_master example shows how to use flexio spi slave driver in interrupt way:
In this example, a flexio simulated slave connect to a spi master.
Supported Boards#
FRDM-K32L2B
Hardware requirements
Mini USB cable
FRDM-K32L2B board
Personal Computer
Board settings
The flexio_spi_slave_interrupt_spi_master example is requires connecting between FlexIO pins with SPI pins The connection should be set as following:
J1-7, J2-6 connected
J1-9, J2-8 connected
J1-11, J2-10 connected
J1-15, J2-12 connected
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
SPI Master interrupt - FLEXIO SPI Slave interrupt example start.
This example use one spi instance as master and one flexio spi slave on one board.
Master and slave are both use interrupt way.
Please make sure you make the correct line connection. Basically, the connection is:
SPI_master -- FLEXIO_SPI_slave
SCK -- SCK
PCS0 -- PCS0
MOSI -- MOSI
MISO -- MISO
This is FLEXIO SPI slave call back.
SPI master <-> FLEXIO SPI slave transfer all data matched!
FRDM-MCXC242
Hardware requirements
Mini USB cable
FRDM-MCXC242 board
Personal Computer
Board settings
The flexio_spi_slave_interrupt_spi_master example is requires connecting between FlexIO pins with SPI pins The connection should be set as following: FLEXIO SPI1 PCS0 J4-6 J1-9 SCK J4-8 J1-11 MISO J2-20 J3-1 MOSI J2-18 J3-3
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
SPI Master interrupt - FLEXIO SPI Slave interrupt example start.
This example use one spi instance as master and one flexio spi slave on one board.
Master and slave are both use interrupt way.
Please make sure you make the correct line connection. Basically, the connection is:
SPI_master -- FLEXIO_SPI_slave
SCK -- SCK
PCS0 -- PCS0
MOSI -- MOSI
MISO -- MISO
This is FLEXIO SPI slave call back.
SPI master <-> FLEXIO SPI slave transfer all data matched!
FRDM-MCXC444
Hardware requirements
Type-C USB cable
FRDM-MCXC444 board
Personal Computer
Board settings
The flexio_spi_slave_interrupt_spi_master example is requires connecting between FlexIO pins with SPI pins The connection should be set as following: FLEXIO SPI1 PCS0 J4-1 J2-6 SCK J4-3 J2-12 MISO J2-10 J2-18 MOSI J2-8 J2-20
Prepare the Demo
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
SPI Master interrupt - FLEXIO SPI Slave interrupt example start.
This example use one spi instance as master and one flexio spi slave on one board.
Master and slave are both use interrupt way.
Please make sure you make the correct line connection. Basically, the connection is:
SPI_master -- FLEXIO_SPI_slave
SCK -- SCK
PCS0 -- PCS0
MOSI -- MOSI
MISO -- MISO
This is FLEXIO SPI slave call back.
SPI master <-> FLEXIO SPI slave transfer all data matched!