flexio_spi_int_spi_transfer_master#
Overview#
The flexio_spi_master_interrupt_spi_slave example shows how to use flexio spi master driver in interrupt way:
In this example, a flexio simulated master connect to a spi slave .
Supported Boards#
EVK-MIMXRT595
Hardware requirements
Mini/micro USB cable
EVK-MIMXRT595 board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Note: Please disconnect JS23 1-2, and connect JS23-2 to JP23-3 to provide 1.8V to VDDIO_3
SLAVE(SPI5) connect to MASTER(FlexIO0)
Pin Name Board Location Pin Name Board Location
MOSI JP26-2 MOSI J28-4
MISO JP26-3 MISO J28-5
SCK JP26-4 SCK J28-6
PCS0 JP26-1 PCS0 J28-3
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the terminal:
FLEXIO Master - SPI Slave interrupt example start.
This example use one flexio spi as master and one spi instance as slave on one board.
Master and slave are both use interrupt way.
Please make sure you make the correct line connection. Basically, the connection is:
FLEXI_SPI_master -- SPI_slave
SCK -- SCK
PCS0 -- PCS0
MOSI -- MOSI
MISO -- MISO
This is SPI slave call back.
FLEXIO SPI master <-> SPI slave transfer all data matched!
FRDM-K32L2B
Hardware requirements
Mini USB cable
FRDM-K32L2B board
Personal Computer
Board settings
The flexio_spi_master_interrupt_spi_slave example is requires connecting between FlexIO pins with SPI pins The connection should be set as following:
J1-7, J2-6 connected
J1-9, J2-8 connected
J1-11, J2-10 connected
J1-15, J2-12 connected
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
FLEXIO Master - SPI Slave interrupt example start.
This example use one flexio spi as master and one spi instance as slave on one board.
Master and slave are both use interrupt way.
Please make sure you make the correct line connection. Basically, the connection is:
FLEXI_SPI_master -- SPI_slave
SCK -- SCK
PCS0 -- PCS0
MOSI -- MOSI
MISO -- MISO
This is SPI slave call back.
FLEXIO SPI master <-> SPI slave transfer all data matched!
FRDM-MCXC242
Hardware requirements
Mini USB cable
FRDM-MCXC242 board
Personal Computer
Board settings
The flexio_spi_master_interrupt_spi_slave example is requires connecting between FlexIO pins with SPI pins The connection should be set as following: FLEXIO SPI1 PCS0 J4-6 J1-9 SCK J4-8 J1-11 MISO J2-20 J3-1 MOSI J2-18 J3-3
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
FLEXIO Master - SPI Slave interrupt example start.
This example use one flexio spi as master and one spi instance as slave on one board.
Master and slave are both use interrupt way.
Please make sure you make the correct line connection. Basically, the connection is:
FLEXI_SPI_master -- SPI_slave
SCK -- SCK
PCS0 -- PCS0
MOSI -- MOSI
MISO -- MISO
This is SPI slave call back.
FLEXIO SPI master <-> SPI slave transfer all data matched!
FRDM-MCXC444
Hardware requirements
Type-C USB cable
FRDM-MCXC444 board
Personal Computer
Board settings
The flexio_spi_master_interrupt_spi_slave example is requires connecting between FlexIO pins with SPI pins The connection should be set as following: FLEXIO SPI1 PCS0 J4-1 J2-6 SCK J4-3 J2-12 MISO J2-10 J2-18 MOSI J2-8 J2-20
Prepare the Demo
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
FLEXIO Master - SPI Slave interrupt example start.
This example use one flexio spi as master and one spi instance as slave on one board.
Master and slave are both use interrupt way.
Please make sure you make the correct line connection. Basically, the connection is:
FLEXI_SPI_master -- SPI_slave
SCK -- SCK
PCS0 -- PCS0
MOSI -- MOSI
MISO -- MISO
This is SPI slave call back.
FLEXIO SPI master <-> SPI slave transfer all data matched!