MCUXpresso SDK Documentation

flexio_spi_int_b2b_transfer_master

flexio_spi_int_b2b_transfer_master#

Overview#

The flexio_spi_master_interrupt example shows how to use flexio spi master driver in interrupt way:

In this example, a flexio simulated master connect to a flexio simulated spi slave .

Supported Boards#

EVKB-IMXRT1050
Hardware requirements
  • Mini/micro USB cable

  • EVKB-MIMXRT1050 board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

        SLAVE           connect to      MASTER
Pin Name   Board Location     Pin Name    Board Location
SOUT       SW5-2                SIN       SW5-3
SIN        SW5-3                SOUT      SW5-2
SCK        SW5-1                SCK       SW5-1
PCS0       SW5-4                PCS0      SW5-4

Note: Please start up slave example then connect PCS0(SW5-4) and start up master example, otherwise the high level signal from master board will affect the boot of slave board.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

You can see the similar message shows following in the terminal if the example runs successfully.

FlexIO SPI interrupt example
Slave is working...

Slave runs successfully!
MIMXRT1060-EVKB
Hardware requirements
  • Mini/micro USB cable

  • Two MIMXRT1060-EVKB boards

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

        SLAVE           connect to      MASTER
Pin Name   Board Location     Pin Name    Board Location
SOUT       SW2-2                SIN       SW2-3
SIN        SW2-3                SOUT      SW2-2
SCK        SW2-1                SCK       SW2-1
PCS0       SW2-4                PCS0      SW2-4

Note: Please start up slave example then connect PCS0(SW2-4) and start up master example, otherwise the high level signal from master board will affect the boot of slave board.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

You can see the similar message shows following in the terminal if the example runs successfully.

FlexIO SPI interrupt example
Slave is working...

Slave runs successfully!
MIMXRT1060-EVKC
Hardware requirements
  • Mini/micro USB cable

  • Two MIMXRT1060-EVKC boards

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

        SLAVE           connect to      MASTER
Pin Name   Board Location     Pin Name    Board Location
SOUT       SW2-2                SIN       SW2-3
SIN        SW2-3                SOUT      SW2-2
SCK        SW2-1                SCK       SW2-1
PCS0       SW2-4                PCS0      SW2-4

Note: Please start up slave example then connect PCS0(SW2-4) and start up master example, otherwise the high level signal from master board will affect the boot of slave board.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

You can see the similar message shows following in the terminal if the example runs successfully.

FlexIO SPI interrupt example
Slave is working...

Slave runs successfully!
EVK-MIMXRT1015
Hardware requirements
  • Mini/micro USB cable

  • Two EVK-MIMXRT1015 boards

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER      connect to      SLAVE
Pin Name   Board Location   Pin Name   Board Location
MOSI       J18-5            MOSI       J18-5
MISO       J18-6            MISO       J18-6
SCK        J18-3            SCK        J18-3
PCS0       J18-1            PCS0       J18-1
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

You can see the similar message shows following in the terminal if the example runs successfully.

FlexIO SPI interrupt example
Master Start...

Master runs successfully!

================================

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

EVK-MIMXRT1020
Hardware requirements
  • Mini/micro USB cable

  • Two EVK-MIMXRT1020 boards

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

        SLAVE           connect to      MASTER
Pin Name   Board Location     Pin Name    Board Location
 MOSI        J18-6                MOSI       J18-6
 MISO        J18-5                MISO       J18-5
 SCK         J18-3                SCK        J18-3
 PCS0        J18-4                PCS0       J18-4
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

You can see the similar message shows following in the terminal if the example runs successfully.

FlexIO SPI interrupt example
Master Start...

Master runs successfully!

================================

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

MIMXRT1024-EVK
Hardware requirements
  • Mini/micro USB cable

  • Two MIMXRT1024-EVK boards

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

        SLAVE           connect to      MASTER
Pin Name   Board Location     Pin Name    Board Location
 MOSI        J18-12               MOSI       J18-12
 MISO        J18-10               MISO       J18-10
 SCK         J18-6                SCK        J18-6
 PCS0        J18-8                PCS0       J18-8
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

You can see the similar message shows following in the terminal if the example runs successfully.

FlexIO SPI interrupt example
Master Start...

Master runs successfully!

================================

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

MIMXRT1040-EVK
Hardware requirements
  • Mini/micro USB cable

  • Two MIMXRT1040-EVK boards

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

        SLAVE           connect to      MASTER
Pin Name   Board Location     Pin Name    Board Location
SOUT       SW2-2                SIN       SW2-3
SIN        SW2-3                SOUT      SW2-2
SCK        SW2-1                SCK       SW2-1
PCS0       SW2-4                PCS0      SW2-4

Note: Please start up slave example then connect PCS0(SW2-4) and start up master example, otherwise the high level signal from master board will affect the boot of slave board.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

You can see the similar message shows following in the terminal if the example runs successfully.

FlexIO SPI interrupt example
Slave is working...

Slave runs successfully!
EVK-MIMXRT1064
Hardware requirements
  • Mini/micro USB cable

  • Two EVK-MIMXRT1064 boards

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

        SLAVE           connect to      MASTER
Pin Name   Board Location     Pin Name    Board Location
SOUT       SW5-2                SIN       SW5-3
SIN        SW5-3                SOUT      SW5-2
SCK        SW5-1                SCK       SW5-1
PCS0       SW5-4                PCS0      SW5-4

Note: Please start up slave example then connect PCS0(SW5-4) and start up master example, otherwise the high level signal from master board will affect the boot of slave board.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

You can see the similar message shows following in the terminal if the example runs successfully.

FlexIO SPI interrupt example
Slave is working...

Slave runs successfully!
FRDM-MCXA156
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA156 Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER(FlexIO SPI)          connect to      SLAVE(FlexIO SPI)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J8 pin 13                       SIN         J8 pin 13
SIN        J8 pin 14                       SOUT        J8 pin 14
SCK        J8 pin 15                       SCK         J8 pin 15
PCS0       J8 pin 16                       PCS0        J8 pin 16
GND        J8 pin 8                        GND         J8 pin 8
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J21.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

FlexIO SPI interrupt example
Master Start...

Master runs successfully!
FRDM-MCXN236
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXN236 board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER(FlexIO SPI)          connect to      SLAVE(FlexIO SPI)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J8 pin 26                        SIN         J8 pin 26
SIN        J8 pin 25                        SOUT        J8 pin 25
SCK        J8 pin 27                        SCK         J8 pin 27
PCS0       J8 pin 28                        PCS0        J8 pin 28
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J10.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

FlexIO SPI interrupt example
Master Start...

Master runs successfully!
FRDM-MCXN947
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXN947 Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER(FlexIO SPI)          connect to      SLAVE(FlexIO SPI)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J8 pin 26                       SIN         J8 pin 26
SIN        J8 pin 25                       SOUT        J8 pin 25
SCK        J8 pin 27                       SCK         J8 pin 27
PCS0       J8 pin 28                       PCS0        J8 pin 28
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J17.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

FlexIO SPI interrupt example
Master Start...

Master runs successfully!
FRDM-MCXN947T
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXN947T Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER(FlexIO SPI)          connect to      SLAVE(FlexIO SPI)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J8 pin 26                       SIN         J8 pin 26
SIN        J8 pin 25                       SOUT        J8 pin 25
SCK        J8 pin 27                       SCK         J8 pin 27
PCS0       J8 pin 28                       PCS0        J8 pin 28
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J17.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

FlexIO SPI interrupt example
Master Start...

Master runs successfully!
FRDM-MCXW71
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW71 Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER(FlexIO SPI)          connect to      SLAVE(FlexIO SPI)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J1 pin 3                         SIN         J1 pin 3
SIN        J1 pin 2                         SOUT        J1 pin 2
SCK        J1 pin 4                         SCK         J1 pin 4
PCS0       J1 pin 1                         PCS0        J1 pin 1
Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board J10.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the demo in the terminal window:

FlexIO SPI interrupt example
Master Start...

Master runs successfully!
MCX-W71-EVK
Hardware requirements
  • Type-C USB cable

  • MCX-W71-EVK Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER(FlexIO SPI)          connect to      SLAVE(FlexIO SPI)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J1 pin 13                        SIN         J1 pin 13
SIN        J1 pin 7                         SOUT        J1 pin 7
SCK        J1 pin 15                        SCK         J1 pin 15
PCS0       J1 pin 5                         PCS0        J1 pin 5
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J14.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the demo in the terminal window:

FlexIO SPI interrupt example
Master Start...

Master runs successfully!
KW45B41Z-EVK
Hardware requirements
  • Mini/micro USB cable

  • KW45B41Z-EVK Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER(FlexIO SPI)          connect to      SLAVE(FlexIO SPI)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J1 pin 7                         SIN         J1 pin 7
SIN        J1 pin 4                         SOUT        J1 pin 4
SCK        J1 pin 8                         SCK         J1 pin 8
PCS0       J1 pin 3                         PCS0        J1 pin 3
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J14.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the demo in the terminal window:

FlexIO SPI interrupt example
Master Start...

Master runs successfully!
KW47-EVK
Hardware requirements
  • Type-C USB cable

  • KW47-EVK Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER(FlexIO SPI)          connect to      SLAVE(FlexIO SPI)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J1 pin 13                        SIN         J1 pin 13
SIN        J1 pin 7                         SOUT        J1 pin 7
SCK        J1 pin 15                        SCK         J1 pin 15
PCS0       J1 pin 5                         PCS0        J1 pin 5
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J14.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the demo in the terminal window:

FlexIO SPI interrupt example
Master Start...

Master runs successfully!
MCX-N5XX-EVK
Hardware requirements
  • Mini/micro USB cable

  • MCX-N5XX-EVK Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER(FlexIO SPI)          connect to      SLAVE(FlexIO SPI)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J20 pin 26                       SIN         J20 pin 26
SIN        J20 pin 25                       SOUT        J20 pin 25
SCK        J20 pin 27                       SCK         J20 pin 27
PCS0       J20 pin 28                       PCS0        J20 pin 28
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J5.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

FlexIO SPI interrupt example
Master Start...

Master runs successfully!
MCX-N9XX-EVK
Hardware requirements
  • Mini/micro USB cable

  • MCX-N9XX-EVK Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER(FlexIO SPI)          connect to      SLAVE(FlexIO SPI)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J20 pin 26                       SIN         J20 pin 26
SIN        J20 pin 25                       SOUT        J20 pin 25
SCK        J20 pin 27                       SCK         J20 pin 27
PCS0       J20 pin 28                       PCS0        J20 pin 28
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J5.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

FlexIO SPI interrupt example
Master Start...

Master runs successfully!
MCX-W72-EVK
Hardware requirements
  • Type-C USB cable

  • MCX-W72-EVK Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER(FlexIO SPI)          connect to      SLAVE(FlexIO SPI)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J1 pin 13                        SIN         J1 pin 13
SIN        J1 pin 7                         SOUT        J1 pin 7
SCK        J1 pin 15                        SCK         J1 pin 15
PCS0       J1 pin 5                         PCS0        J1 pin 5
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J14.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the demo in the terminal window:

FlexIO SPI interrupt example
Master Start...

Master runs successfully!
MIMXRT700-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT700-EVK board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER(FlexIO SPI)          connect to      SLAVE(FlexIO SPI)
Pin Name   Board Location                   Pin Name    Board Location
MOSI       J5 Pin 6                         MOSI      J5 pin 6
MISO       J5 pin 3                         MISO      J5 Pin 3
SCK        J5 pin 4                         SCK       J5 pin 4
PCS        J5 pin 5                         PCS       J5 pin 5
GND        J6 pin 7                         GND       J6 pin 7
Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

FlexIO SPI interrupt example
Master Start...

Master runs successfully!
KW47-LOC
Hardware requirements
  • Type-C USB cable

  • KW47-LOC Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER(FlexIO SPI)          connect to      SLAVE(FlexIO SPI)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J2 pin 6                         SIN         J2 pin 6
SIN        J2 pin 5                         SOUT        J2 pin 5
SCK        J2 pin 4                         SCK         J2 pin 4
PCS0       J2 pin 3                         PCS0        J2 pin 3

Short the JP24-2 and JP24-3 with the jumper, other jumpers keep default configuration.

Prepare the Demo
  1. Connect a USB cable between the host PC and the LOC board J3.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the demo in the terminal window:

FlexIO SPI interrupt example
Master Start...

Master runs successfully!
MCXW72-LOC
Hardware requirements
  • Type-C USB cable

  • MCXW72-LOC Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER(FlexIO SPI)          connect to      SLAVE(FlexIO SPI)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J2 pin 6                         SIN         J2 pin 6
SIN        J2 pin 5                         SOUT        J2 pin 5
SCK        J2 pin 4                         SCK         J2 pin 4
PCS0       J2 pin 3                         PCS0        J2 pin 3

Short the JP24-2 and JP24-3 with the jumper, other jumpers keep default configuration.

Prepare the Demo
  1. Connect a USB cable between the host PC and the LOC board J3.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the demo in the terminal window:

FlexIO SPI interrupt example
Master Start...

Master runs successfully!
FRDM-MCXA266
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA266 Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER(FlexIO SPI)          connect to      SLAVE(FlexIO SPI)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J8 pin 13                        SIN         J8 pin 13
SIN        J8 pin 14                        SOUT        J8 pin 14
SCK        J8 pin 15                        SCK         J8 pin 15
PCS0       J8 pin 16                        PCS0        J8 pin 16
GND        J8 pin 2                         GND         J8 pin 2
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

FlexIO SPI interrupt example
Master Start...

Master runs successfully!
FRDM-MCXA366
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA366 Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER(FlexIO SPI)          connect to      SLAVE(FlexIO SPI)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J8 pin 13                        SIN         J8 pin 13
SIN        J8 pin 14                        SOUT        J8 pin 14
SCK        J8 pin 15                        SCK         J8 pin 15
PCS0       J8 pin 16                        PCS0        J8 pin 16
GND        J8 pin 2                         GND         J8 pin 2
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

FlexIO SPI interrupt example
Master Start...

Master runs successfully!
FRDM-MCXW72
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW72 Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER(FlexIO SPI)          connect to      SLAVE(FlexIO SPI)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J5 pin 6                         SIN         J5 pin 6
SIN        J5 pin 5                         SOUT        J5 pin 5
SCK        J5 pin 4                         SCK         J5 pin 4
PCS0       J5 pin 3                         PCS0        J5 pin 3

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board J10.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the demo in the terminal window:

FlexIO SPI interrupt example
Master Start...

Master runs successfully!
FRDM-MCXA577
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA577 Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER(FlexIO SPI)          connect to      SLAVE(FlexIO SPI)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J8 pin 13                        SIN         J8 pin 13
SIN        J8 pin 14                        SOUT        J8 pin 14
SCK        J8 pin 15                        SCK         J8 pin 15
PCS0       J8 pin 16                        PCS0        J8 pin 16
GND        J8 pin 2                         GND         J8 pin 2
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

FlexIO SPI interrupt example
Master Start...

Master runs successfully!
FRDM-MCXA287
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA287 Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

MASTER(FlexIO SPI)          connect to      SLAVE(FlexIO SPI)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J8 pin 13                        SIN         J8 pin 13
SIN        J8 pin 14                        SOUT        J8 pin 14
SCK        J8 pin 15                        SCK         J8 pin 15
PCS0       J8 pin 16                        PCS0        J8 pin 16
GND        J8 pin 2                         GND         J8 pin 2
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

FlexIO SPI interrupt example
Master Start...

Master runs successfully!