flexio_i2c_interrupt_flexcomm_i2c_transfer#
Overview#
The flexio_i2c_interrupt example shows how to use flexio i2c master driver in interrupt way:
In this example, a flexio simulated i2c master connect to an I2C slave.
Supported Boards#
EVK-MIMXRT595
Hardware requirements
Micro USB cable
EVK-MIMXRT595 board
Personal Computer
Board settings
The flexio_i2c_interrupt example is requires connecting the FLEXIO pins with the I2C pins The connection should be set as following:
Pin Name Board Location CONNECTS TO Pin Name Board Location
FLEXIO_I2C_SCL J27-1 I2C_SCL J28-10
FLEXIO_I2C_SDA J27-2 I2C_SDA J28-9
Prepare the Demo
Connect a micro USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
FlexIO I2C interrupt - I2C interrupt
Master will send data :
0x00 0x01 0x02 0x03 0x04 0x05 0x06 0x07
0x08 0x09 0x0A 0x0B 0x0C 0x0D 0x0E 0x0F
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1A 0x1B 0x1C 0x1D 0x1E 0x1F
Slave received data :
0x00 0x01 0x02 0x03 0x04 0x05 0x06 0x07
0x08 0x09 0x0A 0x0B 0x0C 0x0D 0x0E 0x0F
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1A 0x1B 0x1C 0x1D 0x1E 0x1F