MCUXpresso SDK Documentation

flexcomm_spi_interrupt_b2b_master

flexcomm_spi_interrupt_b2b_master#

Overview#

The spi_interrupt_b2b_master example shows how to use spi functional API to do interrupt transfer as a master:

In this example, the spi instance as master. Master sends a piece of data to slave, receive data from slave,and check if the data master received is correct. This example needs to work with spi_interrupt_b2b_slave example.

Supported Boards#

EVK-MIMXRT595
Hardware requirements
  • Micro USB cable

  • EVK-MIMXRT595 board

  • Personal Computer

Board settings

The example provides 2 options of SPI interfaces in communication.

  1. SPI5 (default, normal SPI: #define USE_HS_SPI 0)

  2. SPI14 (optional, high speed SPI: #define USE_HS_SPI 1) User can change the USE_HS_SPI value in spi_interrupt_b2b_master.c to choose different SPI interface.

Connect SPI master on board to SPI slave on other board. Only 1 set of signals need to be connected, either SPI5 or SPI14 depending on the USE_HS_SPI setting. NOTE: To use SPI14 on EVK board, please connect JP32 1-2.

    Master_board(SPI14)             Slave_board(SPI14) 
Pin Name   Board Location     Pin Name   Board Location
MISO       J36 pin 5          MISO       J36 pin 5
MOSI       J36 pin 3          MOSI       J36 pin 3
SCK        J36 pin 7          SCK        J36 pin 7
PCS0       J36 pin 1          PCS0       J36 pin 1
GND        J36 pin 9          GND        J36 pin 9

Connect SPI master on board to SPI slave on other board

    Master_board(SPI5)           Slave_board(SPI5)                          
Pin Name   Board Location     Pin Name   Board Location                     
MISO       JP26 pin 3          MISO      JP26 pin 3  
MOSI       JP26 pin 2          MOSI      JP26 pin 2  
SCK        JP26 pin 4          SCK       JP26 pin 4  
PCS0       JP26 pin 1          PCS0      JP26 pin 1  
GND        JP26 pin 5          GND       JP26 pin 5  
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:

SPI board to board interrupt master example started!

SPI transfer finished!
EVK-MIMXRT685
Hardware requirements
  • Micro USB cable

  • EVK-MIMXRT685 board

  • Personal Computer

Board settings

Connect SPI master on board to SPI slave on other board.

    Master_board(SPI5)           Slave_board(SPI5)
Pin Name   Board Location     Pin Name   Board Location
MISO       J28 pin 5          MISO       J28 pin 5
MOSI       J28 pin 4          MOSI       J28 pin 4
SCK        J28 pin 6          SCK        J28 pin 6
PCS0       J28 pin 3          PCS0       J28 pin 3
GND        J28 pin 7          GND        J28 pin 7
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:

SPI board to board interrupt master example started!

SPI transfer finished!
FRDM-MCXW23
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW23 Board

  • Personal Computer

Board settings
MASTER_BOARD           CONNECTS TO         SLAVE_BOARD
Pin Name      Board Location            Pin Name      Board Location 
SPI_SSEL1     J1-5                      SPI_SSEL1     J1-5          
SPI_MOSI      J4-2                      SPI_MOSI      J4-2          
SPI_MISO      J4-1                      SPI_MISO      J4-1          
SPI_SCK       J4-6                      SPI_SCK       J4-6          
GND           J3-7                      GND           J3-7          

Use the default jumper settings.

Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board J10.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:

​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ SPI board to board interrupt master example started!

SPI transfer finished! ​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

FRDM-RW612
Hardware requirements
  • Micro USB cable

  • FRDM-RW612 board

  • Personal Computer

Board settings

Connect SPI master on board to SPI slave on other board.

    Master_board(SPI1)           Slave_board(SPI1)
Pin Name   Board Location     Pin Name   Board Location
MISO       J1 pin 4           MISO       J1 pin 4
MOSI       J1 pin 2           MOSI       J1 pin 2
SCK        J2 pin 12          SCK        J2 pin 12
PCS0       J2 pin 6           PCS0       J2 pin 6
GND        J3 pin 14          GND        J3 pin 14
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J10) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:

SPI board to board interrupt master example started!

SPI transfer finished!
LPCXpresso51U68
Hardware requirements
  • Micro USB cable

  • LPCXpresso51U68 board

  • Personal Computer

Board settings

Populate jumper JP3. Connect SPI master on board to SPI slave on other board

Master - SPI3
Pin Name   Board Location
MISO       J4 pin 3
MOSI       J4 pin 2
SCK        J4 pin 4
PCS2       J4 pin 7
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J6) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:

SPI board to board interrupt master example started!

SPI transfer finished!
LPCXpresso54628
Hardware requirements
  • Micro USB cable

  • LPCXpresso54628 board

  • Personal Computer

Board settings

SPI one board: Transfer data from SPI master interface on board to other SPI interface on other board

INSTANCE0(SPI9)                                       
Pin Name   Board Location                             
MISO       J9 pin 11
MOSI       J9 pin 13
SCK        J9 pin 9
PCS0       J9 pin 15
GND        P3 Pin 1
Prepare the Demo
  1. Connect a Micro USB cable between the PC host and the LPC-Link USB port (J8) on the board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:

SPI board to board interrupt master example started!

SPI transfer finished!
LPCXpresso54S018
Hardware requirements
  • Micro USB cable

  • LPCXpresso54S018 board

  • Personal Computer

Board settings

SPI one board: Transfer data from SPI master interface on board to other SPI interface on other board

INSTANCE0(SPI9)                                       
Pin Name   Board Location                             
MISO       J9 pin 11
MOSI       J9 pin 13
SCK        J9 pin 9
PCS0       J9 pin 15
##### Prepare the Demo
1.  Connect a Micro USB cable between the PC host and the LPC-Link USB port (J8) on the board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Reset the SoC and run the project.

##### Running the demo
This demo is an external flash plain load demo, ROM will copy image in external flash to SRAMX to run:
1. Build the demo to generate a bin file.
   Note: If need to generate bin file using MCUXpresso IDE, below steps need to be followed:
         Set in example Properties->C/C++ Build->Settings->Build steps->Post-build steps->Edit
         enbable arm-none-eabi-objcopy -v -O binary "&{BuildArtifactFileName}" "&{BuildArtifactFileBaseName}.bin" 
         
         This plainload example linked the vector table to 0x00000000, but program to external flash 0x10000000.

2. Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):

   a. Open SEGGER J-FLASH Lite, select device LPC54S018.

   b. Click the 'Erase Chip' to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)

   c. Select the bin data file, set the '.bin/Erase Start' address to 0x10000000, then click 'Program Device'
Note: Please use above way to program the binary file built by armgcc tool chain to external flash. 
      For IAR, KEIL, MCUXpresso IDE, you can use the IDE tool to program the external flash.  
When the demo runs successfully, the log would be seen on the terminal like:

SPI board to board interrupt master example started!

SPI transfer finished!


LPCXpresso54S018M
Hardware requirements
  • Micro USB cable

  • LPCXpresso54S018M board

  • Personal Computer

Board settings

SPI one board: Transfer data from SPI master interface on board to other SPI interface on other board

INSTANCE0(SPI9)                                       
Pin Name   Board Location                             
MISO       J9 pin 11
MOSI       J9 pin 13
SCK        J9 pin 9
PCS0       J9 pin 15
##### Prepare the Demo
1.  Connect a Micro USB cable between the PC host and the LPC-Link USB port (J8) on the board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Reset the SoC and run the project.

##### Running the demo
This demo is an external flash plain load demo, ROM will copy image in external flash to SRAMX to run:
1. Build the demo to generate a bin file.
   Note: If need to generate bin file using MCUXpresso IDE, below steps need to be followed:
         Set in example Properties->C/C++ Build->Settings->Build steps->Post-build steps->Edit
         enbable arm-none-eabi-objcopy -v -O binary "&{BuildArtifactFileName}" "&{BuildArtifactFileBaseName}.bin" 
         
         This plainload example linked the vector table to 0x00000000, but program to external flash 0x10000000.

2. Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):

   a. Open SEGGER J-FLASH Lite, select device LPC54S018M.

   b. Click the 'Erase Chip' to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)

   c. Select the bin data file, set the '.bin/Erase Start' address to 0x10000000, then click 'Program Device'
Note: Please use above way to program the binary file built by armgcc tool chain to external flash. 
      For IAR, KEIL, MCUXpresso IDE, you can use the IDE tool to program the external flash.  
When the demo runs successfully, the log would be seen on the terminal like:

SPI board to board interrupt master example started!

SPI transfer finished!


LPCXpresso55S06
Hardware requirements
  • Micro USB cable

  • Two LPCXpresso55S06 boards

  • Personal Computer

Board settings

SPI one board: Transfer data from SPI master interface on board to other SPI interface on other board

    Master_board(SPI3)           Slave_board(SPI3)                          
Pin Name   Board Location     Pin Name   Board Location                     
MISO       J12   pin 2        MISO       J12   pin 2
MOSI       J12   pin 1        MOSI       J12   pin 1
SCK        J10   pin 16       SCK        J10   pin 16
SSEL0      J10   pin 14       SSEL0      J10   pin 14
GND        J9    pin 8        GND        J9    pin 8
Prepare the Demo
  1. Connect a Micro USB cable between the PC host and the LPC-Link USB port (J1) on the board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:

​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ SPI board to board interrupt master example started!

SPI transfer finished! ​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~


LPCXpresso55S16
Hardware requirements
  • Micro USB cable

  • Two LPCXpresso55S16 boards

  • Personal Computer

Board settings

SPI one board: Transfer data from SPI master interface on board to other SPI interface on other board

    Master_board(SPI7)           Slave_board(SPI7)                          
Pin Name   Board Location     Pin Name   Board Location                     
MISO       J9    pin 11       MISO       J9    pin 11
MOSI       J9    pin 9        MOSI       J9    pin 9
SCK        J9    pin 13       SCK        J9    pin 13
SSEL1      J9    pin 2        SSEL1      J9    pin 2
GND        J9    pin 8        GND        J9    pin 8

The jumper setting: Default jumpers configuration does not work, you will need to add JP20 and JP21 (JP22 optional for ADC use)

##### Prepare the Demo
1.  Connect a Micro USB cable between the PC host and the LPC-Link USB port (J1) on the board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Reset the SoC and run the project.

##### Running the demo
When the demo runs successfully, the log would be seen on the terminal like:

​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
SPI board to board interrupt master example started!

SPI transfer finished!
​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

LPCXpresso55S28
Hardware requirements
  • Micro USB cable

  • Two LPCXpresso55S28 boards

  • Personal Computer

Board settings

SPI one board: Transfer data from SPI master interface on board to other SPI interface on other board

    Master_board(SPI7)           Slave_board(SPI7)                          
Pin Name   Board Location     Pin Name   Board Location                     
MISO       P17  pin 12          MISO      P17  pin 12
MOSI       P17  pin 10          MOSI      P17  pin 10
SCK        P17  pin 14           SCK      P17  pin 14
SSEL1      P17  pin 1          SSEL1      P17  pin 1
GND        P17  pin 7           GND       P17  pin 7
##### Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
1.  Connect a Micro USB cable between the PC host and the LPC-Link USB port (P6) on the board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Reset the SoC and run the project.

##### Running the demo
When the demo runs successfully, the log would be seen on the terminal like:

​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
SPI board to board interrupt master example started!

SPI transfer finished!
​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

LPCXpresso55S36
Hardware requirements
  • Micro USB cable

  • Two LPCXpresso55S36 boards

  • Personal Computer

Board settings

Short JP51 1-2, JP52 1-2.

SPI one board: Transfer data from SPI master interface on board to other SPI interface on other board

    Master_board(SPI2)           Slave_board(SPI2)                          
Pin Name   Board Location     Pin Name   Board Location                     
MISO       J122  pin 12       MISO       J122  pin 12 
MOSI       J8    pin 3        MOSI       J8    pin 3
SCK        J122  pin 8        SCK        J122  pin 8
SSEL0      J122  pin 6        SSEL0      J122  pin 6
GND        J92   pin 14       GND        J92   pin 14
##### Prepare the Demo
1.  Connect a Micro USB cable between the PC host and the LPC-Link USB port (J1) on the board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Reset the SoC and run the project.

##### Running the demo
When the demo runs successfully, the log would be seen on the terminal like:

​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
SPI board to board interrupt master example started!

SPI transfer finished!
​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

LPCXpresso55S69
Hardware requirements
  • Micro USB cable

  • Two LPCXpresso55s69 boards

  • Personal Computer

Board settings

SPI one board: Transfer data from SPI master interface on board to other SPI interface on other board

    Master_board(SPI7)           Slave_board(SPI7)                          
Pin Name   Board Location     Pin Name   Board Location                     
MISO       P17  pin 12          MISO      P17  pin 12
MOSI       P17  pin 10          MOSI      P17  pin 10
SCK        P17  pin 14           SCK      P17  pin 14
SSEL1      P17  pin 1          SSEL1      P17  pin 1
GND        P17  pin 7           GND       P17  pin 7
##### Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
1.  Connect a Micro USB cable between the PC host and the LPC-Link USB port (P6) on the board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Reset the SoC and run the project.

##### Running the demo
When the demo runs successfully, the log would be seen on the terminal like:

​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
SPI board to board interrupt master example started!

SPI transfer finished!
​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

MIMXRT685-AUD-EVK
Hardware requirements
  • Micro USB cable

  • MIMXRT685-AUD-EVK board

  • Personal Computer

Board settings

Make sure the JP41 2-3 is connected.

Connect SPI master on board to SPI slave on other board.

    Master_board(SPI5)           Slave_board(SPI5)
Pin Name   Board Location     Pin Name   Board Location
MISO       J28 pin 5          MISO       J28 pin 5
MOSI       J28 pin 4          MOSI       J28 pin 4
SCK        J28 pin 6          SCK        J28 pin 6
PCS0       J28 pin 3          PCS0       J28 pin 3
GND        J28 pin 7          GND        J28 pin 7
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:

SPI board to board interrupt master example started!

SPI transfer finished!
RD-RW612-BGA
Hardware requirements
  • Micro USB cable

  • RD-RW612-BGA board

  • Personal Computer

Board settings

Connect JP30 1-2, JP9, JP19, JP23, JP51. Disconnect JP47 and connect JP47-1 to GND(J8-6). Extra rework is needed for the slave board besides the above connection, remove R97, R415, R594 and install R409, R49, R13.

Connect SPI master on board to SPI slave on other board.

    Master_board(SPI0)           Slave_board(SPI0)
Pin Name   Board Location     Pin Name   Board Location
MISO       J5 pin 5           MISO       J5 pin 5
MOSI       J5 pin 4           MOSI       J5 pin 4
SCK        J5 pin 6           SCK        J5 pin 6
PCS0       J5 pin 3           PCS0       J5 pin 3
GND        J5 pin 7           GND        J5 pin 7
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:

SPI board to board interrupt master example started!

SPI transfer finished!
MCXW23-EVK
Hardware requirements
  • Mini/micro USB cable

  • MCXW23-EVK Board

  • Personal Computer

Board settings
MASTER_BOARD           CONNECTS TO         SLAVE_BOARD
Pin Name      Board Location            Pin Name      Board Location 
SPI_SSEL1     J24-3                     SPI_SSEL1     J24-3
SPI_MOSI      J18-6                     SPI_MOSI      J18-6
SPI_MISO      J18-5                     SPI_MISO      J18-5
SPI_SCK       J18-4                     SPI_SCK       J18-4
GND           J18-8                     GND           J18-8

Use the default jumper settings.

Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J33.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:

​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ SPI board to board interrupt master example started!

SPI transfer finished! ​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~