MCUXpresso SDK Documentation

flexcomm_spi_dma_b2b_transfer_master#

Overview#

The spi_dma_b2b_transfer_master example shows how to use driver API to transfer in DMA way.

In this example, one spi instance as master and another spi instance on the other board as slave. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct. This example needs to work with spi_dma_b2b_transfer_slave example.

Note: This example will run in master mode, please prepare another board for slave, and the slave board should be started first.

Project Infomation#

1.How to set the baudrate of SPI? The baudrate of SPI is easy to set, just make sure the source clock of SPI. The formula is below:

baudrate = PCLK_SPIn / DIVVAL SPIn->DIV = DIVVAL -1 For example, if the needed baudrate of SPI is 500khz, and the SPI clock is 12MHz DIVVAL = 12000000/500000 DIVVAL = 24 SPIn->DIV = DIVVAL -1 = 23

Program Flow:#

Main routine: 1.Initialize the hardware. Configure pin settings, clock settings by using BOARD_InitHardware();

2.Send information to terminal by using debug console.

3.Initialize the SPI with configuration.

4.Set up DMA configuration for master SPI. Initialize DMA and DMA channel setting(create handle and set callback) for both SPI RX and TX, set prioritory for TX channel and RX channel.

5.Start SPI master transfer in DMA way. Initialize buffers and start SPI transfer in DMA way.

6.Check if data from master is all right. Waiting for transmission complete, print received data and log information to terminal.

7.De-initialize the SPI and DMA.

Supported Boards#

EVK-MIMXRT595
Hardware requirements
  • Micro USB cable

  • EVK-MIMXRT595 board

  • Personal Computer

Board settings

The example provides 2 options of SPI interfaces in communication.

  1. SPI5 (default, normal SPI: #define USE_HS_SPI 0)

  2. SPI14 (optional, high speed SPI: #define USE_HS_SPI 1) User can change the USE_HS_SPI value in spi_dma_b2b_transfer_master.c to choose different SPI interface.

Connect SPI master on board to SPI slave on other board. Only 1 set of signals need to be connected, either SPI5 or SPI14 depending on the USE_HS_SPI setting. NOTE: To use SPI14 on EVK board, please connect JP32 1-2.

    Master_board(SPI14)             Slave_board(SPI14) 
Pin Name   Board Location     Pin Name   Board Location
MISO       J36 pin 5          MISO       J36 pin 5
MOSI       J36 pin 3          MOSI       J36 pin 3
SCK        J36 pin 7          SCK        J36 pin 7
PCS0       J36 pin 1          PCS0       J36 pin 1
GND        J36 pin 9          GND        J36 pin 9

Connect SPI master on board to SPI slave on other board

    Master_board(SPI5)           Slave_board(SPI5)                          
Pin Name   Board Location     Pin Name   Board Location                     
MISO       JP26 pin 3          MISO      JP26 pin 3  
MOSI       JP26 pin 2          MOSI      JP26 pin 2  
SCK        JP26 pin 4          SCK       JP26 pin 4  
PCS0       JP26 pin 1          PCS0      JP26 pin 1  
GND        JP26 pin 5          GND       JP26 pin 5  
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:

This is SPI DMA tranfer master example.
This example will communicate with another slave SPI on the other board.
Please start the slave board first!

The received data are:
    0x00  0x01  0x02  0x03  0x04  0x05  0x06  0x07  0x08  0x09  0x0A  0x0B  0x0C  0x0D  0x0E  0x0F
    0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17  0x18  0x19  0x1A  0x1B  0x1C  0x1D  0x1E  0x1F
    0x20  0x21  0x22  0x23  0x24  0x25  0x26  0x27  0x28  0x29  0x2A  0x2B  0x2C  0x2D  0x2E  0x2F
    0x30  0x31  0x32  0x33  0x34  0x35  0x36  0x37  0x38  0x39  0x3A  0x3B  0x3C  0x3D  0x3E  0x3F
SPI transfer all data matched!

EVK-MIMXRT685
Hardware requirements
  • Micro USB cable

  • EVK-MIMXRT685 board

  • Personal Computer

Board settings

Connect SPI master on board to SPI slave on other board.

    Master_board(SPI5)           Slave_board(SPI5)
Pin Name   Board Location     Pin Name   Board Location
MISO       J28 pin 5          MISO       J28 pin 5
MOSI       J28 pin 4          MOSI       J28 pin 4
SCK        J28 pin 6          SCK        J28 pin 6
PCS0       J28 pin 3          PCS0       J28 pin 3
GND        J28 pin 7          GND        J28 pin 7
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:

This is SPI DMA tranfer master example.
This example will communicate with another slave SPI on the other board.
Please start the slave board first!

The received data are:
    0x00  0x01  0x02  0x03  0x04  0x05  0x06  0x07  0x08  0x09  0x0A  0x0B  0x0C  0x0D  0x0E  0x0F
    0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17  0x18  0x19  0x1A  0x1B  0x1C  0x1D  0x1E  0x1F
    0x20  0x21  0x22  0x23  0x24  0x25  0x26  0x27  0x28  0x29  0x2A  0x2B  0x2C  0x2D  0x2E  0x2F
    0x30  0x31  0x32  0x33  0x34  0x35  0x36  0x37  0x38  0x39  0x3A  0x3B  0x3C  0x3D  0x3E  0x3F
SPI transfer all data matched!

FRDM-MCXW23
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW23 Board

  • Personal Computer

Board settings
MASTER_BOARD           CONNECTS TO         SLAVE_BOARD
Pin Name      Board Location            Pin Name      Board Location 
SPI_SSEL1     J1-5                      SPI_SSEL1     J1-5          
SPI_MOSI      J4-2                      SPI_MOSI      J4-2          
SPI_MISO      J4-1                      SPI_MISO      J4-1          
SPI_SCK       J4-6                      SPI_SCK       J4-6          
GND           J3-7                      GND           J3-7          

Use the default jumper settings.

Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board J10.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:

This is SPI DMA transfer master example.
This example will communicate with another slave SPI on the other board.
Please start the slave board first!

The received data are:
    0x00  0x01  0x02  0x03  0x04  0x05  0x06  0x07  0x08  0x09  0x0A  0x0B  0x0C  0x0D  0x0E  0x0F
    0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17  0x18  0x19  0x1A  0x1B  0x1C  0x1D  0x1E  0x1F
    0x20  0x21  0x22  0x23  0x24  0x25  0x26  0x27  0x28  0x29  0x2A  0x2B  0x2C  0x2D  0x2E  0x2F
    0x30  0x31  0x32  0x33  0x34  0x35  0x36  0x37  0x38  0x39  0x3A  0x3B  0x3C  0x3D  0x3E  0x3F
SPI transfer all data matched!

​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
FRDM-RW612
Hardware requirements
  • Micro USB cable

  • FRDM-RW612 board

  • Personal Computer

Board settings

Connect SPI master on board to SPI slave on other board.

    Master_board(SPI1)           Slave_board(SPI1)
Pin Name   Board Location     Pin Name   Board Location
MISO       J1 pin 4           MISO       J1 pin 4
MOSI       J1 pin 2           MOSI       J1 pin 2
SCK        J2 pin 12          SCK        J2 pin 12
PCS0       J2 pin 6           PCS0       J2 pin 6
GND        J3 pin 14          GND        J3 pin 14
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J10) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:

This is SPI DMA tranfer master example.
This example will communicate with another slave SPI on the other board.
Please start the slave board first!

The received data are:
    0x00  0x01  0x02  0x03  0x04  0x05  0x06  0x07  0x08  0x09  0x0A  0x0B  0x0C  0x0D  0x0E  0x0F
    0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17  0x18  0x19  0x1A  0x1B  0x1C  0x1D  0x1E  0x1F
    0x20  0x21  0x22  0x23  0x24  0x25  0x26  0x27  0x28  0x29  0x2A  0x2B  0x2C  0x2D  0x2E  0x2F
    0x30  0x31  0x32  0x33  0x34  0x35  0x36  0x37  0x38  0x39  0x3A  0x3B  0x3C  0x3D  0x3E  0x3F
SPI transfer all data matched!

LPCXpresso54628
Hardware requirements
  • Micro USB cable

  • Two LPCXpresso54628 boards

  • Personal Computer

Board settings

Populate jumper JP6. Connect SPI master on board to SPI slave on other board

    Master_board(SPI9)           Slave_board(SPI9)                          
Pin Name   Board Location     Pin Name   Board Location                     
MISO       J9  pin 11          MISO       J9  pin 11
MOSI       J9  pin 13          MOSI       J9  pin 13
SCK        J9  pin 9           SCK        J9  pin 9
PCS0       J9  pin 15          PCS0       J9  pin 15
GND        J14 pin 5           GND        J14 pin 5

Change the solder jumper JS27 to 2-3 to use P3_30 pin as SSEL or to use the Arduino connector J9 Pin 15.

##### Prepare the Demo
1.  Connect a micro USB cable between the PC host and the LPC-Link USB port (J8) on the board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Reset the SoC and run the project.

##### Running the demo
When the demo runs successfully, the log would be seen on the terminal like:

This is SPI DMA transfer master example. This example will communicate with another slave SPI on the other board. Please start the slave board first!

The received data are: 0x00 0x01 0x02 0x03 0x04 0x05 0x06 0x07 0x08 0x09 0x0A 0x0B 0x0C 0x0D 0x0E 0x0F 0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17 0x18 0x19 0x1A 0x1B 0x1C 0x1D 0x1E 0x1F 0x20 0x21 0x22 0x23 0x24 0x25 0x26 0x27 0x28 0x29 0x2A 0x2B 0x2C 0x2D 0x2E 0x2F 0x30 0x31 0x32 0x33 0x34 0x35 0x36 0x37 0x38 0x39 0x3A 0x3B 0x3C 0x3D 0x3E 0x3F SPI transfer all data matched!


LPCXpresso55S06
Hardware requirements
  • Micro USB cable

  • Two LPCXpresso55S06 boards

  • Personal Computer

Board settings

Connect SPI master on board to SPI slave on other board

    Master_board(SPI3)           Slave_board(SPI3)                          
Pin Name   Board Location     Pin Name   Board Location                     
MISO       J12   pin 2        MISO       J12   pin 2
MOSI       J12   pin 1        MOSI       J12   pin 1
SCK        J10   pin 16       SCK        J10   pin 16
SSEL0      J10   pin 14       SSEL0      J10   pin 14
GND        J9    pin 8        GND        J9    pin 8
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:

This is SPI DMA transfer master example.
This example will communicate with another slave SPI on the other board.
Please start the slave board first!

The received data are:
    0x00  0x01  0x02  0x03  0x04  0x05  0x06  0x07  0x08  0x09  0x0A  0x0B  0x0C  0x0D  0x0E  0x0F
    0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17  0x18  0x19  0x1A  0x1B  0x1C  0x1D  0x1E  0x1F
    0x20  0x21  0x22  0x23  0x24  0x25  0x26  0x27  0x28  0x29  0x2A  0x2B  0x2C  0x2D  0x2E  0x2F
    0x30  0x31  0x32  0x33  0x34  0x35  0x36  0x37  0x38  0x39  0x3A  0x3B  0x3C  0x3D  0x3E  0x3F
SPI transfer all data matched!

​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

LPCXpresso55S16
Hardware requirements
  • Micro USB cable

  • Two LPCXpresso55S16 boards

  • Personal Computer

Board settings

Connect SPI master on board to SPI slave on other board

    Master_board(SPI7)           Slave_board(SPI7)                          
Pin Name   Board Location     Pin Name   Board Location                     
MISO       J9    pin 11       MISO       J9    pin 11
MOSI       J9    pin 9        MOSI       J9    pin 9
SCK        J9    pin 13       SCK        J9    pin 13
SSEL1      J9    pin 2        SSEL1      J9    pin 2
GND        J9    pin 8        GND        J9    pin 8

The jumper setting: Default jumpers configuration does not work, you will need to add JP20 and JP21 (JP22 optional for ADC use)

Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:

This is SPI DMA transfer master example.
This example will communicate with another slave SPI on the other board.
Please start the slave board first!

The received data are:
    0x00  0x01  0x02  0x03  0x04  0x05  0x06  0x07  0x08  0x09  0x0A  0x0B  0x0C  0x0D  0x0E  0x0F
    0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17  0x18  0x19  0x1A  0x1B  0x1C  0x1D  0x1E  0x1F
    0x20  0x21  0x22  0x23  0x24  0x25  0x26  0x27  0x28  0x29  0x2A  0x2B  0x2C  0x2D  0x2E  0x2F
    0x30  0x31  0x32  0x33  0x34  0x35  0x36  0x37  0x38  0x39  0x3A  0x3B  0x3C  0x3D  0x3E  0x3F
SPI transfer all data matched!

​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

LPCXpresso55S28
Hardware requirements
  • Micro USB cable

  • Two LPCXpresso55S28 boards

  • Personal Computer

Board settings

Connect SPI master on board to SPI slave on other board

    Master_board(SPI7)           Slave_board(SPI7)                          
Pin Name   Board Location     Pin Name   Board Location                     
MISO       P17  pin 12          MISO      P17  pin 12
MOSI       P17  pin 10          MOSI      P17  pin 10
SCK        P17  pin 14           SCK      P17  pin 14
SSEL1      P17  pin 1          SSEL1      P17  pin 1
GND        P17  pin 7           GND       P17  pin 7
Prepare the Demo

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:

This is SPI DMA transfer master example.
This example will communicate with another slave SPI on the other board.
Please start the slave board first!

The received data are:
    0x00  0x01  0x02  0x03  0x04  0x05  0x06  0x07  0x08  0x09  0x0A  0x0B  0x0C  0x0D  0x0E  0x0F
    0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17  0x18  0x19  0x1A  0x1B  0x1C  0x1D  0x1E  0x1F
    0x20  0x21  0x22  0x23  0x24  0x25  0x26  0x27  0x28  0x29  0x2A  0x2B  0x2C  0x2D  0x2E  0x2F
    0x30  0x31  0x32  0x33  0x34  0x35  0x36  0x37  0x38  0x39  0x3A  0x3B  0x3C  0x3D  0x3E  0x3F
SPI transfer all data matched!

​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

LPCXpresso55S36
Hardware requirements
  • Micro USB cable

  • Two LPCXpresso55S36 boards

  • Personal Computer

Board settings

Shor JP51 1-2, JP52 1-2.

Connect SPI master on board to SPI slave on other board

    Master_board(SPI2)           Slave_board(SPI2)                          
Pin Name   Board Location     Pin Name   Board Location                     
MISO       J122  pin 12       MISO       J122  pin 12 
MOSI       J8    pin 3        MOSI       J8    pin 3
SCK        J122  pin 8        SCK        J122  pin 8
SSEL0      J122  pin 6        SSEL0      J122  pin 6
GND        J92   pin 14       GND        J92   pin 14
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:

This is SPI DMA transfer master example.
This example will communicate with another slave SPI on the other board.
Please start the slave board first!

The received data are:
    0x00  0x01  0x02  0x03  0x04  0x05  0x06  0x07  0x08  0x09  0x0A  0x0B  0x0C  0x0D  0x0E  0x0F
    0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17  0x18  0x19  0x1A  0x1B  0x1C  0x1D  0x1E  0x1F
    0x20  0x21  0x22  0x23  0x24  0x25  0x26  0x27  0x28  0x29  0x2A  0x2B  0x2C  0x2D  0x2E  0x2F
    0x30  0x31  0x32  0x33  0x34  0x35  0x36  0x37  0x38  0x39  0x3A  0x3B  0x3C  0x3D  0x3E  0x3F
SPI transfer all data matched!

​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

LPCXpresso55S69
Hardware requirements
  • Micro USB cable

  • Two LPCXpresso55s69 boards

  • Personal Computer

Board settings

Connect SPI master on board to SPI slave on other board

    Master_board(SPI7)           Slave_board(SPI7)                          
Pin Name   Board Location     Pin Name   Board Location                     
MISO       P17  pin 12          MISO      P17  pin 12
MOSI       P17  pin 10          MOSI      P17  pin 10
SCK        P17  pin 14           SCK      P17  pin 14
SSEL1      P17  pin 1          SSEL1      P17  pin 1
GND        P17  pin 7           GND       P17  pin 7
Prepare the Demo

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:

This is SPI DMA transfer master example.
This example will communicate with another slave SPI on the other board.
Please start the slave board first!

The received data are:
    0x00  0x01  0x02  0x03  0x04  0x05  0x06  0x07  0x08  0x09  0x0A  0x0B  0x0C  0x0D  0x0E  0x0F
    0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17  0x18  0x19  0x1A  0x1B  0x1C  0x1D  0x1E  0x1F
    0x20  0x21  0x22  0x23  0x24  0x25  0x26  0x27  0x28  0x29  0x2A  0x2B  0x2C  0x2D  0x2E  0x2F
    0x30  0x31  0x32  0x33  0x34  0x35  0x36  0x37  0x38  0x39  0x3A  0x3B  0x3C  0x3D  0x3E  0x3F
SPI transfer all data matched!

​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

MIMXRT685-AUD-EVK
Hardware requirements
  • Micro USB cable

  • MIMXRT685-AUD-EVK board

  • Personal Computer

Board settings

Make sure the JP41 2-3 is connected.

Connect SPI master on board to SPI slave on other board.

    Master_board(SPI5)           Slave_board(SPI5)
Pin Name   Board Location     Pin Name   Board Location
MISO       J28 pin 5          MISO       J28 pin 5
MOSI       J28 pin 4          MOSI       J28 pin 4
SCK        J28 pin 6          SCK        J28 pin 6
PCS0       J28 pin 3          PCS0       J28 pin 3
GND        J28 pin 7          GND        J28 pin 7
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:

This is SPI DMA tranfer master example.
This example will communicate with another slave SPI on the other board.
Please start the slave board first!

The received data are:
    0x00  0x01  0x02  0x03  0x04  0x05  0x06  0x07  0x08  0x09  0x0A  0x0B  0x0C  0x0D  0x0E  0x0F
    0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17  0x18  0x19  0x1A  0x1B  0x1C  0x1D  0x1E  0x1F
    0x20  0x21  0x22  0x23  0x24  0x25  0x26  0x27  0x28  0x29  0x2A  0x2B  0x2C  0x2D  0x2E  0x2F
    0x30  0x31  0x32  0x33  0x34  0x35  0x36  0x37  0x38  0x39  0x3A  0x3B  0x3C  0x3D  0x3E  0x3F
SPI transfer all data matched!

RD-RW612-BGA
Hardware requirements
  • Micro USB cable

  • RD-RW612-BGA board

  • Personal Computer

Board settings

Connect JP30 1-2, JP9, JP19, JP23, JP51. Disconnect JP47 and connect JP47-1 to GND(J8-6). Extra rework is needed for the slave board besides the above connection, remove R97, R415, R594 and install R409, R49, R13.

Connect SPI master on board to SPI slave on other board.

    Master_board(SPI0)           Slave_board(SPI0)
Pin Name   Board Location     Pin Name   Board Location
MISO       J5 pin 5           MISO       J5 pin 5
MOSI       J5 pin 4           MOSI       J5 pin 4
SCK        J5 pin 6           SCK        J5 pin 6
PCS0       J5 pin 3           PCS0       J5 pin 3
GND        J5 pin 7           GND        J5 pin 7
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:

This is SPI DMA tranfer master example.
This example will communicate with another slave SPI on the other board.
Please start the slave board first!

The received data are:
    0x00  0x01  0x02  0x03  0x04  0x05  0x06  0x07  0x08  0x09  0x0A  0x0B  0x0C  0x0D  0x0E  0x0F
    0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17  0x18  0x19  0x1A  0x1B  0x1C  0x1D  0x1E  0x1F
    0x20  0x21  0x22  0x23  0x24  0x25  0x26  0x27  0x28  0x29  0x2A  0x2B  0x2C  0x2D  0x2E  0x2F
    0x30  0x31  0x32  0x33  0x34  0x35  0x36  0x37  0x38  0x39  0x3A  0x3B  0x3C  0x3D  0x3E  0x3F
SPI transfer all data matched!

MCXW23-EVK
Hardware requirements
  • Mini/micro USB cable

  • MCXW23-EVK Board

  • Personal Computer

Board settings
MASTER_BOARD           CONNECTS TO         SLAVE_BOARD
Pin Name      Board Location            Pin Name      Board Location 
SPI_SSEL1     J24-3                     SPI_SSEL1     J24-3
SPI_MOSI      J18-6                     SPI_MOSI      J18-6
SPI_MISO      J18-5                     SPI_MISO      J18-5
SPI_SCK       J18-4                     SPI_SCK       J18-4
GND           J18-8                     GND           J18-8

Use the default jumper settings.

Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J33.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:

This is SPI DMA transfer master example.
This example will communicate with another slave SPI on the other board.
Please start the slave board first!

The received data are:
    0x00  0x01  0x02  0x03  0x04  0x05  0x06  0x07  0x08  0x09  0x0A  0x0B  0x0C  0x0D  0x0E  0x0F
    0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17  0x18  0x19  0x1A  0x1B  0x1C  0x1D  0x1E  0x1F
    0x20  0x21  0x22  0x23  0x24  0x25  0x26  0x27  0x28  0x29  0x2A  0x2B  0x2C  0x2D  0x2E  0x2F
    0x30  0x31  0x32  0x33  0x34  0x35  0x36  0x37  0x38  0x39  0x3A  0x3B  0x3C  0x3D  0x3E  0x3F
SPI transfer all data matched!

​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~