MCUXpresso SDK Documentation

dspi_interrupt_b2b_transfer_master

dspi_interrupt_b2b_transfer_master#

Overview#

The dspi_interrupt_b2b_transfer example shows how to use DSPI driver in interrupt way:

In this example , we need two boards, one board used as DSPI master and another board used as DSPI slave. The file ‘dspi_interrupt_b2b_transfer_master.c’ includes the DSPI master code. This example uses the transactional API in DSPI driver.

  1. DSPI master send/received data to/from DSPI slave in interrupt . (DSPI Slave using interrupt to receive/send the data)

Supported Boards#