dsc_i2c_polling_b2b_transfer_slave#
Overview#
The i2c_polling_b2b_transfer_slave example shows how to use i2c driver as slave to do board to board transfer with a polling master:
In this example, one i2c instance as slave and another i2c instance on the other board as master. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct.
Supported Boards#
MC56F83000-EVK
Hardware requirements
Micro USB cable
MC56F83000-EVK board
Personal Computer
Board hardware common setting
Power setting:
Connect J19 pin2 and pin3 Connect J12 pin1 and pin2 Connect J13 pin1 and pin2 Connect J15 pin1 and pin2 Connect J16 pin2 and pin3 Connect J17 pin1 and pin2
Onboard OSJTAG debugger setting:
Leave J5 open Leave J6 open Note: J6 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J11 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J10), leave all J11 pins open.
Board settings
MASTER_BOARD connects to SLAVE_BOARD as below:
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
I2C0_SCL J2-20 I2C0_SCL J2-20
I2C0_SDA J2-18 I2C0_SDA J2-18
GND J2-14 GND J2-14
Prepare the Demo
Connect USB cable between the host PC and the JM60 USB(J8) port on the target board. It setups OSJTAG and COM port in PC device manager.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board with OSJTAG debug configuration.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. Please be noted that default FCF(flash configuration field) setting makes MCU boot from bootloader. So after reset button press, it will wait 5s(wait in bootloader) to run the application code.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
I2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of I2C example .
~~~~~~~~~~~~~~~~~~~~~~~~~~~~
TWR-MC56F8200
Hardware requirements
Mini USB cable
TWR-MC56F8200 board
Personal Computer
Board hardware common setting
HW reworkd(workaround):
Connect J18(the mini USB port) pin4 and pin5. Note: This is due to HW design error, correct setting should be: J18 pin4 left empty and pin5 connected GND.
Power setting:
Connect J11 pin1 and pin2 Connect J6 pin1 and J7 pin2
UART setting:
Connect J8 pin3 and pin4 Connect J9 pin3 and pin4
Onboard OSJTAG debugger setting:
Connect J20 pin1 and pin2. Leave J17 open. Note: J17 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J21 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J14), leave all J21 pins open
Board settings
Pull-up SCL/SDA each to 3.3V with resistor(2.2K~5.1K ohm)
MASTER_BOARD connects to SLAVE_BOARD as below:
MASTER_BOARD CONNECTS TO SLAVE_BOARD Pin Name Board Location Pin Name Board Location I2C0_SCL J501-21 I2C0_SCL J501-21 I2C0_SDA J501-23 I2C0_SDA J501-23 GND J501-8 GND J501-8
Prepare the Demo
Connect USB cable between the host PC and the JM60 USB(J18) port on the target board. It setups OSJTAG and COM port in PC device manager.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board with OSJTAG debug configuration.
Launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
I2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of I2C example .
~~~~~~~~~~~~~~~~~~~~~~~~~~~~
TWR-MC56F8400
Hardware requirements
Mini USB cable
TWR-MC56F8400 board
Personal Computer
Board hardware common setting
Power setting:
Connect J11 pin1 and pin2 Connect J6 pin1 and J7 pin2
UART setting:
Connect J8 pin3 and pin4 Connect J9 pin3 and pin4
Onboard OSJTAG debugger setting:
Connect J20 pin1 and pin2. Leave J17 open. Note: J17 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J21 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J14), leave all J21 pins open
Board settings
Pull-up SCL/SDA each to 3.3V with resistor(2.2K~5.1K ohm)
MASTER_BOARD connects to SLAVE_BOARD as below:
MASTER_BOARD CONNECTS TO SLAVE_BOARD Pin Name Board Location Pin Name Board Location I2C0_SCL J501-21 I2C0_SCL J501-21 I2C0_SDA J501-23 I2C0_SDA J501-23 GND J501-8 GND J501-8
Prepare the Demo
Connect USB cable between the host PC and the JM60 USB(J18) port on the target board. It setups OSJTAG and COM port in PC device manager.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board with OSJTAG debug configuration.
Launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
I2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of I2C example .
~~~~~~~~~~~~~~~~~~~~~~~~~~~~