MCUXpresso SDK Documentation

dsc_i2c_interrupt_b2b_transfer_slave

dsc_i2c_interrupt_b2b_transfer_slave#

Overview#

The i2c_interrupt_b2b_transfer_slave example shows how to use i2c driver as slave to do board to board transfer with interrupt:

In this example, one i2c instance as slave and another i2c instance on the other board as master. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct.

Supported Boards#

MC56F83000-EVK
Hardware requirements
  • Micro USB cable

  • MC56F83000-EVK board

  • Personal Computer

Board hardware common setting
  1. Power setting:

    Connect J19 pin2 and pin3 Connect J12 pin1 and pin2 Connect J13 pin1 and pin2 Connect J15 pin1 and pin2 Connect J16 pin2 and pin3 Connect J17 pin1 and pin2

  2. Onboard OSJTAG debugger setting:

    Leave J5 open Leave J6 open Note: J6 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J11 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J10), leave all J11 pins open.

Board settings

MASTER_BOARD connects to SLAVE_BOARD as below:

MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name   Board Location     Pin Name   Board Location
I2C0_SCL   J2-20              I2C0_SCL   J2-20
I2C0_SDA   J2-18              I2C0_SDA   J2-18
GND        J2-14              GND        J2-14
Prepare the Demo
  1. Connect USB cable between the host PC and the JM60 USB(J8) port on the target board. It setups OSJTAG and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with OSJTAG debug configuration.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. Please be noted that default FCF(flash configuration field) setting makes MCU boot from bootloader. So after reset button press, it will wait 5s(wait in bootloader) to run the application code.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .
TWR-MC56F8200
Hardware requirements
  • Mini USB cable

  • TWR-MC56F8200 board

  • Personal Computer

Board hardware common setting
  1. HW reworkd(workaround):

    Connect J18(the mini USB port) pin4 and pin5. Note: This is due to HW design error, correct setting should be: J18 pin4 left empty and pin5 connected GND.

  2. Power setting:

    Connect J11 pin1 and pin2 Connect J6 pin1 and J7 pin2

  3. UART setting:

    Connect J8 pin3 and pin4 Connect J9 pin3 and pin4

  4. Onboard OSJTAG debugger setting:

    Connect J20 pin1 and pin2. Leave J17 open. Note: J17 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J21 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J14), leave all J21 pins open

Board settings
  • Pull-up SCL/SDA each to 3.3V with resistor(2.2K~5.1K ohm)

    MASTER_BOARD connects to SLAVE_BOARD as below:

    MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
    Pin Name   Board Location     Pin Name   Board Location
    I2C0_SCL   J501-21            I2C0_SCL   J501-21
    I2C0_SDA   J501-23            I2C0_SDA   J501-23
    GND        J501-8             GND        J501-8
    
Prepare the Demo
  1. Connect USB cable between the host PC and the JM60 USB(J18) port on the target board. It setups OSJTAG and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with OSJTAG debug configuration.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .
TWR-MC56F8400
Hardware requirements
  • Mini USB cable

  • TWR-MC56F8400 board

  • Personal Computer

Board hardware common setting
  1. Power setting:

    Connect J11 pin1 and pin2 Connect J6 pin1 and J7 pin2

  2. UART setting:

    Connect J8 pin3 and pin4 Connect J9 pin3 and pin4

  3. Onboard OSJTAG debugger setting:

    Connect J20 pin1 and pin2. Leave J17 open. Note: J17 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J21 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J14), leave all J21 pins open

Board settings
  • Pull-up SCL/SDA each to 3.3V with resistor(2.2K~5.1K ohm)

    MASTER_BOARD connects to SLAVE_BOARD as below:

    MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
    Pin Name   Board Location     Pin Name   Board Location
    I2C0_SCL   J501-21            I2C0_SCL   J501-21
    I2C0_SDA   J501-23            I2C0_SDA   J501-23
    GND        J501-8             GND        J501-8
    
Prepare the Demo
  1. Connect USB cable between the host PC and the JM60 USB(J18) port on the target board. It setups OSJTAG and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with OSJTAG debug configuration.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .