MCUXpresso SDK Documentation

flash_component_octal_xspi

flash_component_octal_xspi#

Overview#

octal flash demo shows the use of nor flash component to erase, program, and read an external serial nor flash device.

Supported Boards#

MIMXRT700-EVK
Hardware requirements
  • Mini/micro USB cable

  • RT700 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

***NOR Flash Component Demo Start!***

***NOR Flash Initialization Start!***

***NOR Flash Initialization Success!***


***NOR Flash Page 0 Read/Write Success!***


***NOR Flash Page 1 Read/Write Success!***


***NOR Flash Page 2 Read/Write Success!***


***NOR Flash Page 3 Read/Write Success!***


***NOR Flash Page 4 Read/Write Success!***


***NOR Flash Page 5 Read/Write Success!***


***NOR Flash Page 6 Read/Write Success!***


***NOR Flash Page 7 Read/Write Success!***


***NOR Flash Page 8 Read/Write Success!***


***NOR Flash Page 9 Read/Write Success!***


***NOR Flash Page 10 Read/Write Success!***


***NOR Flash Page 11 Read/Write Success!***


***NOR Flash Page 12 Read/Write Success!***


***NOR Flash Page 13 Read/Write Success!***


***NOR Flash Page 14 Read/Write Success!***


***NOR Flash Page 15 Read/Write Success!***

***NOR Flash All Pages Read/Write Success!***