flash_component_nand_semc#
Overview#
nand flash demo shows the use of nand flash component to erase, program, and read anexternal nand flash device.
Supported Boards#
MIMXRT1170-EVKB
Hardware requirements
Mini/micro USB cable
EVB-MIMXRT1170 board
Personal Computer
Board settings
To make the examples works, please add resistors: R1872,R1873,R1874,R1875,R1876,R1877,R1878,R1879
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
***NAND Flash Component Demo Start!***
***NAND Flash Initialization Start!***
***NAND Flash Initialization Success!***
***NAND Flash Erase The First Block Start!***
***NAND Flash Erase Check Start!***
***NAND Flash Erase block Success!***
***NAND Flash Page Program Start!***
***NAND Flash Page Read Start!***
.....
.....
.....
***NAND Flash Page Read/Write Success!***