MCUXpresso SDK Documentation

cmsis_lpspi_int_b2b_transfer_slave

cmsis_lpspi_int_b2b_transfer_slave#

Overview#

The lpspi_int_b2b_transfer example shows how to use LPSPI CMSIS driver in interrupt way:

In this example , we need two boards, one board used as LPSPI master and another board used as LPSPI slave. The file ‘cmsis_lpspi_int_b2b_transfer_slave.c’ includes the LPSPI slave code. This example uses the transactional API in LPSPI driver.

  1. LPSPI master send/received data to/from LPSPI slave in interrupt .

Supported Boards#