MCUXpresso SDK Documentation

cmsis_lpspi_edma_b2b_transfer_slave

cmsis_lpspi_edma_b2b_transfer_slave#

Overview#

The cmsis_lpspi_edma_b2b_transfer example shows how to use LPSPI CMSIS driver with eDMA.

In this example, we need two boards, one board used as LPSPI master and another board used as LPSPI slave. The file ‘cmsis_lpspi_edma_b2b_transfer_slave.c’ includes the LPSPI slave code.

The LPSPI master send/receive data to/from LPSPI slave using eDMA.

Running the demo#

When the demo runs successfully, you will see output in the terminal like this:

LPSPI CMSIS driver board to board edma example.

Slave example is running...

This is LPSPI_SlaveSignalEvent_t
Slave receive data from master has completed!
This is LPSPI_SlaveSignalEvent_t
Slave transmit data to master has completed!

Slave received:
     1  2  3  4  5  6  7  8  9  A  B  C  D  E  F 10
    11 12 13 14 15 16 17 18 19 1A 1B 1C 1D 1E 1F 20
    21 22 23 24 25 26 27 28 29 2A 2B 2C 2D 2E 2F 30
    31 32 33 34 35 36 37 38 39 3A 3B 3C 3D 3E 3F 40

Slave example is running...

Supported Boards#