MCUXpresso SDK Documentation

cmsis_spi_int_b2b_transfer_master

Contents

cmsis_spi_int_b2b_transfer_master#

Overview#

The cmsis_spi_int_b2b_transfer example shows how to use SPI CMSIS driver in interrupt way:

In this example , we need two boards, one board used as SPI master and another board used as SPI slave. The file ‘cmsis_spi_int_b2b_transfer_master.c’ includes the SPI master code.

  1. SPI master send/received data to/from SPI slave in interrupt way.