MCUXpresso SDK Documentation

cmsis_lpc_i2c_int_b2b_transfer_slave

cmsis_lpc_i2c_int_b2b_transfer_slave#

Overview#

CMSIS-Driver defines generic peripheral driver interfaces for middleware making it reusable across a wide range of supported microcontroller devices. The API connects microcontroller peripherals with middleware that implements for example communication stacks, file systems, or graphic user interfaces. More information and usage method please refer to http://www.keil.com/pack/doc/cmsis/Driver/html/index.html.

The i2c_interrupt_b2b_transfer_master example shows how to use CMSIS i2c driver as master to do board to board transfer with interrupt:

In this example, one i2c instance as master and another i2c instance on the other board as slave. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct.

Supported Boards#

EVK-MIMXRT595
Hardware requirements
  • Micro USB cable

  • EVK-MIMXRT595 board

  • Personal Computer

Board settings

I2C one board:

  • Transfer data from MASTER_BOARD to SLAVE_BOARD of I2C interface, I2C11 pins of MASTER_BOARD are connected with I2C11 pins of SLAVE_BOARD

EVK-MIMXRT595        CONNECTS TO         EVK-MIMXRT595
Pin  Name   Board Location     Pin Name   Board Location
P4_22 SDA    J28-9              P4_22       J28-9
P4_21 SCL    J28-10             P4_21       J28-10
GND          J28-7              GND         J28-7
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The following message shows in the terminal if the example runs successfully.

CMSIS I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .
EVK-MIMXRT685
Hardware requirements
  • Micro USB cable

  • EVK-MIMXRT685 board

  • Personal Computer

Board settings

I2C one board:

  • Transfer data from MASTER_BOARD to SLAVE_BOARD of I2C interface, I2C4 pins of MASTER_BOARD are connected with I2C4 pins of SLAVE_BOARD

MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name   Board Location     Pin Name   Board Location
P0_29       J27-2               P0_29      J27-2
P0_30       J27-1               P0_30      J27-1
GND         J28-7               GND        J28-7
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The following message shows in the terminal if the example runs successfully.

CMSIS I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .
FRDM-MCXW23
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW23 Board

  • Personal Computer

Board settings
MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name   Board Location     Pin Name   Board Location
I2C_SCL    J2-1               I2C_SCL    J2-1
I2C_SDA    J2-2               I2C_SDA    J2-2
GND        J2-4               GND        J2-4
Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board J10.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following message shows in the terminal if the example runs successfully.

CMSIS I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .
FRDM-RW612
Hardware requirements
  • Micro USB cable

  • FRDM-RW612 board

  • Personal Computer

Board settings

I2C one board:

  • Transfer data from MASTER_BOARD to SLAVE_BOARD of I2C interface, I2C2 pins of MASTER_BOARD are connected with I2C2 pins of SLAVE_BOARD

MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name   Board Location     Pin Name   Board Location
GPIO_16     J2-18              GPIO_16     J2-18
GPIO_17     J2-20              GPIO_17     J2-20
GND         J2-14              GND         J2-14
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J10) on the board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the example.

Running the demo

The following message shows in the terminal if the example runs successfully.

CMSIS I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .
LPCXpresso51U68
Hardware requirements
  • Micro USB cable

  • Two LPCXpresso51U68 boards

  • Personal Computer

Board settings

I2C one board:

  • Transfer data from MASTER_BOARD to SLAVE_BOARD of I2C interface, I2C4 pins of MASTER_BOARD are connected with I2C4 pins of SLAVE_BOARD

MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name   Board Location     Pin Name   Board Location
I2C_SCL    J1-1               I2C_SCL    J1-1
I2C_SDA    J1-3               I2C_SDA    J1-3
GND        J1-7               GND        J1-7
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the LPC-Link USB port (J6) on the board.

  2. Open a serial terminal on PC for JLink serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following message shows in the terminal if the example runs successfully.

CMSIS I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .
LPCXpresso54628
Hardware requirements
  • Micro USB cable

  • Two LPCXpresso54628 boards

  • Personal Computer

Board settings

I2C one board:

  • Transfer data from MASTER_BOARD to SLAVE_BOARD of I2C interface, I2C8 pins of MASTER_BOARD are connected with I2C8 pins of SLAVE_BOARD

MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name   Board Location     Pin Name   Board Location
I2C_SCL    J9-2               I2C_SCL    J9-2
I2C_SDA    J9-4               I2C_SDA    J9-4
GND        J9-7               GND        J9-7
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the LPC-Link USB port (J8) on the board.

  2. Open a serial terminal on PC for JLink serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following message shows in the terminal if the example runs successfully.

CMSIS I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .
LPCXpresso54S018
Hardware requirements
  • Micro USB cable

  • Two LPCXpresso54S018 boards

  • Personal Computer

Board settings

I2C one board:

  • Transfer data from MASTER_BOARD to SLAVE_BOARD of I2C interface, I2C8 pins of MASTER_BOARD are connected with I2C8 pins of SLAVE_BOARD

MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name   Board Location     Pin Name   Board Location
I2C_SCL    J9-2               I2C_SCL    J9-2
I2C_SDA    J9-4               I2C_SDA    J9-4
GND        J9-7               GND        J9-7
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the LPC-Link USB port (J8) on the board.

  2. Open a serial terminal on PC for JLink serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

This demo is an external flash plain load demo, ROM will copy image in external flash to SRAMX to run:

  1. Build the demo to generate a bin file. Note: If need to generate bin file using MCUXpresso IDE, below steps need to be followed: Set in example Properties->C/C++ Build->Settings->Build steps->Post-build steps->Edit enbable arm-none-eabi-objcopy -v -O binary “&{BuildArtifactFileName}” “&{BuildArtifactFileBaseName}.bin”

      This plainload example linked the vector table to 0x00000000, but program to external flash 0x10000000.
    
  2. Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):

    a. Open SEGGER J-FLASH Lite, select device LPC54S018.

    b. Click the ‘Erase Chip’ to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)

    c. Select the bin data file, set the ‘.bin/Erase Start’ address to 0x10000000, then click ‘Program Device’ Note: Please use above way to program the binary file built by armgcc tool chain to external flash. For IAR, KEIL, MCUXpresso IDE, you can use the IDE tool to program the external flash.
    The following message shows in the terminal if the example runs successfully.

CMSIS I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .
LPCXpresso54S018M
Hardware requirements
  • Micro USB cable

  • Two LPCXpresso54S018M boards

  • Personal Computer

Board settings

I2C one board:

  • Transfer data from MASTER_BOARD to SLAVE_BOARD of I2C interface, I2C8 pins of MASTER_BOARD are connected with I2C8 pins of SLAVE_BOARD

MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name   Board Location     Pin Name   Board Location
I2C_SCL    J9-2               I2C_SCL    J9-2
I2C_SDA    J9-4               I2C_SDA    J9-4
GND        J9-7               GND        J9-7
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the LPC-Link USB port (J8) on the board.

  2. Open a serial terminal on PC for JLink serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

This demo is an external flash plain load demo, ROM will copy image in external flash to SRAMX to run:

  1. Build the demo to generate a bin file. Note: If need to generate bin file using MCUXpresso IDE, below steps need to be followed: Set in example Properties->C/C++ Build->Settings->Build steps->Post-build steps->Edit enbable arm-none-eabi-objcopy -v -O binary “&{BuildArtifactFileName}” “&{BuildArtifactFileBaseName}.bin”

      This plainload example linked the vector table to 0x00000000, but program to external flash 0x10000000.
    
  2. Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):

    a. Open SEGGER J-FLASH Lite, select device LPC54S018M.

    b. Click the ‘Erase Chip’ to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)

    c. Select the bin data file, set the ‘.bin/Erase Start’ address to 0x10000000, then click ‘Program Device’ Note: Please use above way to program the binary file built by armgcc tool chain to external flash. For IAR, KEIL, MCUXpresso IDE, you can use the IDE tool to program the external flash.
    The following message shows in the terminal if the example runs successfully.

CMSIS I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .
LPCXpresso55S06
Hardware requirements
  • Micro USB cable

  • Two LPCXpresso55S06 boards

  • Personal Computer

Board settings
MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name   Board Location     Pin Name   Board Location
I2C_SCL    J9-2               I2C_SCL    J9-2
I2C_SDA    J9-4               I2C_SDA    J9-4
GND        J9-8               GND        J9-8   
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the LPC-Link USB port (J1) on the board.

  2. Open a serial terminal on PC for JLink serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following message shows in the terminal if the example runs successfully.

CMSIS I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .
LPCXpresso55S16
Hardware requirements
  • Micro USB cable

  • Two LPCXpresso55S16 boards

  • Personal Computer

Board settings
MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name   Board Location     Pin Name   Board Location
I2C_SCL    J9-2               I2C_SCL    J9-2
I2C_SDA    J9-4               I2C_SDA    J9-4
GND        J9-8               GND        J9-8   

The jumper setting: Default jumpers configuration does not work, you will need to add JP20 and JP21 (JP22 optional for ADC use)

Prepare the Demo
  1. Connect a micro USB cable between the PC host and the LPC-Link USB port (J1) on the board.

  2. Open a serial terminal on PC for JLink serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following message shows in the terminal if the example runs successfully.

CMSIS I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .
LPCXpresso55S28
Hardware requirements
  • Micro USB cable

  • Two LPCXpresso55S28 boards

  • Personal Computer

Board settings
MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name   Board Location     Pin Name   Board Location
I2C_SCL    P17-1              I2C_SCL    P17-1
I2C_SDA    P17-3              I2C_SDA    P17-3
GND        P17-7              GND        P17-7 
Prepare the Demo

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a micro USB cable between the PC host and the LPC-Link USB port (P6) on the board.

  2. Open a serial terminal on PC for JLink serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following message shows in the terminal if the example runs successfully.

CMSIS I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .
LPCXpresso55S36
Hardware requirements
  • Micro USB cable

  • Two LPCXpresso55S36 boards

  • Personal Computer

Board settings

Short JP52 1-2.

MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name   Board Location     Pin Name   Board Location
I2C_SCL    J122-12            I2C_SCL    J122-12
I2C_SDA    J122-6             I2C_SDA    J122-6
GND        J92-14             GND        J92-14  
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the LPC-Link USB port (J1) on the board.

  2. Open a serial terminal on PC for JLink serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following message shows in the terminal if the example runs successfully.

CMSIS I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .
LPCXpresso55S69
Hardware requirements
  • Micro USB cable

  • Two LPCXpresso55s69 boards

  • Personal Computer

Board settings
MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name   Board Location     Pin Name   Board Location
I2C_SCL    P17-1              I2C_SCL    P17-1
I2C_SDA    P17-3              I2C_SDA    P17-3
GND        P17-7              GND        P17-7 
Prepare the Demo

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a micro USB cable between the PC host and the LPC-Link USB port (P6) on the board.

  2. Open a serial terminal on PC for JLink serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following message shows in the terminal if the example runs successfully.

CMSIS I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .
MIMXRT685-AUD-EVK
Hardware requirements
  • Micro USB cable

  • MIMXRT685-AUD-EVK board

  • Personal Computer

Board settings

Make sure JP42 2-3 is connected.

I2C one board:

  • Transfer data from MASTER_BOARD to SLAVE_BOARD of I2C interface, I2C4 pins of MASTER_BOARD are connected with I2C4 pins of SLAVE_BOARD

MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name   Board Location     Pin Name   Board Location
P0_29       J27-2               P0_29      J27-2
P0_30       J27-1               P0_30      J27-1
GND         J28-7               GND        J28-7
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The following message shows in the terminal if the example runs successfully.

CMSIS I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .
RD-RW612-BGA
Hardware requirements
  • Micro USB cable

  • RD-RW612-BGA board

  • Personal Computer

Board settings

JP50 connected.

I2C one board:

  • Transfer data from MASTER_BOARD to SLAVE_BOARD of I2C interface, I2C2 pins of MASTER_BOARD are connected with I2C2 pins of SLAVE_BOARD

MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name   Board Location     Pin Name   Board Location
GPIO_16     HD1-14              GPIO_16     HD1-14
GPIO_17     HD1-13              GPIO_17     HD1-13
GND         HD1-11              GND         HD1-11
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the example.

Running the demo

The following message shows in the terminal if the example runs successfully.

CMSIS I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .
MCXW23-EVK
Hardware requirements
  • Mini/micro USB cable

  • MCXW23-EVK Board

  • Personal Computer

Board settings
MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name   Board Location     Pin Name   Board Location
I2C_SCL    J18-5              I2C_SCL    J18-5
I2C_SDA    J18-6              I2C_SDA    J18-6
GND        J18-8              GND        J18-8
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J33.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following message shows in the terminal if the example runs successfully.

CMSIS I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .