MCUXpresso SDK Documentation

cmsis_spi_dma_transfer

cmsis_spi_dma_transfer#

Overview#

CMSIS-Driver defines generic peripheral driver interfaces for middleware making it reusable across a wide range of supported microcontroller devices. The API connects microcontroller peripherals with middleware that implements for example communication stacks, file systems, or graphic user interfaces. More information and usage method please refer to http://www.keil.com/pack/doc/cmsis/Driver/html/index.html.

The cmsis_spi_dma_transfer example shows how to use CMSIS SPI driver in dma way: In this example , one spi instance used as master and another spi instance used as slave in the same board. SPI master send/received data to/from SPI slave in dma . (SPI Slave using dma to receive/send the data)

Running the demo#

When the example runs successfully, you can see the similar information from the terminal as below. SPI CMSIS DMA transfer example start. This example use one spi instance as master and another as slave on one board. Master use DMA way , slave uses interrupt. Please make sure you make the correct line connection. Basically, the connection is: SPI_master – SPI_slave
CLK – CLK
PCS – PCS
MISO – MISO
MOSI – MOSI This is SlaveSignalEvent. This is MasterSignalEvent.

SPI transfer all data matched!