Hardware requirements#
Micro USB cable
MIMXRT685-AUD-EVK board
Adafruit TFT LCD shield w/Cap Touch V2.3
Personal Computer
Board settings#
There are different versions of Adafruit 2.8” TFT LCD shields. The shields marked v2.0 works directly with this project. For the other shields, please solder the center pin of IOREF pads to the 3.3V pad, and solder the pads 11, 12, and 13. See the link for details: https://community.nxp.com/t5/MCUXpresso-Community-Articles/Modifying-the-latest-Adafruit-2-8-quot-LCD-for-SDK-graphics/ba-p/1131104
Attach the LCD shield to the LPC board. Ensure VDDIO_1 is 3.3V (JP12 2-3 connected) and JP41 2-3 connected.
Prepare the Demo#
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo#
The GUI will be shown on the LCD.