MCUXpresso SDK Documentation

Hardware requirements#

  • Type-C USB cable

  • FRDM-MCXN947 board

  • 3.5” TFT LCD module by NXP (P/N PAR-LCD-S035) Rev.A

  • Personal Computer

Board settings#

Attach the LCD shield to the FRDM board.

Prepare the Demo#

  1. Power the board using a type-c USB cable connected to J2 USB port on the board, attach debugger to J5 connector

  2. Build the project.

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo#

If this example runs correctly, the sample GUI is displayed.