Hardware requirements#
Type-C USB cable
FRDM-MCXN236 board
Personal Computer
3.5” TFT LCD module by NXP (P/N PAR-LCD-S035) Rev.A
Board settings#
Attach the LCD shield to the FRDM board.
Prepare the Demo#
Connect a micro USB cable between the PC host and the MCU-Link USB port (J10) on the board
Build the project.
Download the program to the target board.
Reset the SoC and run the project.
Running the demo#
If this example runs correctly, the sample GUI is displayed.