Hardware requirements#
Type-C USB cable
FRDM-IMXRT700 board
Personal computer
Board settings#
Example running at 325MHz which need PMIC power supply.
PMIC is required to drive 1.1V on VDD2, then JP1 and JP3 on the FRDM-IMXRT700 need to be shorted for proper operation Prepare the Demo ================
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.