Hardware requirements#
Micro USB cable
MIMX8ULP-EVK/EVK9 board
J-Link Debug Probe
5V power supply
RK055AHD091 panel or RK055MHD091 panel
Board settings#
Connect the MIPI panel to MIMX8ULP-EVK board J18.
Prepare the Demo#
Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.
Connect a micro USB cable between the host PC and the J17 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Build the project, this project uses RK055MHD091 panel by default, to use the RK055AHD091 panel, change #define USE_MIPI_PANEL MIPI_PANEL_RK055MHD091 to #define USE_MIPI_PANEL MIPI_PANEL_RK055AHD091 in lcdif_support.h.
Generate flash.bin with imx-mkimage and download it according to Getting Started doc
Open two serials lines provided at J17 USB port. (e.g. /dev/ttyUSB0~3, /dev/ttyUSB2 for A Core, /dev/ttyUSB3 for M Core)
Boot to uboot and let uboot not using diplay => setenv video_off yes;saveenv then re-power on the board
Let Stop in Uboot
Running the demo#
When the example runs, the screen shows what described in overview.