Dependency Patterns#
Here are frequently used dependency patterns.
Pattern1: start with
allOf, with one levelanyOfandnotcomponentA: allOf: - component1 - component2 - anyOf: - component3 - component4 - anyOf: - component5 - component6 - not: device: - MK64F12 - MK63F12
The recommended dependency patterns for this.
config MCUX_COMPONENT_componentA bool "Component A, pattern 1" select MCUX_COMPONENT_component1 select MCUX_COMPONENT_component2 depends on !MCUX_HW_DEVICE_MK64F12 && !MCUX_HW_DEVICE_MK63F12 # not choice prompt "Component A anyOf1" default MCUX_DEPENDENCY_COMPONENT_componentA_DEPEND_ANYOF_1 config MCUX_DEPENDENCY_COMPONENT_componentA_DEPEND_ANYOF_1 bool "Select component3" select MCUX_COMPONENT_component3 config MCUX_DEPENDENCY_COMPONENT_componentA_DEPEND_ANYOF_2 bool "Select component4" select MCUX_COMPONENT_component4 endchoice choice prompt "Component A anyOf2" default MCUX_DEPENDENCY_COMPONENT_componentA_DEPEND_ANYOF_3 config MCUX_DEPENDENCY_COMPONENT_componentA_DEPEND_ANYOF_3 bool "Select component5" select MCUX_COMPONENT_component5 config MCUX_DEPENDENCY_COMPONENT_componentA_DEPEND_ANYOF_4 bool "Select component6" select MCUX_COMPONENT_component6 endchoice
Pattern 2: start with
allOf, with 2 levelanyOf/allOfcomponentB: dependency: allOf: - component1 - component2 - compiler: - iar - mdk - anyOf: - allOf: - component3 - component4 - device: - MK64F12 - MK63F12 - allOf: - component5 - component6 - device: - LPC54005 - LPC54016
The Kconfig dependency pattern is like
config MCUX_COMPONENT_componentB bool "Component B, pattern 2 choise" select MCUX_COMPONENT_component1 select MCUX_COMPONENT_component2 depends on MCUX_COMPILER_IAR || MCUX_COMPILER_MDK # All device scope shall be explicitly specified here, otherwise for a device which is not in the scope which means the dependency is not satisfied, but componentC is still showed and configurable depends on MCUX_HW_DEVICE_MK64F12 || MCUX_HW_DEVICE_MK63F12 || MCUX_HW_DEVICE_LPC54005 || MCUX_HW_DEVICE_LPC54016 if MCUX_COMPONENT_componentB choice prompt "ComponentB anyOf" default MCUX_DEPENDENCY_COMPONENT_componentC_DEPEND_ALLOF_1 config MCUX_DEPENDENCY_COMPONENT_componentC_DEPEND_ALLOF_1 bool "Select component3 and component 4 in device MK64F12, MK63F12" select MCUX_COMPONENT_component3 select MCUX_COMPONENT_component4 depends on MCUX_HW_DEVICE_MK64F12 || MCUX_HW_DEVICE_MK63F12 config MCUX_DEPENDENCY_COMPONENT_componentC_DEPEND_ALLOF_2 bool "Select component5 and component4" select MCUX_COMPONENT_component5 select MCUX_COMPONENT_component6 depends on MCUX_HW_DEVICE_LPC54005 || MCUX_HW_DEVICE_LPC54016 endchoice endif
If under each
allOf, there is only one component, then you can useselectcomponentB: dependency: allOf: - component1 - component2 - compiler: - iar - mdk - anyOf: - allOf: - component3 - device: - MK64F12 - MK63F12 - allOf: - component5 - device: - LPC54005 - LPC54016
config MCUX_COMPONENT_componentB bool "Component B, pattern 2 select" select MCUX_COMPONENT_component1 select MCUX_COMPONENT_component2 depends on MCUX_COMPILER_IAR || MCUX_COMPILER_MDK # All device scope shall be explicitly specified here, otherwise for a device which is not in the scope which means the dependency is not satisfied, but componentC is still showed and configurable depends on MCUX_HW_DEVICE_MK64F12 || MCUX_HW_DEVICE_MK63F12 || MCUX_HW_DEVICE_LPC54005 || MCUX_HW_DEVICE_LPC54016 select MCUX_COMPONENT_component3 if MCUX_HW_DEVICE_MK64F12 || MCUX_HW_DEVICE_MK63F12 select MCUX_COMPONENT_component5 if MCUX_HW_DEVICE_LPC54005 || MCUX_HW_DEVICE_LPC54016
Pattern 3: start with
anyOf, with one levelallOfcomponentE: dependency: anyOf: - allOf: - component1 - component2 - core: - cm4 - cm4f - device: - MK64F12 - MK63F12 - allOf: - component3 - component4
The Kconfig dependency pattern is like
config MCUX_COMPONENT_componentC bool "Component C, pattern 3" if MCUX_COMPONENT_componentC choice prompt "Component C anyOf" default MCUX_DEPENDENCY_COMPONENT_componentC_DEPEND_ALLOF_component1_component2 config MCUX_DEPENDENCY_COMPONENT_componentC_DEPEND_ALLOF_component1_component2 bool "Select component1 and component2" select MCUX_COMPONENT_component1 select MCUX_COMPONENT_component2 depends on MCUX_HW_CORE_CM4 || MCUX_HW_CORE_CM4F depends on MCUX_HW_DEVICE_MK64F12 || MCUX_HW_DEVICE_MK63F12 config MCUX_DEPENDENCY_COMPONENT_componentC_DEPEND_ALLOF_component3_component4 bool "Select component3 and component4" select MCUX_COMPONENT_component3 select MCUX_COMPONENT_component4 endchoice endif