MCUXpresso SDK Documentation

Toolchain introduction

Toolchain introduction#

The MCUXpresso SDK release for i.MX 93W includes the build system to be used with some toolchains. In this chapter, the toolchain support is presented and detailed.

Compiler/Debugger#

The MCUXpresso SDK i.MX 93W release supports building and debugging with the toolchains listed in Table 1.

The user can choose the appropriate one for development.

  • Arm GCC + SEGGER J-Link GDB Server. This is a command line tool option and it supports both Windows OS and Linux OS.

  • IAR Embedded Workbench for Arm and SEGGER J-Link software. The IAR Embedded Workbench is an IDE integrated with editor, compiler, debugger, and other components. The SEGGER J-Link software provides the driver for the J-Link Plus debugger probe and supports the device to attach, debug, and download.

Compiler/Debugger

Supported host OS

Debug probe

Tool website

ArmGCC/J-Link GDB server

Windows OS/Linux OS

J-Link Plus

developer.arm.com/open-source/gnu-toolchain/gnu-rm

www.segger.com

|IAR/J-Link|Windows OS|J-Link Plus|www.iar.com

www.segger.com

Download the corresponding tools for the specific host OS from the website.

Note:

  • To support i.MX 93W, the patch for IAR and Segger J-Link should be installed. (Download link: https://mcuxpresso.nxp.com/download/047466f7e217df2be088da727ac57b8b). For additional information about patch installation, see the readme.txt in the patch.

Parent topic:Toolchain introduction