MCUXpresso SDK Documentation

Run a demo application#

This section describes the steps to download the flash.bin to sd and emmc, run the example applications provided in the MCUXpresso SDK. The hello_world demo application targeted for the i.MX 95 hardware platform is used as an example, although these steps can be applied to any example application in the MCUXpresso SDK.

Connect LPUART on board to console on PC#

To download and run the application, perform these steps:

  1. Connect the development platform to your PC via USB cable between the DBG USB connector (J31) and the PC. It provides console output.

  2. Open the terminal application on the PC, such as PuTTY or TeraTerm, and connect to the debug COM port (to determine the COM port number, see How to determine COM port). Configure the terminal with these settings:

    1. 115200 baud rate

    2. No parity

    3. 8 data bits

    4. 1 stop bit

Parent topic:Run a demo application

Make a flash.bin#

  1. Get the boot images and the imx-mkimage source repository from corresponding Linux BSP release. The boot images required to be put into imx-mkimage/i.MX95 are:

    - oei-m33-tcm.bin

    - oei-m33-ddr.bin

    - m33_image.bin (m33_image-mx95alt.bin/m33_image-mx95evk.bin/m33_image-mx95netc. bin)

    - lpddr5_dmem_qb_v202311.bin (lpddr4x_dmem_qb_v202311.bin for FRDM-IMX95)

    - lpddr5_dmem_v202311.bin (lpddr4x_dmem_v202311.bin for FRDM-IMX95)

    - lpddr5_imem_qb_v202311.bin (lpddr4x_imem_qb_v202311.bin for FRDM-IMX95)

    - lpddr5_imem_v202311.bin (lpddr4x_imem_v202311.bin for FRDM-IMX95)

    - u-boot.bin

    - u-boot-spl.bin

    - bl31.bin

    - tee.bin

    - mx95b0-ahab-container.img

    Note:

    • mx95evk for m33_image.bin is used for rpmsg str echo, rpmsg ping pong and power_mode_switch_rtos.

    • mx95netc for m33_image.bin is used for netc_share.

    • mx95alt for m33_image.bin is used for almost other examples.

  2. Copy binary built by ARMGCC/IAR into imx-mkimage/i.MX95, and rename it to m7_image.bin.

  3. make image for ram target.

    1. Make flash.bin with imx-mkimage.

      make SOC=iMX95 OEI=YES flash_all LPDDR_TYPE=lpddr5 (boot A core and M7)

      or

      make SOC=iMX95 OEI=YES flash_lpboot_sm_m7 LPDDR_TYPE=lpddr5 (does not boot A core, just boot M7)

    2. Make image for ddr target:

      make SOC=iMX95 OEI=YES flash_m7_ddr LPDDR_TYPE=lpddr5

      make SOC=iMX95 OEI=YES flash_lpboot_sm_m7 LPDDR_TYPE=lpddr5

    Note: For FRDM-IMX95, LPDDR_TYPE=lpddr4x.

  4. Burn flash.bin to MicroSD/eMMC at 32 K(0x8000) offset with dd or HxD or UUU and then plug the MicroSD card to the board.

    For example:

    • Burn flash.bin to Micro SD card with dd

      dd if=flash.bin of=/dev/sdh bs=1k seek=32 && sync

    • Burn flash.bin to SD/eMMC with UUU

      1. Connect USB Type-C port to PC through the USB cable. It is used for downloading firmware of the board.

      2. Switch to serial downloader mode; boot core is cortex-m33. sd: uuu -b sd imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all new-flash.bin

      3. Burn flash.bin with uuu.

        emmc: uuu -b emmc imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all new-flash.bin

      Note:

      • imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all (imx-boot-imx95-15x15-lpddr4x-frdm-sd.bin-flash_all for FRDM-IMX95). Get it from linux bsp.

      • new-flash.bin. Generate it yourself.

  5. Change the boot mode to SW7[1:4] = 1011 for sd boot, SW7[1:4] = 1010 for emmc boot. Note: For FRDM-IMX95, SW1[1:2] = 11 for sd boot. SW7[1:2] = 10 for emmc boot

  6. Power on the board .

Parent topic:Run a demo application

Debug an demo application with IAR#

To debug an application with IAR, perform these steps:

  1. download the patch for IAR and Segger J-Link from the NXP website, install it as readme in the patch.

  2. burn a flash.bin to board, see Run a demo application, make sure the size of M7 binary in flash.bin not less than the binary you want to debug.

  3. power on the board, make sure the M7 is booted by SM

  4. Open hello world example with IAR, click download and debug to debug

  5. click button such as step over to debug

Parent topic:Run a demo application