Host setup#
An MCUXpresso SDK build requires that some packages are installed on the Host. Depending on the used Host operating system, install the following tools.
Linux:
Cmake
$ sudo apt-get install cmake $ # Check the version >= 3.0.x $ cmake –-version
Windows:
MinGW
The Minimalist GNU for Windows OS (MinGW) development tools provide a set of tools that are not dependent on third party C-Runtime DLLs (such as Cygwin). The build environment used by the SDK does not utilize the MinGW build tools, but does leverage the base install of both MinGW and MSYS. MSYS provides a basic shell with a Unix-like interface and tools.
Download the latest MinGW mingw-get-setup installer from sourceforge.net/projects/mingw/files/Installer/.
Run the installer. The recommended installation path is
C:\MinGW. However, you may install to any location.Note: The installation path cannot contain any spaces.
Ensure that mingw32-base and msys-base are selected under Basic Setup.

Click Apply Changes in the Installation menu and follow the remaining instructions to complete the installation.

Add the appropriate item to the Windows operating system path environment variable. It can be found under Control Panel->System and Security->System->Advanced System Settings in the Environment Variables… section. The path is:
<mingw_install_dir>\bin.Assuming the default installation path,
C:\MinGW, an example is as shown in Figure 3. If the path is not set correctly, the toolchain does not work.Note: If you have
C:\MinGW\msys\x.x\binin your PATH variable (as required by KSDK 1.0.0), remove it to ensure that the new GCC build system works correctly.
Cmake
Download CMake 3.0.x from www.cmake.org/cmake/resources/software.html.
Install CMake, ensuring that the option Add CMake to system PATH is selected when installing. The user chooses to select whether it is installed into the PATH for all users or just the current user. In this example, it is installed for all users.

Follow the remaining instructions of the installer.
Reboot your system to ensure that the PATH variable is updated.