MCUXpresso SDK Documentation

Install RT700 DSP Build Configuration

Install RT700 DSP Build Configuration#

Build Configuration’ is a term that describes all parameters and necessary build includes for the Tensilica processor implementation for development. It is mandatory to install a specific build configuration before starting development on RT700.

The build configuration is provided by NXP as a binary file and is imported into the Xplorer IDE. The binary file for the OS is available at the Tensilica URL: https://tensilicatools.com/download/rt700-download-page/.

|

|

The build configuration is installed into the IDE using the System Overview panel available in the lower left corner, by default. If the System Overview panel is not visible, toggle using the Window > Show View > System Overview menu item.

|

|

Click OK for build download to install.

|

|

Parent topic:Install Xplorer Toolchains