Logo
25.09.00
MCUXpresso SDK Project v: latest
Document Release Versions
25.09.00-pvw2
25.09.00-pvw1
25.06.00
25.06.00-pvw2
25.06.00-pvw1
latest

Introduction

  • MCUXPresso SDK

Getting Started

  • Github Repository
  • Zip Package

User Guide

  • Drivers
  • Examples
  • Middleware
  • RTOS
  • Boards

Development

  • Build And Configuration System
  • Developing with MCUXpresso SDK

Releases

  • Release Notes
mcuxsdk
  • Docs »
  • Program LPC-Link2 with SEGGER J-Link
  • Open on Repo Report an issue

Program LPC-Link2 with SEGGER J-Link

In addition to standalone probes, the onboard LPC-Link2 debug probe is used to debug HiFi4 DSP over SWD ports. The RT600 EVK has an LPC4300 MCU (top right corner on EVK) and by default has been pre-programmed as CMSIS-DAP probe. CMSIS-DAP is not compatible with HiFi4. Therefore, a few extra steps are required to flash it with J-Link firmware and support both Arm CM33 core and HiFi4 DSP core.

The steps are:

  1. Install LPCScrypt, a command-line tool for programming onboard LPC-Link2 debug probe with the latest CMSIS-DAP and J-Link firmware. LPCScrypt is available for download from:https://www.nxp.com/design/microcontrollers-developer-resources/lpc-microcontroller-utilities/lpcscrypt-v2.1.0:LPCSCRYPT.

  2. After the download is complete, run the installer.

    Note: During the installation, the DFU, and VCOM drivers are automatically installed for all platforms.

  3. To update the LPC-Link2 debug circuit firmware, unplug the USB cable on J5 and then connect to the DFULink jumper. In the MIMXRT685-EVK, JP1 is the LPCXpresso DFU jumper as shown in Figure 1.

  4. Connect JP1 using the jumper.

    |

|

  1. Reconnect the board to the host computer over the debug link USB connector J5.

  2. Launch LPCScrypt by double-clicking the Boot LPCScrypt file in the LPCScrypt install location: C:\ProgramData\Microsoft\Windows\Start Menu\Programs\LPCScrypt.

    |

|

  1. In that command shell, run the program_JLINK script to install the JLink debug firmware.

    |

|

**Note:** File paths in this document use the Windows directory separator, on Linux or Mac OSX. The file paths must be replaced with ‘/.’ For Windows users, shortcuts to the scripts are available from the LPCScrypt entry on the Start menu.
  1. Verify once you select the firmware (in this case J-Link), LPCScrypt. The console appears as shown in Figure 4.

    |

|

  1. Open/ Disconnect JP1 and power cycle the board. The onboard LPC-Link2 is ready to be used as SEGGER J-Link probe.

    Every EVK/ LPC-Link2 has a different J-Link S/N. Therefore, make sure to write down the S/N for xt-ocd and topology.xml as indicated in Install Xtensa On Chip Debugger Daemon.

    |

|

  1. Another benefit is that LPC-Link2 debug probe creates a virtual serial port over USB, so the extra UART2USB cable for debugging is not required.

    |

|

The download link provides the document, demo videos and details on LPC-Link2. If you have any questions, or have difficulties to program the probe, see [https://www.nxp.com/design/microcontrollers-developer-resources/lpc-microcontroller-utilities/lpcscrypt-v2.1.0:LPCSCRYPT](https://www.nxp.com/design/microcontrollers-developer-resources/lpc-microcontroller-utilities/lpcscrypt-v2.1.0:LPCSCRYPT).

Parent topic:Install Xplorer Toolchains


Copyright 2025, NXP. Last generated on Sep 19, 2025 12:55+0200; branch release/25.09.00, revision 464f40b81f246522a152bbaeafd2821c65adbc1a.