Enable MCUXpresso SDK DSP#
The following DSP-specific enablements are available inside the MCUXpresso SDK release package for RT600.
<SDK_ROOT>/devices/MIMXRT685S/
Unified device and peripheral driver source code that can be compiled for both Arm and DSP cores.
**Note:** Only a limited subset of peripheral drivers and components is supported on the DSP.
- ```
<SDK_ROOT>/boards/evkmimxrt685/dsp_examples/
DSP example applications
<SDK_ROOT>/middleware/multicore/rpmsg_lite/
Unified RPMsg-Lite multicore communication library, with porting layers for Arm and DSP cores
- ```
<SDK_ROOT>/middleware/dsp/audio_framework/
Xtensa Audio Framework \(XAF\) for DSP core
<SDK_ROOT>/middleware/dsp/audio_framework/libxa_af_hostless/
Source code and documentation for the core XAF framework
- ```
<SDK_ROOT>/middleware/dsp/audio_framework/testxa_af_hostless/
Utilities and tests for developing applications with the XAF framework
<SDK_ROOT>/middleware/dsp/audio_framework/testxa_af_hostless/test/plugins
XAF components and codec binaries
<SDK_ROOT>/middleware/dsp/naturedsp/hifi4/
NatureDSP Math Library for HiFi4 DSP
**Parent topic:**[Install MCUXpresso SDK](../topics/install_mcuxpresso_sdk.md)