Bluetooth Low Energy Demo Applications User Guide#
Table of Contents
- Introduction
- Bluetooth Low Energy applications
- Hardware configurations
- Building and running a Bluetooth LE example application
- Bluetooth LE stack and demo applications
- ANCS/AMS client (ancs_c)
- Beacon
- Bluetooth LE FSCI Black Box
- EATT Central
- EATT Peripheral
- FSCI Bridge
- HCI Black Box
- HID Device (Mouse)
- HID Host
- Localization Reader
- Localization Reader Host
- Localization User Device
- Low-power temperature sensor and collector
- Tire Pressure Monitoring System Sensor and Monitor
- Low-power extended advertising Peripheral and Central
- NCP FSCI Black Box
- NCP Localization Reader
- Over the Air Programming (OTAP)
- Wireless UART
- Bluetooth LE Shell
- Implemented stack features
- Implemented profile and services
- Supported platforms
- User interface
- Usage
- Throughput feature
- Decision-Based Advertising Filtering (DBAF) feature
- Periodic Advertising with Responses (PAwR) feature
- Monitoring Advertisers (MonAdv) feature
- Connection Subrating feature
- LE Power Control feature
- Hybrid (Dual-mode) Bluetooth Low Energy and Generic FSK
- Wireless UART Host
- References
- Acronyms
- Note about the source code in the document