Config Tools for i.MX Applications Processors 26.09 documentation

System Manager Configuration Tool#

The System Manager Configuration tool allows you to configure a project with the System Manager (SM) application on i.MX 9 series processors.

System Manager is a low-level system function that runs on a System Control Processor (SCP) and supports isolation and management of power domains, clocks, resets, sensors, and pins on complex application processors. It typically executes on Cortex-M processor architectures and delivers a comprehensive abstraction layer for the underlying hardware functionality. The primary purpose of SM is to allow isolation between software running on different cores in the SoC. SM maintains exclusive access to critical resources—such as power, clocks, reset, and PMIC—while providing an RPC interface to those clients (agents), enabling access control, arbitration, and aggregation policies for shared critical resources.

_images/system_manager_tool.png

System Manager tool#

SM configuration#

Configuration of SM determines how the device (SoC) will be divided between Logical Machines (LM) and specifies the ownership of peripherals and memory. This ownership is used to determine API access rights to resources (clocks, pins, and so on) and CPU access rights to peripherals and memory (for example, RDC configuration). SM determines which LM will boot at POR and what RPC API functions the agents on those LM can call.

NXP provides the SM along with example board configurations. The configuration specifies the associated device and board (in most cases, a new configuration must be created for a customer product).

SM project settings and files description#

The SM tool loads and processes data from a specified location of an SM Firmware project (for example, nxp-imx/imx-sm) by using the Project Settings wizard available in the System Manager toolbar.

_images/system_manager_toolbar_project_settings_wizard_and_import_export_options.png

System Manager toolbar - Project Settings wizard and Import/Export options#

Create an empty configuration based on the available board and device configuration (this option is suitable for developers of new or unsupported boards) or import an existing SM project configuration from CFG (for example, mx95evk.cfg from an SM FW repository) or a JSON file. Problems that occur during the configuration import are displayed in the report dialog that can be exported. In case of any issues, review the report and adjust the configuration accordingly.

_images/problems_reporting_during_import.png

Problems reporting during import#

The SM tool generates SM configuration source files that can be exported to the project location. The tool generates source files of the following types:

  • Doxygen DOX file (config.dox)

  • MAK file (config.mak)

  • Configuration header files (for example, config_scmi.h, config_trdc_h)

Apart from that, the SM tool can convert CFG files to the JSON format in the form of Resource Database JSON files and a user configuration JSON file. These files can be exported by using the export dialog.

  • atomic_resources.json contains available device and board specific atomic resources that can be configured by SM FW for a selected chip (pins, clocks, power domains, security peripheral regions, controls, faults).

  • macro_resources.json contains predefined macro resources defined by SM FW. A macro resource defines a group of atomic resources that describe a larger logical cluster of HW resources. For example, macro resource LPUART1 can specify a power domain, clock, or memory block checker—a peripheral instance that can be assigned to any of the Resource Owners specified by HW and SM FW: Domain (DOM), Logical Machine (LM), or Agent.

  • chip_data.json contains chip-specific information needed for SM FW configuration, such as security peripheral description.

  • error_log.json contains configuration problems that occur during input files parsing or output generation.

  • user_configuration.json contains the current SM project configuration state.

_images/generated_user_configuration_json_file.png

Generated user_configuration.json file#

User interface overview#

The SM tool consists of several views available to configure the SM project and to generate expected SM FW source files.

System view#

The System view shows an overview of configurable elements and their important details of the System Manager project in the form of a project navigation tree. The System view allows you to configure Resource Owner specific settings, such as RPC protocol, Transport, Mailbox, and Assignment Templates (definition of a group of parameters that will be assigned to a Resource Owner). These are the main categories that can be configured.

  • Project Configuration – SM project configuration name and description, compiler Mak file configuration

  • Board Configuration – Board specific settings, SM debug options, Global Assignment Templates definition, creation of custom User Macro Resources

  • Logical Machines – LM specific settings (for example, RPC), Mode Select Configurations from the LM perspective, Start-Stop Sequences configuration, Assignment Templates definition

    • Agents – SCMI Agent specific settings (for example, Mailbox), Assignment Templates definition

      • RPC Channels – Channel settings (for example, transport)

  • Domains – DOM specific settings, Assignment Templates definition

  • mSel Configurations Overview - Mode Select Configurations from the mSel perspective

To configure a generic System Manager project setting, for example, Project Mak file or debug features, use the System view tree to select the desired node. Every selection of the tree node shows available configuration settings in the configuration Details view. To expand/collapse all child nodes of the active selection, use the Expand/Collapse buttons on the System view header.

_images/system_view.png

System View#

Details view configuration#

The Details view displays SM element settings and allows you to change them.

The information is dynamically updated to reflect modifications in the System, Boot, or Resources views.

In the Details view, the following actions can be performed:

  • To display the element information, point the mouse cursor at the SM element.

  • Inspect the SM element in the System, Boot, or Resources views.

  • Modify the SM element settings by left-clicking the element value. There are the following types of settings:

    • Textbox – Left-click and type the value.

    • Dropdown – Left-click and select one of the offered values.

    • Checkbox – Left-click to set (enable) the element.

    • Button - Left-click to trigger an action or move to a specific configuration section.

    • Information – This setting type cannot be modified and is used to inform about a specified value.

  • Add an element to the table by left-clicking the plus button.

  • Remove an element from the table by left-clicking the cross button.

  • Navigate to the parent setting via the Navigation bar on the top of the Details view.

_images/configuration_details_view_of_the_selected_agent.png

Configuration details view of the selected agent#

Resources view#

The Resources view shows an overview of resources assigned to Resource Owners and is used as a way of navigation to show the details of the selected resource assignment. The assignment is usually set by the Assignment Template that represents assigned parameters to the resource. After an Assignment Template is set to a resource, it is possible to configure additional available parameters related to the resource in the Configuration Details view.

The top of the Resources view contains various filters that can be used to specify the overview intention. Filter Resource Owners using specified filters and Resources using the search bar or specified filters.

Access control takes two forms, API access via an agent’s MU and RDC access for a DID. Each LM is a unique DID and can have multiple agents, which all have the same DID.

To assign a resource to a Resource Owner (LM, SCMI_AGENT, DOM) use the Resources view.

  • Assign and configure Resource parameters - Select the cell with the corresponding Resource (row) and the Resource Owner (column) in the Resources view. Click the Assign button in the configuration Details view.

  • Assign a resource with pre-configured Assignment Templates - Using the System and Details views configure the Assignment Templates for the desired Resource owner - Set the name (identifier) and Resource parameters to be configured (parameters that do not relate to the assigning Resource are ignored).

  • Assign a resource with pre-configured mandatory (required) Assignment Templates DFMT0 and DFMT1 - Resources that configure Atomic Resource of the type MDAC require mandatory Assignment Templates DFMT0 for CPU and DFMT1 for non-CPU bus-masters to apply. The required templates are assigned automatically.

_images/selection_of_resource_assignment_in_the_resources_view.png

Selection of Resource Assignment in the Resources view#

  • Create a new memory sector - Select the corresponding Resource (row) with the <MEM> suffix and the Resource Owner (column) in the Resources View. Double-click the desired cell and select Create a new memory sector. Then configure the memory sector parameters (Start Address, Size or End Address, and Permissions) in the Details View.

  • Assign an existing memory sector to a Resource owner - Expand the Resource (row) with the <MEM> suffix node, select the memory sector, and double-click the cell to select the template or assign the memory sector.

_images/example_of_memory_resource_assignment_m7mix_0x20380000_0x2047ffff_to_ele_domain.png

Example of Memory resource assignment - M7MIX<0x20380000-0x2047ffff> to ELE Domain#

  • To modify parameters of the resource assignment, select the resource and use the Details view:

    • Use the Template Assignment section to select and see configured parameters assigned by the Assignment Template. Modify the Assignment Template parameters by selecting the checkbox to enable editing.

      Note: Updating the selected Assignment Template affects all Resources that are assigned to this template.

    • To configure additional parameters to the selected Assignment template, select the settings below the Assignment Template selection.

      Note: The parameters that are not available are not related to the Resource. The parameters that are grayed are configured by the Assignment Template and cannot be overwritten. To change a grayed setting value, create a new Assignment Template, choose another, or update the selected one.

  • To remove the Resource assignment, select the cell with the corresponding Resource (row) and the Resource Owner (column) in the Resources view. Then click the Unassign button in the configuration Details view.

  • To find a desired Resource or to adjust the overview table, use the Filter or the search bar. Combine the selection of Resources and Owners filters with the search bar filtering. The search bar supports case-sensitive and regular expression search. Enable it by clicking the buttons on the right side of the search bar.

    Note: Macro Resources can be expanded in the Resources view to see all Atomic Resources that are included in the resource assignment.

_images/filtering_a_resource.png

Filtering a resource#

Boot view#

The Boot view shows an overview of an independent lifecycle execution of LMs and configuration of boot Mode Select (mSel) options. The following options can be configured:

  • Add or remove a new mSel mode from the System Manager configuration by clicking the Add/Remove buttons in the header of the Boot view.

  • In the Boot view, the mSel table lists logical machines in the boot order. If a machine’s boot is disabled, it stays in its position but its index changes to 0 and the remaining machines are renumbered accordingly. To reorder items, select one and click the Up or Down button.

  • In the Details view of the selected Logical Machine, the Relative time to the time the SM starts to boot Logical machines can be configured.

  • In the Boot view, each LM can have multiple boot configurations with different start and stop sequences. It can be determined if the LM is booted when the SM boots in every mSel section.

    • Configuration of the “bootskip” flag skips an error due to no image in the boot container.

    • Select the Start and Stop commands to execute when an LM is booted or shut down (sequences).

      • To add, remove, or modify a Start-Stop Sequence, select the LM to be affected from the desired mSel section and use the Details view.

      • Use plus/minus buttons to add or remove a Start-Stop Sequence

      • Double-click the Start-Stop Sequence to open its configuration details to be modified

        • Modify the index (identifier) and user name of the Start-Stop Sequence

        • Use plus/minus buttons to add or remove Resource Commands to be called in the sequence.

        • Double-click the Resource Command to open its configuration details to be modified (selection of Resource Command, optional arguments, and unit test flag)

_images/boot_view.png

Boot view#

Code generation#

If the settings are correct and no error is reported, the code generation engine instantly regenerates the source code. The resulting code appears in the Code preview view of the System Manager tool.

Code preview automatically highlights differences between the current and immediately preceding iteration of the code. It is possible to choose between two modes of highlighting by clicking the Set viewing style for source differences. Highlighting can be disabled from the same dropdown menu. Such features as Copy, Search, Zoom-in, Zoom-out, and Export source are available in the Code Preview view. The search can also be invoked by CTRL+F or from the context menu.

_images/highlighted_change_of_the_code.png

Highlighted change of the code#

Use cases workflow#

This section describes how to configure specific System Manager parts or functions. The typical use case of the tool starts with importing the existing configuration. Creating an empty configuration suits the development of a new board or processor not yet supported by the official System Manager Firmware release.

  1. After selecting a supported processor, import an existing configuration of the SM project in CFG format using the Project settings wizard.

  2. To configure a generic System Manager project setting, for example Project Mak file or debug features, use the tree in the System view to select the desired element. Every selection of the tree element shows you available configuration settings in the Configuration Details view.

  3. To configure a setting related to booting of the Logical Machines, use the Boot view.

    1. To add or remove the mSel configuration, use the plus/minus buttons in the left pane of the Boot view.

    2. In the desired mSel section configure parameters for each Logical Machine:

      1. Select LM and use Details view to configure Boot related parameters and add or modify Start/Stop sequences of Resource Command calls.

      2. Enable the Boot parameter so that the index of the Logical Machine corresponds to the actual boot order (index 0 means the LM does not boot).

      3. Enable the optional “Skip” parameter to skip the booting error message and select the Start and Stop sequences.

  4. Use the Resources view to assign a Resource to a Resource Owner (every Resource Owner is related to a specific TRDC domain).

    1. To find a desired Resource or to adjust the overview table, use the Filter or Search bar.

    2. To add a new assignment, double-click on the desired Macro or the Atomic resource (row) related to the Owner (column) and assign a resource or a template.

    3. To remove an existing assignment, select the assignment and click the Unassign button in the Details view.

    4. To modify an assignment, click the resource and use Details view.

  5. To adjust the overview of the Resource assignments, use the filter or search bar in the Resources view.