Config Tools for i.MX Applications Processors 26.09 documentation

Installing and configuring the System Manager Configuration tool

Installing and configuring the System Manager Configuration tool#

The System Manager Configuration tool is a part of the Config Tools for i.MX. This software is available as an online version (using a web browser) and also as a desktop application installed on the host machine. For the desktop setup executable, there is an installer available at https://nxp.com. For Windows and macOS, the installers work as a wizard that guides you step by step through the installation process. The Debian package is available for Linux. The details about the installation can be found in the Installation Guide for Config Tools for i.MX (document IMXIUG).

To get started with the System Manager Configuration tool on an NXP board, download the GitHub repository and compile the SM for the target configuration.