Config Tools for i.MX Applications Processors 26.09 documentation

DDR Tool#

This section introduces the DDR configuration and validation tool, which is an embedded component of Config Tools for i.MX.

The DDR tool provides two main functionalities: configuration and validation.

Supported devices are indicated in the new project configuration page.

Note: DDR tool is provided “as is” to aid customer capabilities of evaluating, debugging, and optimizing their designs. The results, or any part thereof, provided by the tool cannot be under any circumstances seen as a substitute for the traditional validation and compliance methods, which still need to be performed to declare compliance of the designs with the respective JEDEC standards.

Create a new DDR tool project#

To use the DDR tool, first create a new project.

To create a new DDR tool project, follow these steps:

  1. Open the Config tools for i.MX.

  2. Choose Create a new standalone configuration for processor, board, or kit and click Next.

  3. From Processors, choose one of the devices with DDR tool support and click Finish.

  4. To open the DDR tool view, click the DDR tool icon.

    _images/config_tools_overview.png

    Config Tools overview#

  5. To use the DDR tool, accept the Disclaimer.

    _images/disclaimer.png

    Disclaimer#

DDR configuration#

The DDR configuration provides a user-friendly graphical interface to configure the DDR interface and other associated subsystems. You can use it to change the DDR controller and PHY configuration when a different memory module is used to the configuration and to optimize the parameters associated with signal integrity.

Import initialization script#

Import initialization script allows you to load the initialization script provided by the Register Programming Aid (RPA) tool and bypass the UI configuration.

  1. To import the RPA initialization script, use the Import initialization script button and browse for the desired *.ds file.

    _images/import_initialization_script.png

    Import initialization script#

  2. To load the *.ds file and disable the UI configuration interface, press OK.

    _images/disabled_ui.png

    Disabled UI#

  3. The contents of the imported *.ds file are shown in Code Preview, ddr_config.ds.

    _images/rpa_script_content.png

    RPA script content#

Select custom System manager#

For processors with the System manager, the DDR tool supports the default EVK board. For custom boards, select the System manager for that specific board to run memory tests.

To select a custom System manager, use the Select System Manager button, select Use Custom System Manager and browse for the custom System manager binary.

Note: Modify the SM configuration configs/customer_board.cfg

  1. In the A55 non-secure section:

    1. Make the LM owner of the DDR_CTRL, DDR_PHY, SRC, and SYSCTR_CTL resources

      # Resources
      …
      DDR_CTRL OWNER
      DDR_PHY OWNER
      SRC OWNER
      SYSCTR_CTL OWNER
      
    2. Grant the full DDR access to the LM:

      # Memory EXEC, begin=0x080000000, end=<highest DDR address>
      
  2. Ensure that UART1 is dedicated to the A55 LM, as the A55 test code uses this UART. This is the default in the NXP EVK SM configuration (SM uses UART2), but customers may have changed this.

_images/select_system_manager.png

Select System manager#

To revert to EVK default System manager, select the Use Default System Manager option.

Enable manual configuration#

To switch back to UI configuration, press Enable manual config.

_images/enable_manual_config.png

Enable manual config#

UI configuration#

The UI configuration allows you to manually change Device Information, PHY options, or design-specific configuration. Two modes are available: Basic and Advanced.

Note: Advanced mode is only recommended for experienced users.

Basic mode allows you to configure the parameters that are design-dependent.

  1. Device information

    _images/device_information_ui.png

    Device Information UI#

  2. Board data bus configuration for LPDDR4

    _images/board_data_bus_config_ui.png

    Board data bus config UI#

  3. UART port selection

    _images/uart_selection_ui.png

    UART selection UI#

  4. DBI selection (for LPDDR4)

    _images/dbi_selection.png

    DBI selection#

  5. Inline ECC configuration (for devices with Inline ECC support) allows you to select the following parameters:

    1. Enable/Disable Inline ECC

      _images/inline_ecc.png

      Inline ECC#

    2. ECC region granularity

      _images/ecc_region_granularity.png

      ECC region granularity#

    3. ECC protection configuration for each Main Memory Region

      The ECC config binary/non-binary aligned section summarizes the ECC configuration overview.

      _images/ecc_config_binary_non_binary_aligned_section.png

      ECC config binary/non-binary aligned section#

Advanced mode allows you to configure additional parameters.

  1. The firmware version is the one officially supported by the BSP, but the DDR tool allows you to select multiple versions.

    _images/firmware_version_selection_ui.png

    Firmware version selection UI#

    Note: Use only the Firmware version for your specific SoC and BSP GA version. Not all Firmware versions are supported for each SOC.

  2. PHY log level selection

    _images/phy_log_level_selection.png

    PHY log level selection#

  3. IOMUX configuration

    _images/iomux_configuration_ui.png

    IOMUX configuration UI#

  4. PMIC configuration sequence

    Note: If the Custom PMIC initialization option is enabled, the available commands are: pmic_set : most significant byte is the register, followed by the value pmic_cfg: most significant byte is the I2C bus, followed by the I2C address.

    _images/pmic_configuration_ui.png

    PMIC configuration UI#

  5. Custom configuration

    _images/custom_configuration_ui.png

    Custom configuration UI#

    Note: Any write to an incorrect address may cause unexpected behavior.

  6. DQ ODT and DS configuration

    _images/dq_odt_and_ds_configuration_ui.png

    DQ ODT and DS configuration UI#

  7. CA ODT and DS configuration – Informational Only

    _images/ca_odt_and_ds_configuration_ui.png

    CA ODT and DS configuration UI#

Multi-Vendor Initiative#

Preset configurations for memory devices from other vendors that have been tested by NXP can be made available by selecting Include configurations for memories tested by NXP. They then appear in the Preset drop list.

Note: These preset configurations are only applicable to the EVK board on which the device was tested. Custom designs may require additional changes.

_images/mvi_checkbox.png

Checkbox for enabling MVI Presets#

Code generation#

You can generate the configuration as C code in the Code Preview View, which can be used by the U-Boot SPL driver.

Any change in the GUI triggers code generation; the update is highlighted in the Code Preview.

_images/code_preview.png

Code Preview#

Save files from Code Preview to disk using the DDR tool Export Wizard.

_images/export_generated_files.png

Export generated files#

DDR validation#

The DDR validation uses different scenarios to assess DDR performance, by downloading a test image to the processor’s internal RAM.

DDR validation assesses stability of the DDR interface on the board in a non-OS environment.

_images/ddr_validation.png

DDR validation#

Connection#

This section describes connection to boards of various types.

Boards with Serial Download mode/Manufacture mode#

To connect to a board, do the following:

  1. Configure the board to boot in the Serial Download mode/Manufacture mode and power up the board.

  2. Connect a UART cable from the host computer to the UART of the A-core on the board.

  3. Connect a USB cable from the host computer to the USB port on the board that is used by the Serial Download mode. An “HID-compliant device” or a “USB Input Device” is shown in the Windows Device Manager.

Note: Connect the USB cable directly to the host PC USB port, not through a USB hub.

With the board connected to the host computer, search the UART ports using COM port scan. The COM port drop-down list is populated with all available UART ports.

_images/com_port_selection.png

COM port selection#

Choose the correct UART that is used as the A-core debug UART port.

Boards with JTAG connection available#

  1. Connect the JTAG probe (only the CWTAP probe is supported) to the board.

  2. Select between USB or Ethernet connection.

    _images/connection_type_selection.png

    Connection type selection#

Test scenarios#

Once the DDR configuration and board connection are set up, execute different Test scenarios. Customize each test by setting parameters in Test options.

Depending on the test and options selected, the execution time may differ. By default, a 90-second timeout is set to ensure that the test finishes if an issue occurs. To change the default value, edit the Timeout (seconds) option:

_images/timeout_selection.png

Timeout selection#

When the initial timeout expires, provide input to continue or stop the test execution.

_images/test_execution_timeout_s.png

Test execution timeout(s)#

To start test execution, press the “Start Validation” button. You can check the status of the running test from the Logs console. By default, the log level is set to ERROR. Additional log-level options are available, with different output in the console:

_images/log_level_selection.png

Log level selection#

At the end of the test, the PASS/FAIL status is displayed in “Results”. The test summary is displayed in “Summary”.

_images/test_status.png

Test status#

  • Yellow is for Test failed

  • Orange is for Configuration error

  • Red is for Target connection error or exception in the script

  • Green is for Test passed

If a test fails, the Summary view in the Advisor section displays Symptom and Possible Causes to provide high-level guidance on the debug process when looking for possible DDR subsystem issues.

_images/advisor_section.png

Advisor section#

The DDR tool offers several test scenarios that can be split into Inspection, Optimization, vTSA, and Stressing.

Inspection#

Inspection shows the status of the DDR Controller and DDR PHY configuration, by executing the following tests:

  1. Firmware Init – executes the DDR PHY training to check the DDR PHY configuration.

  2. Operational – performs a basic memory access test by running Write-Read-Compare/ Walking Ones/ Walking Zeros tests. Options such as Start Address, Size, Enable DDR Memory cache, and Access mode/Pattern are available for each test.

    _images/test_options.png

    Test options#

  3. ECC Regions test – tests each ECC region with 1-bit error injection to verify the region’s ECC capability (protected or unprotected).

    Note: The test is possible only for devices with inline ECC support.

Optimization#

DQ ODT and driver strength tests sweep the DQ IO configurations to create board-specific Driver Strength vs. ODT PASS/FAIL map for the Reads and the Writes.

Note: Optimization is not available when UI configuration is bypassed by RPA initialization script import.

_images/dq_odt_and_ds_map.png

DQ ODT and DS map#

For passing cells (Green cells), the option Apply current selection in DDR configuration (right-click on the cell) is enabled. It sets the respective Driver Strength and ODT value into the configuration for use in other scenarios.

_images/apply_dq_odt_and_ds_configuration.png

Apply DQ ODT and DS configuration#

Note: You can use the Driver Strength vs. ODT map as one of the criteria when deriving optimal ODT/Driver Strength values. This map cannot serve as all-encompassing output to make this determination.

Note: NXP strongly recommends using the default ODT and Drive strength values that are tested and validated as part of the GA BSP. To ensure that your design adheres to the board layout requirements, refer to the i.MX 8M Hardware Developer’s Guide.

Vref for 1D optimization test sweeps the PHY Vref and/or DRAM Vref to determine the values needed for PHY training to pass when PHY training fails, and to determine the trained values after the 2D training.

When the test passes, Apply current selection in DDR configuration option is enabled. It sets the respective PHY Vref and DRAM Vref values into the configuration.

_images/apply_current_selection_in_ddr_configuration.png

Apply current selection in DDR configuration#

Vref for the CA optimization test executes only 1D training and reads the VrefCA after the training is complete.

When the test passes, the Apply the current selection in the DDR configuration option is enabled. It sets the VrefCA value in the configuration.

vTSA#

vTSA performs Virtual Timing Signal Analysis by running tests to determine margins of the DDR subsystem.

Diag Write Margin/ Diag Read Margin tests create virtual data eye diagrams for each DQ lane.

_images/diagnostic_data_eyes.png

Diagnostic data eyes#

CA bus signals test creates post-training diagrams of the 6 CA control lines for each channel and CS.

_images/diagrams_of_the_6_ca_control_lines.png

Diagrams of the 6 CA control lines#

CA eye test creates post-training eyes of the 6 CA control lines for each channel and CS.

_images/command_address_eye.png

Command/Address eye#

Note: Details about vTSA are provided in the FAQ section.

Stressing#

To test the stability of the DDR configuration more extensively, you can use the Stressing scenario, with its suite of tests that covers different situations.

Two ways of running Stress tests are available:

  1. Single run runs the test suite one time with different options selected (Size, Enable DDR Memory cache, Stop on fail). In case of failure, you can check the status of each test in the suite in the Logs console, with Log level set to INFO

    _images/stress_tests.png

    Stress tests#

  2. Test duration runs the test suite for a selected time. This is suitable for overnight tests.

    _images/stress_tests_options.png

    Stress tests options#

    In the Logs console, you can monitor test execution and see the number of iterations and the duration.

    _images/stress_tests_results.png

    Stress tests results#

    Note: Ensure the Timeout (seconds) setting is higher than the Test duration setting, otherwise the test ends with timeout.

FAQ#

  1. What does vTSA mean?

    1. vTSA is an abbreviation for Virtual Timing Signal Analysis.

    2. A “virtual” TSA uses the memory controller itself to test margins without test equipment. “Virtual” does not mean simulation!

    3. Memory controllers can alter timings, voltage references, termination settings, and so on, for both incoming and outgoing signals.

    4. “Training” is a process when the memory controller sweeps these parameters and finds the configuration with the most margin for operation.

    5. A vTSA simply logs this information for output, which provides insight into the signaling margin of the system without the need for test equipment.

    6. Initialization and calibration settings can be dumped to a file for analysis as well.

  2. What is the vTSA output?

    1. Virtual Timing Signal Analysis(vTSA) provides write and read data eye diagrams virtually by running a series of write/read transactions as opposed to the hardware method of using a high-speed oscilloscope to perform manual physical TSA (pTSA) measurements.

    2. Therefore, vTSA output approximates the actual write/read eyes.

    3. Expect some variation between trained values of delay lines and VREF in comparison to the vTSA report of these values.

    4. vTSA only reports the values it detects in the “widest” part of the reported eye, which may itself vary from run-to-run.

    5. The key takeaway from using this tool is to display the virtual write/read eyes to convince the user of the robustness of their design.

      _images/read_eye.png

      Read eye#

  3. Need more information about vTSA?

    1. The vTSA tool is an approximation of an actual pTSA. Thus, you may note some variation between the trained delay line value and the vTSA “mid” value. This variation can be up to ~20 ps. Verify that the trained delay line value has ample margin within the data eye.

    2. For the trained VREF value, the LPDDR4 device Mode Register 14 (MR14), which holds the trained VREF value, applies to all byte lanes. Per JEDEC, MR14 is not per byte lane; it applies to all byte lanes.

    3. For a board that follows the NXP DDR layout guidelines, there should be plenty of margin around the trained VREF value. See the guidelines in the respective NXP Hardware Developer Guide.

  4. How is a data eye margin generated?

    1. There are several delay steps available to shift each DQ and DQS.

    2. As DQ crosses the unit interval, from zero-step delay to 1 unit interval step delay, each step is tested with a write-read-compare test to determine pass or fail.

    3. The DQ traverse of the unit interval is repeated for all available VREF steps.

    4. Delay steps generate a line, and repeating the lines at each VREF step generates data eye margin.

    5. The crossing of DQS signal with trained VREF and delay step is placed in the generated data eye margin.

    6. Each passing dot in the margin eye already meets the setup, hold, and voltage requirement.

      _images/data_eye_margin_generation.png

      Data eye margin generation#

  5. What represents the information next to the data eye?

    1. Unit interval = 1/data rate; for example, at 3200MT/s data rate the unit interval = 312.5 ps

    2. The x-axis displays the time. It is one unit interval in percentage. -50 % to +50 %

    3. The x-axis data eye margin width opening is displayed as the percentage of one unit interval. For example: Step w=80.56 % of UI

    4. The y-axis displays the voltage.

    5. The y-axis open data eye margin height/amplitude opening is displayed in voltage. Ex: Vref h=0.35 V

      _images/data_eye_information.png

      Data eye information#

  6. How much margin is considered good?

    1. To determine the required margin mask, you must do the following:

      • Optimize the DDR interface

      • Once settings are optimized, generate the worst-case data eye margin using the worst-case conditions (temperature, voltage, frequency, pattern) for a customer board DDR interface.

      • Use DDR training to optimize/center the strobe to the eye margin

    2. A green pixel in the data eye margin indicates a passing cell. It means for that green pixel the setup and hold time as well as the VIHLac/dc are satisfactory.

    3. Any additional green pixels around the strobe location in the data eye margin are additional margin available to DDR for that DQ.

  7. Why is the trained Vref sometimes not in the exact center of the eye?

    1. VREF training selects a value that satisfies all byte lanes’ passing VREF window and programs it into the LPDDR4 MR14 register. For a single byte lane, the trained VREF value may not appear centered in the data eye, but it provides the best margin for that lane while satisfying the other byte lanes.

  8. How to check that the wrong UART is selected?

    Set the Log Level to DEBUG and check the messages from console

    _images/wrong_uart_selected_message_1.png

    Wrong UART selected - message 1#

    or

    _images/wrong_uart_selected_message_2.png

    Wrong UART selected - message 2#

  9. How to proceed in case of test timeout?

    1. In case of test timeout, the below pop-up window appears

      _images/test_timeout_pop_up.png

      Test timeout pop-up#

    2. Increase the timeout (second) option and rerun the test. If the following error appears, power off the board, unplug the UART cable, power on the board, then plug in the UART cable.

      _images/uart_connection_error.png

      UART connection error#