GUI Guider Documentation#
- User Guide
- Welcome
- Getting Started
- Quick Start Guide
- IDE Overview
- Advanced Usage
- Development Guide
- Performance Optimization
- Tutorials
- How to use symbols
- Rotate screen and widgets
- Multi-language application
- 1. Authoring translation files
- 2. Extracting source strings and compiling the language pack
- 3. Implementing the language manager
- 4. Translating widget text and applying per-language fonts
- 5. Observing language changes and refreshing the UI
- 6. Wiring up the language manager in GUI Guider
- 7. Verifying the build and iterating on translations
- Notes on resources and layout
- Migration from GUI Guider v1
- Demos
- Reference
- FAQs
- What should I do if a configured property or style is not rendered correctly in the UI editor?
- How can I prevent the simulator from running target specific code?
- How can I reuse an application on a different board?
- What should I do if I create a project at an unsupported resolution from a template?
- What should I check if touch or display does not work?
- How can I customize
lv_confmacros without losing the changes after regeneration?
- Resources and links
- Glossary
- FAQs
- Revision history