V1.10.1 GA (Released on 15 December 2025)#
New features#
Library
LVGL v9.3.0
Performance
G2D enablement and demo
Multitouch demo
Toolchain
MCUXpresso SDK 25.09.00
IAR 9.60.4
Keil MDK 5.42
Linux Factory 6.12.34_2.1.0
Zephyr 4.2
Targets
i.MX8ULPEVK
i.MXRT700EVK RevB
Bug fix
LGLGUIB-4752: The number text area could enter a space, which causes a build error
The space character is allowed to be set in the text area, which should be a number. The application build can fail due to incorrect input.
LGLGUIB-5177: Vertical lines of the chart cannot be set to 0 in the lvgl8 project
The number of vertical lines in the chart widget cannot be set to 0 for the LVGL v8 project, which is allowed by the LVGL library.