MCUXpresso Configuration Tools 26.09 documentation

Peripherals Tool#

Features#

The Peripherals tool features:

  • Configuration of initialization for SDK drivers

  • User-friendly user interface that allows you to inspect and modify settings

  • Smart configuration component selection along the SDK drivers used in toolchain project

  • Instant validation of basic constraints and problems in configuration

  • Generation of initialization source code using SDK function calls

  • Multiple functional-group support for initialization alternatives

  • The tool shows configuration problems in the Problems view and marks them with decorators in other views

  • Integration in MCUXpresso Config Tools framework along with other tools

  • Middleware configuration support (USB, FREEMaster, LwIP)

  • The tool can automatically migrate the settings to a different SDK component version

  • Support of code snippets

Basic terms and definitions#

Basic terms and definitions#

Term

Definition

Functional group

Represents a group of peripherals that are initialized as a group. The tool generates a C function for each functional group that contains the initialization code for the peripheral instances in this group. Only one functional group can be selected as default initialization, the others are treated as alternatives that are not initialized by default.

Peripheral instance

Occurrence of a peripheral (device) of specific type. For example, UART peripheral has three instances on the selected processor, so there are UART0, UART1, and UART2 devices.

Configuration component

Provides user interface for configuring SDK software component (for example, peripheral driver) and generates code for its initialization.

Component instance

Configuration component can have multiple instances with different settings. (for example, for each peripheral instance like UART0, UART1).

Component mode

Specific use case of the component instance (for example, TRANSFER mode of DSPI, or interrupt-based mode of communication).

Workflow#

The following steps briefly describe the basic workflow in the Peripherals tool.

  1. Select Tools>Peripherals from the tools framework main menu to open the Peripherals tool.

  2. In the Peripherals view, select the peripheral instance you would like to configure (use the checkbox).

  3. In case more components are available for use by the peripheral, the Select component dialog appears. The dialog displays the list of suitable configuration components for the selected peripheral matching the SDK driver for the selected processor.

  4. Select the component that you want to use and click OK.

  5. In the settings editor that automatically opens, select the Component mode that you would like to use and configure individual settings.

    Note: The selection of the component mode may impact the appearance of some settings. Therefore, always select the mode as the first step.

  6. Open the Code Preview and see the output source code.

    Note: The source code preview is automatically generated after each change if no error is reported.

  7. Use the Update Code button from the toolbar. Alternatively, export the source code by selecting File>Export… from the Menu bar.

    Note: To export the source code, you can also click the Export button in the Code Preview view.

  8. Save settings in MEX format (used for all settings of all tools) by selecting File>Save from the Menu bar.

User interface overview#

_images/peripheral_view.png

Peripheral view#

_images/components_view.png

Components view#

Common toolbar (Peripherals)#

In addition to general items available to all tools, the Toolbar of the Peripherals tool contains two additional items:

Table toolbar#

Toolbar#

Item

Description

Global settings

Open a tab aggregating global settings of all configuration sets.

Initialization order

Open a dialog for customization of peripheral initialization order.

Note: For details on other items, refer to the Toolbar chapter.

Initialization order dialog#

In the Initialization order dialog, you can customize the initialization order of peripherals within selected functional groups.

_images/initialization_order_dialog.png

Initialization order dialog#

  1. Select the functional group you want to modify using the Functional group dropdown list.

  2. In the Initialization order list, use the up and down arrows to adjust the sequence of initialization.

  3. Click Save order to save your settings, or Cancel to close the dialog without changes.

Components view#

The components view shows a list of configuration components, sorted by category into groups such as Middleware, Peripheral drivers and others.

The view highlights configuration components based on their status.

Table component status#

Component status#

Status

Color highlighting

Enabled

Light gray.

Enabled/with warning

Light gray with the alert symbol.

Enabled/with error

Red with the error symbol.

Disabled

Dark gray.

_images/components_view.png

Components view#

In the Components view, you can perform several actions.

Table components view actions#

Components view actions#

Option

Description

Display configuration-component information

Point the mouse cursor at the configuration component to display general configuration-component information.

Open the Settings Editor of the configuration component

Left-click the configuration component to open its Settings Editor.

Add new configuration components

Left-click the + button and select from the list to add a component. In the Select component dialog, you can filter the list to show only toolchain-project-relevant, or latest version components. You can also click the + buttons next to Middleware/Peripheral drivers/Other categories to add new components in them directly as shown in the figure below the table.

Filter configuration components by name

Type a text string to filter configuration component names in the search bar.

_images/add_component_dialog.png

Add component dialog#

Right-click the configuration component to open a shortcut menu. Several options are available in the shortcut menu.

Table Shortcut menu options#

Shortcut menu options#

Option

Description

Open

Open the configuration component in the Settings Editor.

Open in another view

Duplicates the configuration component in the Settings Editor.

Enable/Disable

Enable/Disable the configuration component.

Edit comment

Create/Edit custom notes for the configuration component.

Lock/Unlock editing of component instance

Lock/Unlock the editing of the component instance.

Save to use case library

Create a template from the configuration component.

Documentation

Display the documentation of the configuration component, if available.

Remove

Remove the component from configuration. Note: If the component has any global settings, a dialog appears prompting you to confirm the removal. If the component does not have any global settings, the component is deleted after removing the last instance.

Migrate

Migrate the component to a different component type or to a component with a newer driver version.

Move to

Choose from available functional groups to move the configuration component to.

Copy to

Choose from available functional groups to copy the configuration component to.

Peripherals view#

The Peripherals view contains a table showing a list of available peripherals on the currently selected processor that can be configured by the Peripherals tool. In case of multicore processors, the displayed peripherals are also core-specific.

Each instance of a peripheral (for example, UART0) occupies one row. The first column contains the peripheral name and a checkbox indicating whether the peripheral is used by any component instance.

The second column contains the name of the component instance handling the peripheral. This name is customizable in the settings editor and it is used in generated code. The name of the component instance cannot contain spaces.

You can enable an instance by selecting the checkbox, or by clicking the switch in the settings editor of the component instance.

Disable a component instance by unchecking the checkbox.

Double-click the second column to open the Settings Editor for the component instance.

Right-click the peripheral to open a shortcut menu. Several options are available in the shortcut menu.

Table Shortcut menu options#

Shortcut menu options#

Option

Description

Open

Open the component instance in the Settings Editor.

Open in another view

Duplicate the component instance in the Settings Editor.

Enable/Disable

Enable/Disable the component instance.

Add component instance

Add a component instance to the peripheral.

Initialized in user code

Mark the peripheral as configured by user code (available on not configured peripherals).

Edit comment

Create/Edit custom notes for the component instance.

Lock/Unlock editing of component instance

Lock/Unlock the editing of the component instance.

Save to use case library

Create a template from the component instance.

Documentation

Display the documentation of the component instance, if available.

Remove

Remove the component instance from configuration. If more instances are in use, a confirmation window allows you to select which instance you want to remove.

Migrate

Migrate the component to a different component type or to a component with a newer driver version.

Move to

Choose from available functional groups to move the component instance to.

Copy to

Choose from available functional groups to copy the component instance to.

Settings editor#

You can edit peripheral component settings in the Settings Editor. Open editors are shown in the central area of the screen, each with its own tab. Multiple editors can be opened at the same time. Changes done in the editor are immediately applied and kept even if the settings editor is closed. Settings that are disabled are highlighted in gray. In case that a component instance is disabled, all settings are highlighted in gray. Tooltips are displayed for all enabled settings when the mouse cursor is placed at settings.

To open Settings Editor, do the following:

  • Double-click the component instance in the Peripherals or Components view to display component instance settings.

  • Left-click the component in the Components view to display global settings of the component.

_images/settings_editor.png

Settings editor#

Settings Editor header#

All components share the Settings Editor header. In the header, you can view and change component information, enable or disable the component, and view component documentation (where applicable).

_images/settings_editor_header.png

Settings Editor header#

Table Settings Editor header#
Settings Editor header#

Header item

Description

Description

Displays the configuration component title.

Name

Displays the component instance name. This name is used in the generated code in constants and function identifiers and is derived from the peripheral name. You can change it at any time by clicking the Custom name button and editing the field.

Mode

Displays the required usage for the component instance and influences available settings. Use the dropdown menu to change the mode (where applicable).

Peripheral

Displays the name of the peripheral to be associated with the component instance. Use the dropdown menu to change it.

Documentation

Click the button to view configuration component-specific documentation in the Documentation view. Not all configuration components are documented, therefore not all setting headers contain the Documentation icon.

Lock editing

Click the button to lock/unlock component editing. Source code is still generated.

Enable/disable component instance switch

Use the switch to enable or disable selected component instance. By disabling the instance, you don’t remove it from the tools configuration, but prevent its inclusion in the generated code.

Presets#

Settings are grouped into larger groups (config sets) that may provide presets with typical values. You can use these presets to quickly set the desired typical combination of settings or return to the default state.

_images/quick_selection_example.png

Quick selection example#

Settings#

The following setting types are available in the Settings Editor.

  • Boolean – Two state setting (yes/no, true/false).

_images/boolean_setting_example.png

Boolean setting example#

  • Integer, Float – Integer or float number.

_images/integer_float_setting_example.png

Integer/Float setting example#

  • String – Textual input. Supports more than a single line.

_images/string_setting_example.png

String setting example#

  • Enumeration – Selection of one item from a list of values.

_images/enumeration_setting_example.png

Enumeration setting example#

  • Set – List of values, multiple of them can be selected.

_images/set_setting_example.png

Set setting example#

  • Structure – Group of multiple settings of different types, may contain settings of any type including nested structures.

_images/structure_setting_example.png

Structure setting example#

  • Array – Array of multiple settings of the same type – you can add/remove items. The array of simple structures may also be represented as a table grid, master-detail, tabs, and radio buttons.

_images/array.png

Array#

The ‘+’ button adds a new item at the end of the array. To rearrange the position or delete an item, right-click the item and select one of the following options: Move up, Move down, Move to top, Move to bottom, or Remove. You can also copy-paste an array from one instance to another by right-clicking the array label and choosing Copy. You can then navigate to another instance array, right-click the table, and choose Paste to add it.

Note: The array can be copied and pasted to another configuration, including in the second running instance of Config Tools.

_images/array_setting_example.png

Array setting example#

  • Info – Read-only information for the user.

_images/info_setting_example.png

Info setting example#

_images/info_setting_as_link_example.png

Info setting as link example#

  • File setting - Link/import an external settings file.

_images/file_setting.png

File setting#

Documentation view#

You can display component-specific documentation by opening the Documentation view.

Note: Not all components might have this option enabled.

_images/documentation_view.png

Documentation view#

You can open the Documentation view in several ways:

  • In the Peripherals view, right-click the peripheral checkbox and choose Documentation from the list.

  • In the Components view, right-click the component and choose Documentation from the list.

  • In the Settings Editor, click the Documentation button next to the component name.

  • In the Settings Editor, click the question mark next to the settings label.

Component use case library#

In the Peripherals tool, you can save, edit, and import/export component use cases for future use. Use cases are saved in a MEX format and can be viewed and modified in the Component use case library. The library displays all created/imported use cases by component type.

To open the Component use case library, select Peripherals>Component use case library from the Menu bar.

To create a component use case, do the following:

  1. Right-click an entry in the Peripherals or Components views.

  2. Select Save to use case library from the context menu.

  3. Enter the name and description in the Use case detail dialog.

  4. Click OK.

Component migration to a different version#

Configuration components that generate configuration code for SDK components often require specific versions (or range of versions) of one or more SDK components.

The SDK component and its version that are expected for the proper function of the configuration component are visible when components are added to the selection dialog:

_images/component_selection.png

Component selection#

It is also visible in the tooltip in the Component view:

_images/tooltip_in_the_component_view.png

Tooltip in the Component view#

You can update the SDK components in the toolchain/IDE project.

When a configuration is open and the SDK component versions in the toolchain project do not match the version referenced in the configuration component, automatic migration is offered in the Component migration dialog. The migration can also be launched manually in the Peripherals tool using the menu Peripherals > Migrate to other component versions.​

_images/migration_dialog.png

Migration dialog#

Each row in the dialog corresponds to one configuration component that can be migrated to another version. The dialog above displays the current version specified in the current configuration component and a combo box that allows you to select the new version that replaces the current one.

In standalone Config Tools, it is possible to migrate settings to any available version. In IDE/toolchain project mode, the combo box contains only the component with the version matching the SDK component currently used in the project.​

The default selection in the toolchain-less configuration is “Do not migrate”. In the toolchain configuration, the default selection is the only version to which migration can be performed. If “Do not migrate” is selected, no changes are made to the particular component.

The Ignore checkbox prevents the component from the migration during next check.​

After you confirm the dialog by selecting “Migrate”, the component is replaced by the component matching the selected version of the SDK component. The settings are migrated to the corresponding settings in the new version of the component, where it is possible.

If the new version of the component contains some new settings, these settings are filled with the default values. Check manually if the components are set properly.

The Migration result dialog is a dialog with the summary of the migration. It automatically opens after migration is successfully completed. This dialog contains the summary of events with various impact that happened during the migration. It also contains a link that opens the generated detailed report in HTML format, and a button that copies the path to the report to the system clipboard.

The generated Migration report contains the date and information about the configuration location, MCU, and toolchain project in its header. It helps identify which configuration it is related to. Below that is a table that contains rows for each migration. A short description of the migration is provided. Each row has two columns where the first contains the path to the migrated setting and the second contains the description of the migration. Each row can have differently colored text that indicates the importance of the message.

Problems#

The tool validates the settings, and problems and errors are reported in the Problems view.

If there is an error related to the setting or component, an error decorator is shown next to the element containing an error.

_images/error_decorators.png

Error decorators#

In the case of a dependency error, a quick-fix button is displayed.

_images/quick_fix_1.png

Quick fix 1#

Right-click the button to display a list of issues, then left-click the issue to display possible solutions.

_images/quick_fix_2.png

Quick fix 2#

You can quickly fix the problem even when it is reported from a table cell as the context menu contains the list of possible quick fixes (see register initialized SCTimer, for example LPC54114 Resources->Outputs setting).

_images/quick_fix_3.png

Quick fix 3#

Code generation#

If the settings are correct and no error is reported, the tool’s code generation engine instantly regenerates the source code. You can view the resulting code in the Code Preview view of the Peripherals tool.

Code Preview automatically highlights differences between the current and immediately preceding iteration of the code. You can choose between two modes of highlighting by clicking the Set viewing style for source differences. You can also disable highlighting altogether from the same dropdown menu. Such features as Copy, Search, Zoom-in, Zoom-out, and Export source are available in the Code Preview view. You can also invoke the search by pressing CTRL+F or from the context menu.

The Peripherals tool produces the following C files:

  • peripherals.c

  • peripherals.h

    Note: For multicore processors, the tool generates peripherals.c/.h for each core, containing functional groups associated with that core. It can be configured in functional group properties.

    Note: Some components, such as the USB or FlexSPI, may generate additional output files.

These files contain initialization code for peripherals produced by selected configuration components including:

  • Constants and function declarations in the header file.

  • Initialized configuration structure variables (constants).

  • Global variables for the user application that are used in the initialization. For example, handles and buffers.

  • Initialization function for each configuration component.

  • Initialization function for each functional group. The function name is the same as the functional group name. It is prefixed by the “prefix” property if defined in the functional group dialog. These functions execute all assigned component initialization functions.

  • Default initialization function that calls the function initializing the selected functional group of peripherals.

    Note: The prefixes of the global definitions (defines, constants, variables, and functions) can be configured in the Properties of the functional group.

_images/code_preview_peripherals.png

Code Preview Peripherals#