Recommended system requirements#
The following lists the minimum system requirements to install and run the software:
One of the following graphical operating systems:
Microsoft Windows 11 (64-bit version)
Ubuntu 24.04 LTS
Note: Linux-hosted variants of the tools are distributed on Linux as 64-bit binaries, which may not work on 32-bit systems.
Supported desktop environments: GNOME
macOS X operating system (macOS Monterey 12 or later).
8 GB RAM or more
Display with resolution 1366 x 768 or more
Internet connection for dynamic download from processor database