MCUXpresso SDK Documentation

Encrypted XIP and MCUboot#

1. Introduction#

To keep image data confidential while it is in transport to the device or while it resides in non-secure storage such as external flash memory, MCUboot supports encrypting and decrypting images on-the-fly during an upgrade. The MCUboot architecture expects XIP to be done from a secure memory, so the encrypted image is decrypted to a secure location such as internal flash or RAM. However, internal RAM is limited in size, and some devices have interfaces to external flash memory only.

Some NXP devices support encrypted XIP on an internal or external flash device using on-the-fly decryption modules (BEE, OTFAD, IPED, NPX, etc.). These decryption engines can be used together with a second-stage bootloader such as MCUboot.

This document describes an extension of the MCUboot functionality that supports encrypted XIP on NXP devices, and its enablement in the OTA examples in the MCUXpresso SDK.

2 Encrypted XIP configuration structures#

In summary, every NXP encryption module utilizing the encrypted XIP feature uses a scheme where on-the-fly decryption is configured by ROM. After device reset, the ROM investigates specific configuration structures typically expected at a particular flash offset in the header of the bootable image, which is MCUboot in our case. If configuration structures are valid, then the ROM configures the encryption module for encrypted XIP.

In the case of an OTA update, it is expected that for security reasons the key (or IV/nonce) of the encrypted execution region is also updated, so configuration blocks also have to be re-generated for each OTA update. Unfortunately, this creates a risk during the update of these configuration blocks, as there is a period of time where a power loss could corrupt the update and result in a bricked device.

Note: The risk is related only to use cases using a custom second-stage bootloader. OTA solutions using only a ROM bootloader typically utilize a dual image feature which safely handles this issue, as the ROM can safely revert to the last functional configuration.

The risk is resolved by moving configuration blocks out of the header of the second stage bootloader to a particular flash area and letting the bootloader configure the encryption module manually by inspecting these configuration blocks.

Image

There is always one static configuration for the MCUboot region, investigated by ROM during startup and used for encrypted XIP initialization of the MCUboot region, and one or two dynamic configurations (depending on mode) for application slots, which are regenerated during an OTA update. The application configuration structure is manually handled by MCUboot to provide more flexibility and robustness to the update process.

The encrypted XIP extension uses a reserved area called encryption metadata, which is used for storage of configuration blocks. The following image shows a generic structure of the encryption metadata.

Image

The metadata sector consists of a platform-specific configuration block and a magic ID. The magic acts as a confirmation of the configuration block’s integrity, as it is written last in a separate flash page.

It is recommended to keep the configuration block and the magic ID in a common flash sector, so that they are separated by flash-page granularity and erased simultaneously during a sector erase. In the example code, the configuration block is typically placed at the beginning of the sector and the magic at the end.

During an OTA update, the extension generates a new configuration block, holds it as a context in RAM, and reconfigures the encryption unit for the updated area. If the OTA update and the verification of the execution area are successful, the configuration block is then persisted in flash. This approach is necessary for some encryption modules (such as IPED and NPX), because reading an invalid cipher causes a device reset, which could lead to an endless reset loop.

3. Encrypted XIP upgrade modes#

The extension supports OVERWRITE_ONLY and FLASH_REMAP upgrade modes. Each strategy has its advantages and disadvantages, so the selection depends on the user and their requirements.

Note: Encrypted XIP with FLASH_REMAP support is currently in an experimental state and enabled only for RW61x devices using IPED encryption. The mode can be evaluated only with ota_mcuboot_basic example

3.1 OVERWRITE_ONLY#

This update strategy combines the platform-specific encrypted XIP feature with the functionality of MCUboot encrypted images created by imgtool.

The following image shows a simplified OTA update flow of a device fleet using the encrypted XIP extension.

Image

The device fleet shares a common MCUboot private key used for decryption of encrypted OTA images residing in staging areas. The MCUboot AES key and hardware encryption module are then used for image re-encryption to the execution area. The hardware key is provisioned by NXP or a user and is typically unique per device instance to prevent image cloning.

For OVERWRITE_ONLY mode an image encrypted by MCUboot is used as a secure capsule for transport and staging in the non-XIP area of a device. This is a feature of MCUboot - for more information please see MCUboot Encrypted images documentation.

In summary, an image payload is encrypted using the AES-CTR cipher by imgtool (see imgtool). The AES key is randomized per OTA image and appended to the image as an encrypted TLV section. The encrypted AES key can be decrypted using a private key in the selected key encryption scheme (RSA-OAEP, AES-KW, ECIES-P256 or ECIES-X25519).

The following image shows key management for OVERWRITE_ONLY mode:

Image

As shown in the image, a user must securely embed the encryption private key into the device. For simplicity, the OTA examples in SDK use private keys embedded as a C array in MCUboot code (see middleware\mcuboot_opensource\boot\nxp_mcux_sdk\keys.c). Users are advised to implement secure provisioning and loading of the private key in the device, for example by encrypting the MCUboot application (including the array) using the encrypted XIP feature of the device, or by staging the private key in trusted sources like OTP or TPM (supported since MCUboot 2.2.0).

3.1.1 OVERWRITE_ONLY partition layout#

The extension customizes the OVERWRITE_ONLY upgrade mode and uses a partition layout with one execution slot for encrypted XIP, one slot for staging an OTA image, and one sector for encryption metadata. The revert functionality is not possible here.

The following image shows the flash memory layout:

Image

The secondary slot acts as a staging area for the encrypted OTA image handled by MCUboot. The execution slot is used to execute the encrypted image using the platform’s on-the-fly decryption.

Note: the placement of the encryption configuration blocks in the flash memory is up to the user.

3.1.2 OTA flow of modified overwrite only mode#

The following image shows a simplified flow of the MCUboot overwrite-only mode extended with the encrypted XIP extension.

Image

Before jumping to the booting process, the on-the-fly decryption is initialized so that MCUboot is able to read and validate the content in the primary slot. The re-encryption process is implemented in customized MCUboot code and in MCUboot hooks (see flash_api.c and bootutil_hooks.c).

3.2 FLASH_REMAP#

This update strategy combines the platform-specific encrypted XIP feature with flash remapping.

The following image shows a simplified OTA update flow of a device fleet using the encrypted XIP extension.

Image

An OTA image is always downloaded to the inactive slot and marked for testing on the next boot. If the new image does not confirm itself as OK, it is deleted and the previous version boots again. This feature is called revert.

The hardware key is provisioned by NXP or a user and is typically unique per device instance to prevent image cloning.

Compared to OVERWRITE_ONLY mode, this update strategy doesn’t use MCUboot encrypted images, so there is no need to secure the MCUboot private key. However, the OTA image is then just a signed plaintext, which is exposed during transport. If the transport isn’t secure, the user must implement their own secure container or utilize SB3 as a secure capsule for the MCUboot image.

Following image shows keys management for FLASH_REMAP mode:

Image

3.2.1 FLASH_REMAP partition layout#

The extension customizes the FLASH_REMAP upgrade mode. The following image shows the flash memory layout:

Image

Note: the placement of the encryption configuration blocks in the flash memory is up to the user.

3.2.2 OTA flow of modified FLASH_REMAP mode#

The following image shows a simplified flow of the MCUboot flash remap mode extended with the encrypted XIP extension.

Image

Before jumping to the booting process, the on-the-fly decryption is initialized so that MCUboot is able to read and validate the content in both slots. Compared to OVERWRITE_ONLY, the encryption is performed by the application during OTA - not from the MCUboot context. MCUboot only initializes encrypted XIP after boot (see flash_api.c and bootutil_hooks.c).

3.2.3 Limitations of FLASH_REMAP mode#

The flash remap feature combined with encrypted XIP adds another layer of complexity. Encrypted data can be decrypted on-the-fly only through logical access (code read, code fetch), as physical access (using the flash driver) returns encrypted data. Due to this, from the application context with an active flash remap, the decrypted content such as the image header and image payload in the inactive (overlaid) slot is not accessible. For example, from the application context, it is not possible to calculate a hash of written data—which is required by some certifications (https://arm-software.github.io/psa-api/fwu/).

3.3 Summary of Encrypted XIP upgrade modes#

Encrypted XIP mode

OVERWRITE_ONLY

FLASH_REMAP

Revert (Fall to previous version)

No

Yes

Analyzing slots from application context

Yes

Only image state

Security of OTA image

MCUBoot encrypted image

Up to user or utilize SB3

Encryption process

By MCUBoot during overwrite

By application during OTA update

4. Supported encryption modules#

Encryption module

State of support

Upgrade modes

Additional documentation

BEE

Supported

OVERWRITE_ONLY

BEE documentation

OTFAD

Supported

OVERWRITE_ONLY

OTFAD documentation

NPX

Partially supported

OVERWRITE_ONLY

NPX documentation

IPED

Supported only for RW61x devices

OVERWRITE_ONLY / FLASH_REMAP

IPED documentation

4.1 Supported boards#

BEE:

OTFAD:

IPED:

NPX:

5. OTA examples instructions#

Start preferentially with an empty board, erasing original content if needed.

5.1 Generate ECIES-P256 key pairs for encrypted image containers (optional)#

Note: For evaluation purposes this part can be skipped, as the OTA examples in the SDK use pre-generated key pairs.

  1. Generate private key using imgtool: imgtool keygen -k enc-ec256-priv.pem -t ecdsa-p256

    • Adjust the content of the middleware\mcuboot_opensource\boot\nxp_mcux_sdk\keys\enc-ec256-priv.pem accordingly.

  2. Extract private key to a C array: imgtool getpriv --minimal -k enc-ec256-priv.pem

    • Adjust the content of the middleware\mcuboot_opensource\boot\nxp_mcux_sdk\keys\enc-ec256-priv-minimal.c accordingly.

  3. Derive the public key: imgtool getpub -k enc-ec256-pub.pem -e pem

    • Adjust the content of the middleware\mcuboot_opensource\boot\nxp_mcux_sdk\keys\enc-ec256-pub.pem accordingly.

5.2 Enable encrypted XIP support and build projects#

There are several ways to enable Encrypted XIP mode.

OVERWRITE_ONLY:

  1. Manually modify content of sblconfig.h

    • Disable default upgrade mode (e.g. CONFIG_BOOT_MODE_FLASH_REMAP) and CONFIG_BOOT_CUSTOM_DEVICE_SETUP

    • Enable CONFIG_BOOT_MODE_ENCRYPTED_XIP_OVERWRITE

    • Note: currently not supported for OTFAD targets

  2. Manually customize Kconfig configuration and generate the project - see Kconfig and customization of OTA examples

  3. Use pre-defined customized builds - see particular chapter in your board readme (see Supported boards)

FLASH_REMAP:

Manually modify content of sblconfig.h

  • Disable default upragde mode (e.g. CONFIG_BOOT_MODE_FLASH_REMAP) and CONFIG_BOOT_CUSTOM_DEVICE_SETUP

  • Enable CONFIG_BOOT_MODE_ENCRYPTED_XIP_REMAP

Then build and load the mcuboot_opensource application.

5.3 Sign and encrypt image#

To sign and encrypt an application binary, imgtool must be provided with the respective key pairs and a set of parameters as in the following examples.

OVERWRITE_ONLY:

This mode requires offline encryption for security.

 imgtool sign --key sign-ecdsa-p256-priv.pem
         --align 4
         --header-size 0x400
         --pad-header
         --slot-size 0x200000
         --max-sectors 800
         --version "1.1"
         -E enc-ec256-pub.pem
         ota_app.bin
         signed_ota_app_encrypted.bin

FLASH_REMAP:

 imgtool sign --key sign-ecdsa-p256-priv.pem
         --align 4
         --header-size 0x400
         --pad-header
         --slot-size 0x200000
         --max-sectors 800
         --version "1.1"
         ota_app.bin
         signed_ota_app.bin

The parameter values can be obtained from the readme file of the target board, e.g. boards\BOARD\ota_examples\mcuboot_opensource\example_board_readme.md.

5.4 Initial image#

There are several methods to run the device for the first time (initial image) when the application uses encrypted XIP.

5.4.1 Load an initial image to flash memory (production)#

See flash_partitioning.h for your board. For example:

#define BOOT_FLASH_ACT_APP                0x60040000  -- active (execution) slot 0 address
#define BOOT_FLASH_CAND_APP               0x60240000  -- candidate slot 1 address
#define BOOT_FLASH_SLOT0_ENC_CFG_ADDRESS  0x60440000  -- encryption metada address - slot 0
#define BOOT_FLASH_SLOT1_ENC_CFG_ADDRESS  0x60441000  -- encryption metada address - slot 1 //FLASH_REMAP only

OVERWRITE_ONLY:

An encrypted OTA image always has to be loaded to the candidate slot address defined by BOOT_FLASH_CAND_APP. The MCUboot code recognizes the empty primary slot and re-encrypts the OTA image from the secondary slot to the primary slot.

FLASH_REMAP:

An OTA image can be loaded to slot 0 or slot 1 using an initial SB3. Please see IPED documentation.

5.4.2 Run unsigned unencrypted OTA application (development)#

An unsigned, unencrypted application can be loaded and run from the execution area using a debug session, and can then process the OTA update as usual.

5.5 Running the example#

OVERWRITE_ONLY:

Expected output for the initial image:

hello sbl.
Bootloader Version 2.3.0
Built Apr 22 2026 13:19:23
Toolchain IAR ANSI C/C++ Compiler V9.70.4.588/W64 for ARM
Upgrade mode: ENCRYPTED XIP: OVERWRITE ONLY
context_boot_go
Image index: 0, Swap type: none
Image 0 upgrade secondary slot -> primary slot
Erasing the primary slot
Encrypted XIP: Erasing configuration block slot 0
Image 0 copying the secondary slot to the primary slot: 0xa64e bytes
boot_write_magic: fa_id=0 off=0x1ffff0 (0x23fff0)
erasing secondary header
erasing secondary trailer
Bootloader chainload address offset: 0x40000
Reset_Handler address offset: 0x40400
Jumping to the image

*************************************
* Basic MCUBoot application example *
*************************************

Built Apr 22 2026 13:20:05
Toolchain IAR ANSI C/C++ Compiler V9.70.4.588/W64 for ARM

$

An example of OTA update:

*************************************
* Basic MCUBoot application example *
*************************************

Built Apr 22 2026 13:20:05
Toolchain IAR ANSI C/C++ Compiler V9.70.4.588/W64 for ARM

$ image
Image 0; name APP; state None:

  Slot 0 APP_PRIMARY; offset 0x40000; size 0x200000 (2097152):
    <IMAGE: size 41280; version 1.0.0+1000>
    SHA256 of image payload: 2EF7A87FCF1A7C9B6FB4...
    log_addr 0x8040000
    *ACTIVE*

  Slot 1 APP_SECONDARY; offset 0x240000; size 0x200000 (2097152):
    <No Image Found>

$ image erase
Erasing inactive slot...done
$ xmodem
Started xmodem download into flash at 0x240000
Initiated XMODEM-CRC transfer. Receiving... (Press 'x' to cancel)
CCCCC
Received 43008 bytes
SHA256 of received data: 8A7CB03313D4FB85D952...
SHA256 of flashed data:  8A7CB03313D4FB85D952...
$
$ image test
write magic number offset = 0x43ff00
$ image
Image 0; name APP; state ReadyForTest:

  Slot 0 APP_PRIMARY; offset 0x40000; size 0x200000 (2097152):
    <IMAGE: size 41280; version 1.0.0+1000>
    SHA256 of image payload: 2EF7A87FCF1A7C9B6FB4...
    log_addr 0x8040000
    *ACTIVE*

  Slot 1 APP_SECONDARY; offset 0x240000; size 0x200000 (2097152):
    <IMAGE: size 41280; version 1.0.1+1000>
    SHA256 of image payload: 62E17385C88450873F4D...
    log_addr 0x8240000

$ reboot
System reset!
hello sbl.
Bootloader Version 2.3.0
Built Apr 22 2026 13:19:23
Toolchain IAR ANSI C/C++ Compiler V9.70.4.588/W64 for ARM
Upgrade mode: ENCRYPTED XIP: OVERWRITE ONLY
Encrypted XIP: Successfuly initialiazed for slot 0
context_boot_go
Image index: 0, Swap type: test
Image 0 upgrade secondary slot -> primary slot
Erasing the primary slot
Encrypted XIP: Erasing configuration block slot 0
Image 0 copying the secondary slot to the primary slot: 0xa64d bytes
boot_write_magic: fa_id=0 off=0x1ffff0 (0x23fff0)
erasing secondary header
erasing secondary trailer
Bootloader chainload address offset: 0x40000
Reset_Handler address offset: 0x40400
Jumping to the image

*************************************
* Basic MCUBoot application example *
*************************************

Built Apr 22 2026 13:20:05
Toolchain IAR ANSI C/C++ Compiler V9.70.4.588/W64 for ARM

$ image
Image 0; name APP; state None:

  Slot 0 APP_PRIMARY; offset 0x40000; size 0x200000 (2097152):
    <IMAGE: size 41280; version 1.0.1+1000>
    SHA256 of image payload: FD9FBFD76F9708A6D761...
    log_addr 0x8040000
    *ACTIVE*

  Slot 1 APP_SECONDARY; offset 0x240000; size 0x200000 (2097152):
    <No Image Found>

$

FLASH_REMAP:

Expected output for the initial image:

hello sbl.
Disabling flash remapping function
Bootloader Version 2.3.0
Built Apr 22 2026 13:36:46
Toolchain IAR ANSI C/C++ Compiler V9.70.4.588/W64 for ARM
Upgrade mode: ENCRYPTED XIP: FLASH REMAP
Encrypted XIP: Successfuly initialiazed for slot 0
Primary slot: version=1.1.2+1000
Image 0 Secondary slot: Image not found
Image 0 loaded from the primary slot
Bootloader chainload address offset: 0x40000
Reset_Handler address offset: 0x40400
Jumping to the image


Booting the primary slot - flash remapping is disabled

*************************************
* Basic MCUBoot application example *
*************************************

Built Apr 20 2026 19:16:47
Toolchain IAR ANSI C/C++ Compiler V9.70.4.588/W64 for ARM

$

An example of OTA update using signed image:

Note: For SB3 OTA image call xmodem_sb3 command

*************************************
* Basic MCUBoot application example *
*************************************

Built Apr 22 2026 14:00:11
Toolchain IAR ANSI C/C++ Compiler V9.70.4.588/W64 for ARM

$ image
Note:This is Remap + Encrypted XIP, image payload can't be read
Image 0; name APP; state None:

  Slot 0 APP_PRIMARY; offset 0x40000; size 0x200000 (2097152):
    <No Image Found>

  Slot 1 APP_SECONDARY; offset 0x240000; size 0x200000 (2097152):
    <No Image Found>

$ image erase
Erasing inactive slot...done
$ xmodem
Started xmodem download into flash at 0x240000
Configured configuration block for slot 1
Initiated XMODEM-CRC transfer. Receiving... (Press 'x' to cancel)
CCCCC
Received 44032 bytes
$
$ image test
write magic number offset = 0x43ff00
$ image
Note:This is Remap + Encrypted XIP, image payload can't be read
Image 0; name APP; state ReadyForTest:

  Slot 0 APP_PRIMARY; offset 0x40000; size 0x200000 (2097152):
    <No Image Found>

  Slot 1 APP_SECONDARY; offset 0x240000; size 0x200000 (2097152):
    <No Image Found>

$ reboot
System reset!
hello sbl.
Disabling flash remapping function
Bootloader Version 2.3.0
Built Apr 22 2026 13:36:46
Toolchain IAR ANSI C/C++ Compiler V9.70.4.588/W64 for ARM
Upgrade mode: ENCRYPTED XIP: FLASH REMAP
Encrypted XIP: Successfuly initialiazed for slot 0
Encrypted XIP: Successfuly initialiazed for slot 1
Primary slot: version=1.0.3+1000
Secondary slot: version=1.0.4+1000
writing copy_done; fa_id=1 off=0x1fffe0 (0x43ffe0)
Image 0 loaded from the secondary slot
Bootloader chainload address offset: 0x240000
Reset_Handler address offset: 0x240400
Jumping to the image


Booting the secondary slot - flash remapping is enabled

*************************************
* Basic MCUBoot application example *
*************************************

Built Apr 22 2026 14:00:11
Toolchain IAR ANSI C/C++ Compiler V9.70.4.588/W64 for ARM

$ image accept
$ image
Note:This is Remap + Encrypted XIP, image payload can't be read
Flash REMAP_OVERLAY active.

Image 0; name APP; state Permanent:

  Slot 0 APP_PRIMARY; offset 0x40000; size 0x200000 (2097152):
    <No Image Found>

  Slot 1 APP_SECONDARY; offset 0x240000; size 0x200000 (2097152):
    <No Image Found>

$