MCUXpresso SDK Documentation

Encrypted XIP using BEE (Bus Encryption Engine)

Encrypted XIP using BEE (Bus Encryption Engine)#

This document extends the documentation of MCUboot and encrypted XIP in OTA examples and provides additional information related to the BEE module.

1. Introduction#

BEE is specific to RT10xx (except RT1010). The engine supports up to two separate regions using two separate AES keys. In the OTA examples, BEE region 1 is used for encrypting the execution slot, and BEE region 0 is reserved for the bootloader.

BEE configuration blocks are organized as EPRDB (Encrypted Protection Region Descriptor Block), where the EPRDB is encrypted using AES-CBC mode with AES key and IV located in KIB (Key Info Block). The KIB is encrypted as EKIB (Encrypted KIB) using a key provisioned by the user. Each BEE region has its PRDB/KIB pair.

The EKIB is decrypted by a key based on selection in BEE_KEYn_SEL fuse:

  • Software key

    • default value in BEE_KEYn_SEL

    • evaluating BEE without fusing the device

  • SW-GP2

    • fused by user and typically used for offline encryption

    • limited functionality due to hardware bugs, see the errata

    • not supported in the examples

  • OTPMK

    • provisioned by NXP in factory

    • unique per device instance - prevents image cloning

    • recommended

The firmware in the execution slot is decrypted/encrypted using AES-CTR, combining the nonce extracted from the PRDB with this device key. The extension automatically detects the device key by evaluating the BEE_KEYn_SEL fuse.

The whole BEE initialization and encryption metadata handling is implemented in the encrypted_xip_platform_bee.c module.

Additional information can be found in the Security Reference Manual of the target device and in application notes AN12800, AN12852, and AN12901.

1.1 Metadata structure#

The structure follows the ROM code, but the BEE configuration is handled manually from the MCUboot context.

Metadata Flash Sector (BEE)
━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━

 0                    ┌─────────────────────────────────────────────────────┐
                      │  ekib          [32 bytes]  encrypted kib_t          │
                      │    aes_key     [16 bytes]                           │
                      │    iv          [16 bytes]                           │
 +32                  ├─────────────────────────────────────────────────────┤
                      │  eprdb         [256 bytes] encrypted prdb_t         │
                      │    tagl/tagh   [8 bytes]                            │
                      │    version     [4 bytes]                            │
                      │    fac_count   [4 bytes]                            │
                      │    enc_region  [64 bytes]                           │
                      │      start     [4 bytes]                            │
                      │      end       [4 bytes]                            │
                      │      aes_mode  [4 bytes]                            │
                      │      nonce     [16 bytes]                           │
                      │      reserved  [36 bytes]                           │
                      │    fac_region  [32 bytes]  × 4 = 128 bytes          │
                      │    reserved    [48 bytes]                           │
 +288                 ├╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌┤
                      │                                                     │
                      │              (erased 0xFF)                          │
                      │                                                     │
 SECTOR_SIZE/2        ╠═════════════════════════════════════════════════════╣
                      │                                                     │
                      │              (erased 0xFF)                          │
                      │                                                     │
 SECTOR_SIZE-32       ├─────────────────────────────────────────────────────┤
                      │  enc_confirm_t [32 bytes]                           │
 SECTOR_SIZE          └─────────────────────────────────────────────────────┘
━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━
bee_cfg_ctx_t (288 bytes, 16-byte aligned):
  [  0.. 31]  ekib                    (32 bytes)  AES-ECB encrypted KIB
  [  0.. 15]    aes_key               (16 bytes)  AES-128 key for BEE runtime decryption of execution slot
  [ 16.. 31]    iv                    (16 bytes)  AES Initial Vector for CBC encryption of PRDB
  [ 32..287]  eprdb                  (256 bytes)  AES-CBC encrypted PRDB (using aes_key + iv from KIB)
  [ 32.. 39]    tagl / tagh           (8 bytes)   fixed magic "TAG_EHDR"
  [ 40.. 43]    version               (4 bytes)   PRDB format version (0x56010000 = v1.0.0)
  [ 44.. 47]    fac_count             (4 bytes)   number of active FAC regions (1–3)
  [ 48..111]    enc_region           (64 bytes)   BEE-encrypted XIP region descriptor
  [ 48.. 51]      start              (4 bytes)    region start address, 4 kB aligned
  [ 52.. 55]      end                (4 bytes)    region end address, 4 kB aligned
  [ 56.. 59]      aes_mode           (4 bytes)    AES mode: 0 = ECB, 1 = CTR
  [ 60.. 63]      lock_option        (4 bytes)    BEE lock option
  [ 64.. 79]      nonce             (16 bytes)    upper 96 bits of AES-CTR counter (address field supplied by HW)
  [ 80..111]      reserved          (32 bytes)    padding / future use
  [112..143]    fac_region_0         (32 bytes)   FAC region: start / end / access mode (debug/read permissions)
  [144..175]    fac_region_1         (32 bytes)   FAC region (unused, zeroed)
  [176..207]    fac_region_2         (32 bytes)   FAC region (unused, zeroed)
  [208..239]    fac_region_3         (32 bytes)   FAC region (unused, zeroed)
  [240..287]    reserved            (48 bytes)    padding to reach exactly 256 bytes

enc_confirm_t (32 bytes):
  [  0.. 31]  magic                  (32 bytes)   written last in a separate flash page — confirms config block
                                                  was fully persisted; absence signals incomplete OTA update