Changelog RPMSG-Lite#
All notable changes to this project will be documented in this file.
The format is based on Keep a Changelog, and this project adheres to Semantic Versioning.
Unreleased#
Fixed#
Fixed MISRA C-2012 violations (Rules 14.4, 8.4, 5.8)
v5.5.0#
Added#
Added MCXE32B dual Cortex-M7 parts support.
Added
rpmsg_lite_are_all_buffers_consumed()API to report when all locally allocated TX buffers were consumed by the peer and returned to the local free buffer pool, with test coverage intests/03_send_receivefor both sides.Added i.MX937 parts support
Removed obsolete unused k32w1 platform layer
v5.4.1#
Fixed#
Corrected isr_counter3 handling in RT700 porting layer platform_deinit_interrupt implementation.
v5.4.0#
Added#
Added i.MX93W parts support
Added i.MX952 parts support
Added mcxl14x parts support
Added mcxw70 parts support
Zephyr rpmsg-lite samples add support for RT600 and RT700 DSP cores
Changed#
Port
platform_get_custom_shmem_configchange return value from uint32_t to int32_t for error handling consistency.
Fixed#
Updated unit tests code to allow correct GCOV code coverage measurement.
Added missing dsb instructions into all ISRs for cm4/cm7 based platform layers.
Fixed CERT EXP34-C by adding
__attribute__((noreturn))toRL_HANG(void)function.MISRA C-2012 Rule 14.3 compliance: Simplified
RL_WORD_ALIGN_UPandRL_WORD_ALIGN_DOWNmacros to eliminate invariant controlling expression violations (CID 5011148)Replaced ternary operator implementations with standard bitwise alignment idioms
Fixed hardcoded
4Uconstant inRL_WORD_ALIGN_UPto useRL_WORD_SIZEfor better portability
Fixed several MISRA compliance violations
v5.3.0#
Added#
RT700 porting layer added support to send rpmsg messages between CM33_0 <-> Hifi1 and CM33_1 <-> Hifi4 cores.
Add new platform macro
RL_PLATFORM_MAX_ISR_COUNTthis will set number of IRQ count per platform. This macro is then used in environment layers to set isr_table size where irq handles are registered. It size should match the bit length of VQ_ID so all combinations can fit into table.Unit tests updated to improve code coverage, new unit tests added covering static allocations in rtos environment layers.
Fixed#
virtio.h removed
typedef uint8_t booleanand in its place use standard C99booltype to avoid potential type conflicts.env_acquire_sync_lock() and env_release_sync_lock() synchronization primitives removed
Kconfig consolidation, when RL_ALLOW_CUSTOM_SHMEM_CONFIG enabled the platform_get_custom_shmem_config() function needs to be implemented in platform layer to provide custom shared memory configuration for RPMsg-Lite instance.
v5.2.1#
Added#
Doc added RPMSG-Lite VirtIO Overview
Doc added RPSMG-Lite Design Considerations
Added frdmimxrt1186 unit testing
Changed#
Remove limitation that
RL_BUFFER_SIZEneeds to be power of 2. It just has to be more than 16 bytes, e.g. 16 bytes of rpmsg header and payload size at least 1 byte and word aligned, if not it will be aligned up.
Fixed#
Fixed CERT-C INT31-C violation in platform_notify function in rpmsg_platform.c for imxrt700_m33, imxrt700_hifi4, imxrt700_hifi1 platforms
v5.2.0#
Added#
Add MCXL20 porting layer and unit testing
New utility macro
RL_CALCULATE_BUFFER_COUNT_DOWN_SAFEto safely determine maximum buffer count within shared memory while preventing integer underflow.RT700 platform add support for MCMGR in DSPs
Changed#
Change
rpmsg_platform.cto support new MCMGR APIImproved input validation in initialization functions to properly handle insufficient memory size conditions.
Refactored repeated buffer count calculation pattern for better code maintainability.
To make sure that remote has already registered IRQ there is required App level IPC mechanism to notify master about it
Fixed#
Fixed
env_wait_for_link_upfunction to handle timeout in link state checks for baremetal and qnx environment, RL_BLOCK mode can be used to wait indefinitely.Fixed CERT-C INT31-C violation by adding compile-time check to ensure
RL_PLATFORM_HIGHEST_LINK_IDremains within safe range for 16-bit casting in virtqueue ID creation.Fixed CERT-C INT30-C violations by adding protection against unsigned integer underflow in shared memory calculations, specifically in
shmem_length - (uint32_t)RL_VRING_OVERHEADandshmem_length - 2U * shmem_config.vring_sizeexpressions.Fixed CERT INT31-C violation in
platform_interrupt_disable()and similar functions by replacing unsafe cast fromuint32_ttoint32_twith a return of0constant.Fixed unsigned integer underflow in
rpmsg_lite_alloc_tx_buffer()where subtracting header size from buffer size could wrap around if buffer was too small, potentially leading to incorrect buffer sizing.Fixed CERT-C INT31-C violation in
rpmsg_lite.cwheresizeparameter was cast fromuint32_ttouint16_twithout proper validation.Applied consistent masking approach to both
sizeandflagsparameters:(uint16_t)(value & 0xFFFFU).This fix prevents potential data loss when size values exceed 65535.
Fixed CERT INT31-C violation in
env_memsetfunctions by explicitly convertingint32_tvalues to unsigned char using bit masking. This prevents potential data loss or misinterpretation when passing values outside the unsigned char range (0-255) to the standard memset() function.Fixed CERT-C INT31-C violations in RPMsg-Lite environment porting: Added validation checks for signed-to-unsigned integer conversions to prevent data loss and misinterpretation.
rpmsg_env_freertos.c: Added validation before converting int32_t to UBaseType_t.rpmsg_env_qnx.c: Fixed format string and added validation before assigning to mqstat fields.rpmsg_env_threadx.c: Added validation to prevent integer overflow and negative values.rpmsg_env_xos.c: Added range checking before casting to uint16_t.rpmsg_env_zephyr.c: Added validation before passing values to k_msgq_init.
Fixed a CERT INT31-C compliance issue in
env_get_current_queue_size()function where an unsigned queue count was cast to a signed int32_t without proper validation, which could lead to lost or misinterpreted data if queue size exceeded INT32_MAX.Fixed CERT INT31-C violation in
rpmsg_platform.cwherememcmp()return value (signed int) was compared with unsigned constant without proper type handling.Fixed CERT INT31-C violation in
rpmsg_platform.cwhere casting from uint32_t to uint16_t could potentially result in data loss. Changed length variable type from uint16_t to uint32_t to properly handle memory address differences without truncation.Fixed potential integer overflow in
env_sleep_msec()function in ThreadX environment implementation by rearranging calculation order in the sleep duration formula.Fixed CERT-C INT31-C violation in RPMsg-Lite where bitwise NOT operations on integer constants were performed in signed integer context before being cast to unsigned. This could potentially lead to misinterpreted data on
imx943platform.Added RL_MAX_BUFFER_COUNT (32768U) and RL_MAX_VRING_ALIGN (65536U) limit to ensure alignment values cannot contribute to integer overflow
Fixed CERT INT31-C violation in vring_need_event(), added cast to
uint16_tfor each operand.
v5.1.4 - 27-Mar-2025#
Added#
Add KW43B43 porting layer
Changed#
Doxygen bump to version 1.9.6
v5.1.3 - 13-Jan-2025#
Added#
Memory cache management of shared memory. Enable with
#define RL_USE_DCACHE (1)inrpmsg_config.hin case of data cache is used.Cmake/Kconfig support added.
Porting layers for imx95, imxrt700, mcmxw71x, mcmxw72x, kw47b42 added.
v5.1.2 - 08-Jul-2024#
Changed#
Zephyr-related changes.
Minor Misra corrections.
v5.1.1 - 19-Jan-2024#
Added#
Test suite provided.
Zephyr support added.
Changed#
Minor changes in platform and env. layers, minor test code updates.
v5.1.0 - 02-Aug-2023#
Added#
RPMsg-Lite: Added aarch64 support.
Changed#
RPMsg-Lite: Increased the queue size to (2 * RL_BUFFER_COUNT) to cover zero copy cases.
Code formatting using LLVM16.
Fixed#
Resolved issues in ThreadX env. layer implementation.
v5.0.0 - 19-Jan-2023#
Added#
Timeout parameter added to rpmsg_lite_wait_for_link_up API function.
Changed#
Improved debug check buffers implementation - instead of checking the pointer fits into shared memory check the presence in the VirtIO ring descriptors list.
VRING_SIZE is set based on number of used buffers now (as calculated in vring_init) - updated for all platforms that are not communicating to Linux rpmsg counterpart.
Fixed#
Fixed wrong RL_VRING_OVERHEAD macro comment in platform.h files
Misra corrections.
v4.0.0 - 20-Jun-2022#
Added#
Added support for custom shared memory arrangement per the RPMsg_Lite instance.
Introduced new rpmsg_lite_wait_for_link_up() API function - this allows to avoid using busy loops in rtos environments, GitHub PR #21.
Changed#
Adjusted rpmsg_lite_is_link_up() to return RL_TRUE/RL_FALSE.
v3.2.0 - 17-Jan-2022#
Added#
Added support for i.MX8 MP multicore platform.
Changed#
Improved static allocations - allow OS-specific objects being allocated statically, GitHub PR #14.
Aligned rpmsg_env_xos.c and some platform layers to latest static allocation support.
Fixed#
v3.1.2 - 16-Jul-2021#
Added#
Addressed MISRA 21.6 rule violation in rpmsg_env.h (use SDK’s PRINTF in MCUXpressoSDK examples, otherwise stdio printf is used).
Added environment layers for XOS.
Added support for i.MX RT500, i.MX RT1160 and i.MX RT1170 multicore platforms.
Fixed#
Fixed incorrect description of the rpmsg_lite_get_endpoint_from_addr function.
Changed#
Updated RL_BUFFER_COUNT documentation (issue #10).
Updated imxrt600_hifi4 platform layer.
v3.1.1 - 15-Jan-2021#
Added#
Introduced RL_ALLOW_CONSUMED_BUFFERS_NOTIFICATION config option to allow opposite side notification sending each time received buffers are consumed and put into the queue of available buffers.
Added environment layers for Threadx.
Added support for i.MX8QM multicore platform.
Changed#
Several MISRA C-2012 violations addressed.
v3.1.0 - 22-Jul-2020#
Added#
Added support for several new multicore platforms.
Fixed#
MISRA C-2012 violations fixed (7.4).
Fixed missing lock in rpmsg_lite_rx_callback() for QNX env.
Correction of rpmsg_lite_instance structure members description.
Address -Waddress-of-packed-member warnings in GCC9.
Changed#
Clang update to v10.0.0, code re-formatted.
v3.0.0 - 20-Dec-2019#
Added#
Added support for several new multicore platforms.
Fixed#
MISRA C-2012 violations fixed, incl. data types consolidation.
Code formatted.
v2.2.0 - 20-Mar-2019#
Added#
Added configuration macro RL_DEBUG_CHECK_BUFFERS.
Several MISRA violations fixed.
Added environment layers for QNX and Zephyr.
Allow environment context required for some environment (controlled by the RL_USE_ENVIRONMENT_CONTEXT configuration macro).
Data types consolidation.
v1.1.0 - 28-Apr-2017#
Added#
Supporting i.MX6SX and i.MX7D MPU platforms.
Supporting LPC5411x MCU platform.
Baremental and FreeRTOS support.
Support of copy and zero-copy transfer.
Support of static API (without dynamic allocations).