Encrypted XIP using OTFAD (On-The-Fly AES Decryption)#
This document extends the documentation of MCUboot and encrypted XIP in OTA examples and provides additional information related to the OTFAD module.
1. Introduction#
OTFAD is available on RT1160 and RT1170 devices and supports up to four independent encrypted regions, each with a separate AES-128 key and counter. In the OTA examples, OTFAD context 1 is used for encrypting the execution slot. Context 0 is reserved for the bootloader region configured by ROM.
OTFAD uses AES-128 in a custom CTR-like mode. The 128-bit input block fed to the AES engine is constructed per the device Security Reference Manual as follows:
[127:96] = BSWAP32(CTR_W0)
[ 95:64] = BSWAP32(CTR_W1)
[ 63:32] = BSWAP32(CTR_W0 ^ CTR_W1)
[ 31: 0] = systemAddress[31:4] | 0000b
Unlike standard AES-CTR (which increments the full 128-bit counter by 1 between blocks), OTFAD only increments the address field (bits[31:0]) between consecutive 16-byte blocks. The upper 96 bits — derived from CTR_W0 and CTR_W1 register values — remain constant across the entire protected region.
1.1 Key protection#
The OTFAD AES-128 key and CTR words are protected using a CAAM red blob. The blob mechanism uses the device-unique OTPMK (One-Time Programmable Master Key), which is provisioned by NXP at manufacturing and is never readable by software. CAAM uses the OTPMK internally to derive a blob encryption key as:
blob_key = KDF(OTPMK, key_modifier)
where key_modifier is a 16-byte random nonce generated alongside the secret and stored in plaintext in the metadata area. It acts as a domain separator, ensuring that each OTA update produces a cryptographically independent blob even on the same device.
The key selection is implicit — CAAM always uses the OTPMK for red blob operations. There is no fuse selection required.
Key protection options summary:
OTPMK
provisioned by NXP in factory
unique per device instance — prevents image cloning
never readable by software — CAAM uses it internally via SNVS
only supported option for OTFAD in the examples
Note: Engineering samples and some development boards may have a zero OTPMK. On such devices, CAAM blob operations will succeed but provide no security. Production devices with a properly burned OTPMK are required for a secure deployment.
1.2 Metadata structure#
Metadata Flash Sector
━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━
0 ┌─────────────────────────────────────────────────────┐
│ tag [4 bytes] │
+4 ├─────────────────────────────────────────────────────┤
│ key_modifier [16 bytes] │
+20 ├─────────────────────────────────────────────────────┤
│ blob [72 bytes] │
+92 ├─────────────────────────────────────────────────────┤
│ start_addr [4 bytes] │
+96 ├─────────────────────────────────────────────────────┤
│ end_addr [4 bytes] │
+100 ├─────────────────────────────────────────────────────┤
│ reserved [12 bytes] │
+112 ├╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌╌┤
│ │
│ (erased 0xFF) │
│ │
SECTOR_SIZE/2 ╠═════════════════════════════════════════════════════╣
│ │
│ (erased 0xFF) │
│ │
SECTOR_SIZE-32 ├─────────────────────────────────────────────────────┤
│ enc_confirm_t [32 bytes] │
SECTOR_SIZE └─────────────────────────────────────────────────────┘
━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━
The OTFAD metadata stored in the encryption metadata flash area consists of:
key_modifier: 16-byte random nonce (plaintext) — used as domain separator for CAAM blob
blob: 72-byte CAAM red blob — contains AES-128 key + CTR_W0 + CTR_W1 encrypted with OTPMK
start_addr / end_addr: system addresses of the OTFAD-protected XIP region
tag: 4-byte validity marker (
"OTFA")
otfad_cfg_ctx_t (112 bytes, 16-byte aligned):
[ 0.. 3] tag (4 bytes) "OTFA" validity marker
[ 4.. 19] key_modifier (16 bytes) random nonce, plaintext
[ 20.. 91] blob (72 bytes) CAAM red blob (OTPMK-protected)
[ 92.. 95] start_addr (4 bytes) OTFAD region start (system address)
[ 96.. 99] end_addr (4 bytes) OTFAD region end (system address)
[100..111] reserved (12 bytes) padding to 16-byte boundary
enc_confirm_t (32 bytes):
[ 0.. 31] magic (32 bytes) written last in a separate flash page — confirms config block
was fully persisted; absence signals incomplete OTA update
The blob itself has the following internal structure:
blob (72 bytes):
[ 0..31] header (32 bytes) CAAM key blob header
[32..55] encrypted secret (24 bytes) AES-encrypted {key[16] + ctr_w0[4] + ctr_w1[4]}
[56..71] MAC (16 bytes) authentication tag
1.3 OTA update flow#
On every OTA update, the extension:
Generates a fresh AES-128 key, CTR_W0, CTR_W1, and key_modifier via CAAM RNG
Encapsulates the secret into a CAAM red blob using OTPMK
Configures OTFAD context 1 for the primary slot region
Re-encrypts the incoming image page by page using the new key and counter
Persists the metadata (blob + key_modifier + addresses) to the encryption metadata flash area
On every boot, MCUboot:
Reads the metadata from the encryption metadata flash area
Decapsulates the CAAM blob to recover the AES key and CTR words (OTPMK never leaves CAAM hardware)
Loads the recovered key and counter into OTFAD context 1
Jumps to the application — OTFAD decrypts transparently on every flash read
1.4 Implementation#
The complete OTFAD initialization, encryption metadata handling, and image re-encryption are implemented in encrypted_xip_platform_otfad.c.
The implementation uses the following SDK drivers:
fsl_otfad— OTFAD context configurationfsl_caam— AES-ECB encryption, RNG, red blob encapsulation/decapsulationmflash_drv— IAP flash programming support
Additional information can be found in the Security Reference Manual of the target device (chapter OTFAD) and in the CAAM reference manual (chapter Blob Protocol).
2. Encryption of MCUboot partition (OVERWRITE_ONLY only)#
Encrypting the MCUboot partition is required only when a private key used for offline encryption is exposed in the bootloader code as a C array; otherwise it is optional. It is not necessary during the development phase.
To simplify the workflow, the MCUXpresso Secure Provisioning Tool (SEC tool) is used.
To provision the device and encrypt the bootloader perform the following steps:
Note: This setup applies to region 0 only. Region 1 is reserved for the execution slot and will be handled dynamically by the application code (out of ROM scope).
Erase the device
Build
mcuboot_opensourceGet the device into ISP mode
On development boards this is typically done by holding the ISP button and pressing the reset button
Open the SEC tool and create a new workspace for the RT11xx target device
Test the ISP connection in the SEC tool
Build Image
Boot: Encrypted (OTFAD) unsigned
Select the
mcuboot_opensourceoutput binary or ELF/OUT image as Source executable imageLifecycle: Open, HAB disabled
Configure OTFAD regions
Click OTFAD encryption
Total regions: 1 region - whole image
OTFAD KEK source: OTP
Generate random KEK, user key and counter for region 0 (see following image)
Configure Region 0 for the MCUboot partition as shown in the following image
Build image
Write image
Click Write image
Note: This operation provisions the device with the KEK permanently. No other fuses are burned, so the board remains usable for development purposes. A user still has to enable encrypted XIP boot (by the ROM) by switching bit BOOT_CFG[1] on the board’s DIP switch. It is also advised to save the SEC tool workspace (or at least the keys) for future use.