Dependency Installation CLI

The MCUXpresso Installer tool offers command-line support for installing available tools or checking the status of installed ones. The MCUXpressoInstallerCLI executable is included alongside the GUI executable on all operating systems.

Help command

  • -h, –help

  • Display help for commands.

Check updates command

  • –check-updates

  • Check if MCUXpresso Installer has updates.

Version command

  • -v, –version

  • Display the application version.

Install command

  • install | i

  • Used to install packages and components from MCUXpresso Installer.

Options:

  • -h, –help - display help for install command. Provides details about options and the choices for arguments.

MCUXpresso Installer - Install Help

  • -a, –all - install all packages available.

  • -p, –packages <packages…> - install one or more packages.

  • -c, –components <components…> - install one or more components.

  • -d, –dump [file] - export the installation log using json format.The user can provide the name of a new or existing json file. If the file is not provided, a reports directory is created in a default location (the MCUXpresso Installer installation path) and a new file is created there. This file can be used in automation systems to identify components installation status. In the file, there are two details provided:

    • envUpdate: marked as true when the MCUXpresso Installer added the component to the user’s PATH

    • exitCode: represents the installation status, 0 for success, non-zero integer for failure with corresponding error code.

  • –undo - undo the latest components installation

MCUXpresso Installer - Install Packages and Components MCUXpresso Installer - Install Packages and Components

List command

  • list | l

  • Used to give details about packages and components.

Options:

  • -h, –help - display help for list command. Provides details about options and the choices for arguments.

  • -a, –all - list all packages and the status of components.

  • -p, –packages <packages…> - this option has the possibility to see updates only for some packages.

  • -c, –components <components…> - this option has the possibility to see updates only for some components.

  • -d, –data - list the data from yaml files which contains the relation between packages and components

MCUXpresso Installer - List Packages and Components

  • -e, –export [path] - export the version report using json format. The user can provide the name of a new or existing json file. If the file is not provided, a reports directory is created in a default location (the MCUXpresso Installer installation path) and a new file is created there. This file can be used in automation systems to identify packages and components status. In the file, there are multiple details provided:

    • name: the name of the components

    • level:

      • “info” (no action needed)

      • “warn” (update available)

      • “error” (component not installed or it does not meet the required minimum version)

    • installedVersion: the highest version found

    • versionToBeInstalled: the version that can be installed using MCUXpresso Installer

{
    "MCUXpresso SDK Developer": [
      {
        "name": "CMake",
        "level": "error",
        "installedVersion": "3.28.1",
        "versionToBeInstalled": "3.30.0"
      },
      {
        "name": "Ninja",
        "level": "error",
        "installedVersion": "",
        "versionToBeInstalled": "1.12.1"
      },
      {
        "name": "Git",
        "level": "info",
        "installedVersion": "2.39.0",
        "versionToBeInstalled": "2.39.0"
      },
      {
        "name": "Arm GNU Toolchain Standalone add-ons",
        "level": "warn",
        "installedVersion": "13.2.1",
        "versionToBeInstalled": "13.2.4"
      },
      ...
    ]
}
  • -u, –updates - this option can be added to the command to show only the components that need updates.

MCUXpresso Installer - List updates from all packages

Note: The list command uses multiple colors to highlight the status of components:

  • default terminal color - the component is up to date

  • yellow - an update is available

  • gray

    • the component is not installed

    • the component is installed, but it does not meet the required minimum version

Note: The options that are using packages name as arguments supports multiple ways to format the package name

  • Full name “Arm GNU Toolchain” - make sure using double quotes when the package name has spaces.

  • Replace spaces with special characters or remove them to avoid using quotes - ArmGNUToolchain, Arm-GNU-Toolchain.

  • The names of the packages are case insensitive: arm-gnu-toolchain.

  • A package name can match multiple packages: “toolchain” can be used for “Arm GNU Toolchain” and “Standalone Toolchain Add-ons” at the same time.