NXP Matter Documentation Logo
v3.0

Matter MCU

  • Getting Started
    • Installation Guide for Matter with MCUX SDK
      • Install Software Tools
        • Alternative : MCUXpresso for VS Code
      • Install MCUX SDK with Matter support
        • Initializing a new workspace with MCUX SDK supporting Matter
        • Existing MCUX SDK workspace
      • Setup Matter Environment
    • Getting Started with Matter examples on NXP MCU platforms (MCUX SDK/FreeRTOS)
      • Prerequisites
      • Build Matter example
        • List the project information
        • Build the project
      • Flashing Matter example
        • Platform-specific requirements
          • NBU image (for MCXW71 and MCXW72 platforms)
        • Additional binaries for OTA and Factory Data
          • MCUboot bootloader (when OTA is enabled - RT1060, RT1170, and RW61x platforms)
          • Factory Data (when factory data is enabled)
          • Important note for MCUXpresso for VS Code Extension users
      • Testing Matter example
    • Supported Platforms
      • FreeRTOS-based platforms with MCUX SDK
        • Platform Support Matrix
        • How to Use This Information
      • Zephyr-based platforms
        • Platform Support Matrix
        • How to Use This Information
  • Development
    • Overview
    • Application Architecture
      • Overview
      • Application build system architecture
        • Matter stack and NXP platform port libraries
        • Application
          • Overview on application CMakeLists.txt
    • Application Customization
      • Overview
      • Prerequisites
      • Create a freestanding example from an existing Matter example
        • How to create a freestanding example
        • How to build a freestanding example
      • Customization options
        • Customize nxp_sdk_reconfig.cmake
        • Customize the application prj.conf
        • Customize SDK middleware configuration
        • Customize Matter Device Configuration with ZAP
          • Using ZAP Tool Script
          • Using ZAP Tool Directly
          • Generating Code After ZAP Changes
    • Integrate Matter as a service in an existing non-Matter application
      • Overview
      • Prerequisites
      • Build System Integration
        • Step 1 : Add Matter in the application CMakeLists.txt
          • Option A - Monolithic Architecture
          • Option B - Modular Architecture
        • Step 2 : Add Matter in the application Kconfig
        • Step 3 : Configure Matter in the application prj.conf
          • Locate or Create prj.conf
          • Configure Matter Settings
        • Step 4 : Update the example’s reconfig.cmake file
      • Code Integration
        • Step 5: Copy Matter application files under your project
        • Step 6: Configure Device Data Model
        • Step 7: Initialize Matter Stack
          • Important notes about initialization:
        • Step 8: Update your application linker file
          • Locate the correct linker template:
          • Integration options:
      • Next Steps
  • Release Notes & Known Issues
    • Release Notes v1.4.2.0.1
      • Release highlights
      • Version information
      • Development tools
      • Features and examples supported
        • FreeRTOS configurations
        • Zephyr configurations
      • Main changes compared to previous release (v1.4.0.2.1)
      • Memory footprint summary (Release mode)
    • Known Issues v1.4.2.0.1
      • Potential build issues
        • CMake build failure with multiple MCUX SDK versions
        • Windows path length limitations causing build failures
        • Kconfig string values not preserved when passed via “CMake Extra Args” (MCUXpresso for VS Code Extension)
        • Matter freestanding examples do not support –bf option
        • Matter Door Lock with Aliro integration example

MPU / Linux® Hosted Matter

  • User Guide
    • Quick Start
      • Introduction
      • i.MX MPU Matter platform
      • How to build the Yocto image with an integrated OpenThread Border Router
      • How to build OpenThread Border Router and OpenThread Daemon with Yocto SDK
      • How to set up OpenThread Border Router and OpenThread Daemon on the target
      • How to build Matter application
      • Security configuration for Matter
      • FAQ
    • Running Matter demos on i.MX MPU platforms
      • Hardware requirements
      • Software requirements
      • Running Matter demos with OTBR and OpenThread on the i.MX MPU platform
        • Setup OTBR on i.MX MPU platform
          • For i.MX93 FRDM / i.MX93 EVK / i.MX95 15x15 EVK + IW612 and i.MX91 EVK / i.MX91 QSB / i.MX91 FRDM + IW610 platform:
          • For i.MX 8M Mini EVK + 88W8987 + K32W platform or i.MX8ULP EVK + IW416 + K32W platform:
          • For i.MX6ULL EVK + 88W8987 + K32W platform:
        • Configure OpenThread Network
        • Factory reset lighting application on K32W DK6
        • Commission the lighting-app on the i.MX controller
        • Control the lighting-app on the i.MX controller
        • Setup ot-daemon on i.MX MPU platform
      • Running other Matter demos on i.MX MPU platform
        • Run example applications with ble-wifi commissioning method
          • Set up BT and connect to a wifi AP on controller device
          • Load the Wi-Fi/BT firmware and set up BT on the end device
          • Run the example application on the end device
          • Finally, commission and control the end devices on the controller device.
        • Run example applications with the on-network commissioning method
      • Running Matter OTA for Wi-Fi/BT firmware and application on the i.MX MPU platform
      • FAQ
        • Why chip-tool failed to control cluster after reboot?
    • Working with the chip-tool-web2
      • Source files
      • Building and running the chip-tool-web2
        • Building the chip-tool-web2
        • Running the chip-tool-web2
          • Introduction
          • Default Setup
          • Custom Setup
          • Verification
          • Accessing the chip-tool-web2
          • Example of opening on Windows
      • Using chip-tool-web2 to commission a Matter device
        • Using Interactive mode
        • Commissioning a Matter device
          • Add Thread Device
          • Add WI-FI Device
          • Add OnNetwork Device
          • Add Device by QRCode
      • List commissioned devices in chip-tool-web2
        • Interact with lighting device
        • Open Commissioning Window
        • Forget Device
        • Unpair Device
      • Subscription of Matter device OnOff cluster in chip-tool-web2
      • Controlling a Matter device media playback cluster
        • Launch or Stop app
        • Playback Control
        • Media Information
          • Report Format
      • Binding for light and switch Matter device
        • Write ACL
        • Write Binding
      • Opening the commissioning window for the commissioned Matter device
      • Controlling a Matter device Energy EVSE Cluster
        • EEVSE Event Trigger
        • EEVSE Charging Enable
        • EEVSE Write
        • EEVSE Charging Disable
        • EEVSE Status
          • Report Format
      • OTA updates on chip-tool-web2
        • Step 1 Upload OTA file
        • Step 2 Run chip-ota-provider-app
        • Step 3 Commissioning with chip-ota-provider-app
        • Step 4 Run chip-ota-requestor-app in the end devices
        • Step 5 Commissioning with chip-ota-requestor-app
        • Step 6 Write ACL
        • Step 7 Send OTA command
      • Network graph on chip-tool-web2
      • Additional Notes
    • Running Matter Commissioning in Home Assistant application on i.MX MPU platforms
      • Overview
      • Deploying the Docker containers on the i.MX MPU platform
      • Running the Home Assistant application on the Phone
      • Commissioning the i.MX Matter device on Home Assistant application
      • Known issues
      • FAQ
        • What to do if the download fails or the download speed of the Docker image is slow?
        • What to do if the commissioning fails?
        • What to do if the commissioning fails with matter-server logs “CHIP_ERROR [chip.native.DIS] Timeout waiting for mDNS resolution.”?
        • What should be done when an attempt to add the OpenThread Border Router’s REST API fails with a ‘Failed to connect’ error?
    • IWxxx Thread & Zigbee Dualpan solution in NXP i.MX Matter
      • Introduction
      • IWxxx Dualpan Architecture
      • IWxxx Zigbee Stack and Examples
        • Zigbee SDK
        • Zigbee Examples
          • Create a new Zigbee application
      • Matter to Zigbee Bridge Example
    • Running Matter MATTER-NCP demos on i.MX MPU platforms
      • Release Version Information
      • Hardware requirements
      • Verification about ble-wifi commissioning
      • Matter chip-tool control chip-all-clusters-app-ncp apps after matter commission successfully
  • Release Notes & Known Issues
    • Release Notes imx_matter_2026_q1
      • What’s new
    • Known Issues imx_matter_2026_q1
      • Known issues

Version

  • Version Information
    • Version Mapping Table
NXP Matter Documentation
  • Search


Copyright 2026 NXP. Document Version: v3.0 — March 2026

NXP Matter Documentation v: v3.0
Document Release Versions
v3.0
v2.0
v1.0
latest