Supported Platforms
This page lists the NXP MCU platforms that support Matter. Each platform has its own guide with detailed configuration information and hardware requirements.
FreeRTOS-based platforms with MCUX SDK
Platform Support Matrix
Platform |
Supported Boards |
Platform Guide |
|---|---|---|
RW612 |
FRDM-RW612, RD-RW612-BGA |
|
RT1060 |
RT1060-EVKB, RT1060-EVKC |
|
RT1170 |
RT1170-EVKB |
|
MCXW71 |
FRDM-MCXW71 |
|
MCXW72 |
FRDM-MCXW72, MCXW72-EVK |
To use the external secure element SE05x with RW612 for authentication, refer SE05x Guide.
How to Use This Information
Find your platform in the table above
Click the platform guide link for information on supported configurations and hardware requirements
For build and deployment instructions, follow our main Getting Started guide instead of the platform-specific build sections
Important: The platform guides are for reference only. Use them to understand your hardware and supported features, but follow the main project documentation for actual build and flash instructions.
Zephyr-based platforms
Platform Support Matrix
Platform |
Supported Boards |
Platform Guide |
|---|---|---|
RW612 |
FRDM-RW612, RD-RW612-BGA |
How to Use This Information
Follow the NXP Zephyr Guide link for complete setup, build, and testing instructions.