Running Matter Commissioning in Home Assistant application on i.MX MPU platforms
The Home Assistant (HA) application runs on both Android and iOS systems. By deploying the Home Assistant and Matter Server Docker containers on the i.MX MPU platform, you can use the HA application on the phone to manage Matter devices intuitively and easily. This document shows how to deploy the Home Assistant and Matter Server Docker containers on i.MX MPU platforms and then shows how to commission i.MX Matter devices in the HA application.
Overview
The i.MX MPU platforms support deploying the HA and matter-server Docker containers. As shown in the figure below, by deploying Docker containers on an i.MX device, the i.MX device becomes the HA server, and the HA application can access the HA server via URL. You can then perform the commissioning.
Figure. HA schematic diagram for i.MX MPU platform
Deploying the Docker containers on the i.MX MPU platform
First download and deploy the Docker containers on an i.MX MPU platform.
Download and deploy the homeassistant and matter-server Docker images.
$ docker run -d --name homeassistant --privileged --restart=unless-stopped -e TZ=MY_TIME_ZONE -v $(pwd)/config:/config -v /run/dbus:/run/dbus:ro --network=host ghcr.io/home-assistant/home-assistant:2026.3
$ docker run -d --name matter-server --restart=unless-stopped --security-opt apparmor=unconfined -v $(pwd)/data:/data --network=host ghcr.io/home-assistant-libs/python-matter-server:8.1.0 --storage-path /data --paa-root-cert-dir /data/credentials
It takes a few minutes to download and deploy the images. You can check the images by running “$ docker image” after the deployment is complete.
root@imx93evk-iwxxx-matter:~# docker images
REPOSITORY TAG IMAGE ID CREATED SIZE
ghcr.io/home-assistant/home-assistant 2026.3 0e091dfce306 3 days ago 3.29GB
ghcr.io/home-assistant-libs/python-matter-server 8.1.0 170aa093ce91 6 months ago 644MB
Running the Home Assistant application on the Phone
Before running the HA application, you need to perform some environmental configuration. First, you can use the commands below to connect to the Wi-Fi AP on the i.MX Docker device and check its IP address.
$ wpa_passphrase ${SSID} ${PASSWORD} > wifiap.conf
$ ifconfig eth0 down
$ modprobe moal mod_para=nxp/wifi_mod_para.conf
$ wpa_supplicant -d -B -i mlan0 -c ./wifiap.conf
$ sleep 5
$ modprobe btnxpuart
$ hciconfig hci0 up
$ ifconfig mlan0 # check IP address
If you need to commission a Thread device in HA, setup OTBR on the i.MX Docker device.
Then, connect to the same Wi-Fi AP, enable Bluetooth on your phone, and open the HA app on your phone and configure the HA server URL.
If you are a new user of this application, you can set the URL when you log in to this application. Enter the URL and click the “Connect” button. The URL should be in the format http://<IP_ADDRESS>:8123 , where <IP_ADDRESS> is the IP address of your i.MX device.
Figure. Configuring the Home Assistant server URL when logging in
Or you can configure the URL in the settings according to the below steps, click the “SETTINGS”, “Home”, “Home Assistant URL” buttons in sequence on the following page to update the URL.
Figure. Configuring the Home Assistant server URL in Settings
Once you have connected the Home Assistant server, you should integrate the Python Matter server to communicate with the i.MX Matter device. You will also need to integrate the Thread and OpenThread Border Router server if you need to commission the Matter Thread device.
Integrate the Python Matter server into the Phone application:
Click “Setting” – “Devices & services” – “+ Add integration” at the bottom-right corner – search for “Matter” – select the “Matter” – enter URL “ws://localhost:5580/ws” – “Submit” to integrate Python Matter Server.
Figure. Integrate the Python Matter server
Integrate the Thread service into the HA instance:
Click “Setting” – “Devices & services” – “+ Add integration” at the bottom-right corner – search for “Thread” - select the “Thread”. The Thread service is added to HA instance as shown below.
Figure. Integrate the Thread service
Integrate the Open Thread Border Router REST API into HA instance:
Click “Setting” – “Devices & services” – “+ Add integration” at the bottom-right corner - search for “Open Thread Border Router” - select the “Open Thread Border Router” – Enter URL “http://ip:8081” (IP is the otbr-agent device’s IP, it uses 8081 port for REST API by default) – Submit, the Open Thread Border Router REST API will add into HA instance.
Figure. Integrate the Thread Border Router
Set the preferred network and sync Thread credentials.
Go to “Setting” - “Devices & services” - “Thread” - click the configuration logo - set or check the right border router as the preferred network. Then, go to “Setting” – “Companion app” – “Troubleshooting” – “Sync Thread credentials” to Sync the credentials.
Figure. Setting the preferred network and sync the Thread credentials.
Commissioning the i.MX Matter device on Home Assistant application
This chapter shows how to commission an i.MX Matter device on HA application.
First, set up the i.MX Matter device. There are two ways to run the Matter application. Take the chip-lighting-app as an example. You can also setup the Matter application on a Thread device.
Run the commands below if the i.MX Matter device is i.MX93 or i.MX91 to enable the ELE. For other boards, proceed to Option 1 or Option 2.
$ systemctl enable nvm_daemon
$ systemctl start nvm_daemon
$ systemctl status nvm_daemon # make sure the daemon active and running.
Option 1
$ wpa_passphrase ${SSID} ${PASSWORD} > wifiap.conf
$ ifconfig eth0 down
$ ifconfig eth1 down
$ modprobe moal mod_para=nxp/wifi_mod_para.conf
$ wpa_supplicant -d -B -i mlan0 -c ./wifiap.conf
$ sleep 5
$ modprobe btnxpuart
$ hciconfig hci0 up
$ chip-lighting-app
Option 2
$ ifconfig eth0 down
$ ifconfig eth1 down
$ modprobe moal mod_para=nxp/wifi_mod_para.conf
$ modprobe btnxpuart
$ hciconfig hci0 up
$ chip-lighting-app --wifi --ble-device 0
After running the chip-lighting-app, you will find a log line similar to the one below, copy the URL and open it in a browser, you can see the QR code of this Matter application.
CHIP:SVR: https://project-chip.github.io/connectedhomeip/qrcode.html?data=MT%3A-24J042C00KA0648G00
Then, you can commission i.MX Matter application as shown in the following pictures. Click the “Settings”, “Devices & services”, “+ Add integration”, “Add Matter device”, “No, it’s new.”, “Open camera here” buttons in sequence on the following pages to start scanning the QR code of the i.MX Matter application.
Figure. How to start the commissioning on the phone app
Once the QR code is scanned, it goes through the following processes to connect to the i.MX Matter application chip-lighting-app.
Figure. Device connection procedure
Once the device has been successfully connected, you are able to control it.
Known issues
When commissioning with the chip-all-cluster-app, you may encounter a “Something went wrong” error in the final steps of the commissioning process on the Home Assistant app. This is a known issue related to the Home Assistant Docker environment.
FAQ
What to do if the download fails or the download speed of the Docker image is slow?
The download failure or slow download speed may be caused by network issues. Use the following commands to set the proxies for the Docker service. Then retry to download and deploy the Docker image again.
$ mkdir /etc/systemd/system/docker.service.d
$ vi /etc/systemd/system/docker.service.d/http-proxy.conf
[Service]
Environment="HTTP_PROXY=${YOUR_HTTP_PROXY_URL}:${YOUR_HTTP_PROXY_PORT}"
Environment="HTTPS_PROXY=${YOUR_HTTPS_PROXY_URL}:${YOUR_HTTPS_PROXY_PORT}"
Environment="NO_PROXY=localhost,127.0.0.*,${YOUR_HOST_network_prefix}.*"
$ systemctl daemon-reload
$ systemctl restart docker
What to do if the commissioning fails?
Check the status of the Docker service, and the network status and the status of the Bluetooth interface.
$ systemctl status docker # check the Docker service status
$ systemctl start docker # start the Docker service
$ ifconfig mlan0 # check the Network status
$ hciconfig hci0 # check the Bluetooth status
You need to make sure that the Docker service is active, an IP has been assigned to the mlan0 interface, and that hci0 is up and running.
root@imx93evk-iwxxx-matter:~# systemctl status docker
* docker.service - Docker Application Container Engine
Loaded: loaded (8;;file://imx93evk-iwxxx-matter/usr/lib/systemd/system/docker.service/usr/lib/systemd/system/docker.service8;;; disabled; preset: disabled)8;;
Active: active (running) since Tue 2024-10-22 07:09:36 UTC; 36s ago
TriggeredBy: * docker.socket
Docs: 8;;https://docs.docker.comhttps://docs.docker.com8;;8;;
Main PID: 681 (dockerd)
Tasks: 12
Memory: 98.1M (peak: 100.0M)
CPU: 1.345s
CGroup: /system.slice/docker.service
`-681 /usr/bin/dockerd -H fd:// --containerd=/run/containerd/containerd.sock
root@imx93evk-iwxxx-matter:~# ifconfig mlan0
mlan0: flags=4163<UP,BROADCAST,RUNNING,MULTICAST> mtu 1500
inet 192.168.3.119 netmask 255.255.254.0 broadcast 192.168.3.255
inet6 2001:470:11e:f:a2cd:f3ff:fe77:e72e prefixlen 64 scopeid 0x0<global>
inet6 fe80::a2cd:f3ff:fe77:e72e prefixlen 64 scopeid 0x20<link>
ether a0:cd:f3:77:e7:2e txqueuelen 1000 (Ethernet)
RX packets 2766 bytes 184053 (179.7 KiB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 643 bytes 71774 (70.0 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
root@imx93evk-iwxxx-matter:~# hciconfig hci0
hci0: Type: Primary Bus: UART
BD Address: A0:CD:F3:77:E7:2F ACL MTU: 1021:7 SCO MTU: 120:6
UP RUNNING
RX bytes:849 acl:0 sco:0 events:57 errors:0
TX bytes:1078 acl:0 sco:0 commands:57 errors:0
If the device is connected to a network cable, use the following command to turn off the Ethernet interface.
$ ifconfig eth0 down
What to do if the commissioning fails with matter-server logs “CHIP_ERROR [chip.native.DIS] Timeout waiting for mDNS resolution.”?
When commissioning device over BLE or IP failures occur, especially when OTBR is set up. You need to check the matter-server container’s logs by “$ docker logs matter-server”, if the logs include “CHIP_ERROR [chip.native.DIS] Timeout waiting for mDNS resolution”, you can try to resolve this issue by running below commands to clear avahi cache then retry the commissioning process.
$ sudo systemctl stop avahi-daemon
$ sudo rm -rf /var/run/avahi-daemon/*
$ sudo systemd-resolve --flush-caches
$ sudo systemctl start avahi-daemon
What should be done when an attempt to add the OpenThread Border Router’s REST API fails with a ‘Failed to connect’ error?
Add the option “–rest-listen-address 0.0.0.0” when starting otbr-agent or otbr-agent-iwxxx, for example:”
$ otbr-agent-iwxxx -I wpan0 -B mlan0 --rest-listen-address 0.0.0.0 spinel+spi:///dev/spidev0.0?gpio-reset-device=/dev/gpiochip5&gpio-int-device=/dev/gpiochip4&gpio-int-line=10&gpio-reset-line=1&spi-mode=0&spi-speed=1000000&spi-reset-delay=0