NXP Matter Documentation Logo
v3.0

Matter MCU

  • Getting Started
    • Installation Guide for Matter with MCUX SDK
      • Install Software Tools
        • Alternative : MCUXpresso for VS Code
      • Install MCUX SDK with Matter support
        • Initializing a new workspace with MCUX SDK supporting Matter
        • Existing MCUX SDK workspace
      • Setup Matter Environment
    • Getting Started with Matter examples on NXP MCU platforms (MCUX SDK/FreeRTOS)
      • Prerequisites
      • Build Matter example
        • List the project information
        • Build the project
      • Flashing Matter example
        • Platform-specific requirements
          • NBU image (for MCXW71 and MCXW72 platforms)
        • Additional binaries for OTA and Factory Data
          • MCUboot bootloader (when OTA is enabled - RT1060, RT1170, and RW61x platforms)
          • Factory Data (when factory data is enabled)
          • Important note for MCUXpresso for VS Code Extension users
      • Testing Matter example
    • Supported Platforms
      • FreeRTOS-based platforms with MCUX SDK
        • Platform Support Matrix
        • How to Use This Information
      • Zephyr-based platforms
        • Platform Support Matrix
        • How to Use This Information
  • Development
    • Overview
    • Application Architecture
      • Overview
      • Application build system architecture
        • Matter stack and NXP platform port libraries
        • Application
          • Overview on application CMakeLists.txt
    • Application Customization
      • Overview
      • Prerequisites
      • Create a freestanding example from an existing Matter example
        • How to create a freestanding example
        • How to build a freestanding example
      • Customization options
        • Customize nxp_sdk_reconfig.cmake
        • Customize the application prj.conf
        • Customize SDK middleware configuration
        • Customize Matter Device Configuration with ZAP
          • Using ZAP Tool Script
          • Using ZAP Tool Directly
          • Generating Code After ZAP Changes
    • Integrate Matter as a service in an existing non-Matter application
      • Overview
      • Prerequisites
      • Build System Integration
        • Step 1 : Add Matter in the application CMakeLists.txt
          • Option A - Monolithic Architecture
          • Option B - Modular Architecture
        • Step 2 : Add Matter in the application Kconfig
        • Step 3 : Configure Matter in the application prj.conf
          • Locate or Create prj.conf
          • Configure Matter Settings
        • Step 4 : Update the example’s reconfig.cmake file
      • Code Integration
        • Step 5: Copy Matter application files under your project
        • Step 6: Configure Device Data Model
        • Step 7: Initialize Matter Stack
          • Important notes about initialization:
        • Step 8: Update your application linker file
          • Locate the correct linker template:
          • Integration options:
      • Next Steps
  • Release Notes & Known Issues
    • Release Notes v1.4.2.0.1
      • Release highlights
      • Version information
      • Development tools
      • Features and examples supported
        • FreeRTOS configurations
        • Zephyr configurations
      • Main changes compared to previous release (v1.4.0.2.1)
      • Memory footprint summary (Release mode)
    • Known Issues v1.4.2.0.1
      • Potential build issues
        • CMake build failure with multiple MCUX SDK versions
        • Windows path length limitations causing build failures
        • Kconfig string values not preserved when passed via “CMake Extra Args” (MCUXpresso for VS Code Extension)
        • Matter freestanding examples do not support –bf option
        • Matter Door Lock with Aliro integration example

MPU / Linux® Hosted Matter

  • User Guide
    • Quick Start
      • Introduction
      • i.MX MPU Matter platform
      • How to build the Yocto image with an integrated OpenThread Border Router
      • How to build OpenThread Border Router and OpenThread Daemon with Yocto SDK
      • How to set up OpenThread Border Router and OpenThread Daemon on the target
      • How to build Matter application
      • Security configuration for Matter
      • FAQ
    • Running Matter demos on i.MX MPU platforms
      • Hardware requirements
      • Software requirements
      • Running Matter demos with OTBR and OpenThread on the i.MX MPU platform
        • Setup OTBR on i.MX MPU platform
          • For i.MX93 FRDM / i.MX93 EVK / i.MX95 15x15 EVK + IW612 and i.MX91 EVK / i.MX91 QSB / i.MX91 FRDM + IW610 platform:
          • For i.MX 8M Mini EVK + 88W8987 + K32W platform or i.MX8ULP EVK + IW416 + K32W platform:
          • For i.MX6ULL EVK + 88W8987 + K32W platform:
        • Configure OpenThread Network
        • Factory reset lighting application on K32W DK6
        • Commission the lighting-app on the i.MX controller
        • Control the lighting-app on the i.MX controller
        • Setup ot-daemon on i.MX MPU platform
      • Running other Matter demos on i.MX MPU platform
        • Run example applications with ble-wifi commissioning method
          • Set up BT and connect to a wifi AP on controller device
          • Load the Wi-Fi/BT firmware and set up BT on the end device
          • Run the example application on the end device
          • Finally, commission and control the end devices on the controller device.
        • Run example applications with the on-network commissioning method
      • Running Matter OTA for Wi-Fi/BT firmware and application on the i.MX MPU platform
      • FAQ
        • Why chip-tool failed to control cluster after reboot?
    • Working with the chip-tool-web2
      • Source files
      • Building and running the chip-tool-web2
        • Building the chip-tool-web2
        • Running the chip-tool-web2
          • Introduction
          • Default Setup
          • Custom Setup
          • Verification
          • Accessing the chip-tool-web2
          • Example of opening on Windows
      • Using chip-tool-web2 to commission a Matter device
        • Using Interactive mode
        • Commissioning a Matter device
          • Add Thread Device
          • Add WI-FI Device
          • Add OnNetwork Device
          • Add Device by QRCode
      • List commissioned devices in chip-tool-web2
        • Interact with lighting device
        • Open Commissioning Window
        • Forget Device
        • Unpair Device
      • Subscription of Matter device OnOff cluster in chip-tool-web2
      • Controlling a Matter device media playback cluster
        • Launch or Stop app
        • Playback Control
        • Media Information
          • Report Format
      • Binding for light and switch Matter device
        • Write ACL
        • Write Binding
      • Opening the commissioning window for the commissioned Matter device
      • Controlling a Matter device Energy EVSE Cluster
        • EEVSE Event Trigger
        • EEVSE Charging Enable
        • EEVSE Write
        • EEVSE Charging Disable
        • EEVSE Status
          • Report Format
      • OTA updates on chip-tool-web2
        • Step 1 Upload OTA file
        • Step 2 Run chip-ota-provider-app
        • Step 3 Commissioning with chip-ota-provider-app
        • Step 4 Run chip-ota-requestor-app in the end devices
        • Step 5 Commissioning with chip-ota-requestor-app
        • Step 6 Write ACL
        • Step 7 Send OTA command
      • Network graph on chip-tool-web2
      • Additional Notes
    • Running Matter Commissioning in Home Assistant application on i.MX MPU platforms
      • Overview
      • Deploying the Docker containers on the i.MX MPU platform
      • Running the Home Assistant application on the Phone
      • Commissioning the i.MX Matter device on Home Assistant application
      • Known issues
      • FAQ
        • What to do if the download fails or the download speed of the Docker image is slow?
        • What to do if the commissioning fails?
        • What to do if the commissioning fails with matter-server logs “CHIP_ERROR [chip.native.DIS] Timeout waiting for mDNS resolution.”?
        • What should be done when an attempt to add the OpenThread Border Router’s REST API fails with a ‘Failed to connect’ error?
    • IWxxx Thread & Zigbee Dualpan solution in NXP i.MX Matter
      • Introduction
      • IWxxx Dualpan Architecture
      • IWxxx Zigbee Stack and Examples
        • Zigbee SDK
        • Zigbee Examples
          • Create a new Zigbee application
      • Matter to Zigbee Bridge Example
    • Running Matter MATTER-NCP demos on i.MX MPU platforms
      • Release Version Information
      • Hardware requirements
      • Verification about ble-wifi commissioning
      • Matter chip-tool control chip-all-clusters-app-ncp apps after matter commission successfully
  • Release Notes & Known Issues
    • Release Notes imx_matter_2026_q1
      • What’s new
    • Known Issues imx_matter_2026_q1
      • Known issues

Version

  • Version Information
    • Version Mapping Table
NXP Matter Documentation
  • Getting Started

Matter on NXP MCU platforms

This section provides comprehensive guidance for developers working with Matter on NXP’s MCU platforms. Whether you’re just getting started or looking to customize advanced features, you’ll find step-by-step instructions, architectural insights, and troubleshooting tips to support your MCU development journey.

Getting Started

Getting Started

  • Installation Guide for Matter with MCUX SDK
    • Install Software Tools
    • Install MCUX SDK with Matter support
    • Setup Matter Environment
  • Getting Started with Matter examples on NXP MCU platforms (MCUX SDK/FreeRTOS)
    • Prerequisites
    • Build Matter example
    • Flashing Matter example
    • Testing Matter example
  • Supported Platforms
    • FreeRTOS-based platforms with MCUX SDK
    • Zephyr-based platforms

Development

Development

  • Overview
  • Application Architecture
    • Overview
    • Application build system architecture
  • Application Customization
    • Overview
    • Prerequisites
    • Create a freestanding example from an existing Matter example
    • Customization options
  • Integrate Matter as a service in an existing non-Matter application
    • Overview
    • Prerequisites
    • Build System Integration
    • Code Integration
    • Next Steps

Release Notes & Known Issues

Release Notes & Known Issues

  • Release Notes v1.4.2.0.1
    • Release highlights
    • Version information
    • Development tools
    • Features and examples supported
    • Main changes compared to previous release (v1.4.0.2.1)
    • Memory footprint summary (Release mode)
  • Known Issues v1.4.2.0.1
    • Potential build issues
Previous Next

Copyright 2026 NXP. Document Version: v3.0 — March 2026

NXP Matter Documentation v: v3.0
Document Release Versions
v3.0
v2.0
v1.0
latest