What is new
MCUXpresso SDK version 24.12.00-pvw2 is an early adopter release provided as preview for early development.
The following changes have been implemented compared to the previous SDK release version (2.16.100).
Bluetooth LE host stack and applications
Added initial experimental support for Bluetooth LE host feature: Periodic Advertising with Responses (PAwR)
Added initial experimental support for Bluetooth LE host feature: Encrypted Advertising Data (EAD)
Minor fixes and stability improvements
Bluetooth LE controller
Added initial experimental support for Bluetooth LE Controller feature: Periodic Advertising with Responses (PAwR)\
Minor fixes and stability improvements
Transceiver Drivers (XCVR)
Added API to control PA ramp type and duration
Connectivity framework
Major Changes (User Applications may be impacted)
Supporting CMake/Kconfig for SDK 24.12.00: user shall now use
CmakeLists.txtandKconfigfiles from root folder. Compilation should be done usingwest buildcommand. In order to see the Framework Kconfig, use commandwest build -t guiconfigBoard files and linker scripts moved to examples repository
Bugfixes
[platform lowpower]
Entering Deep down power mode will no longer call
PLATFORM_EnterPowerDown(). This API is now called only when going to Power down mode
Platform specific
Deep sleep mode is supported.
Power down mode is supported in low power reference design applications as experimental.
XTAL32K-less support using FRO32K is experimental
FRO32K notifications callback is debug only and should not be used for final product firmware builds
Overal folder restructuring for SDK 24.12.00
[Platform]:
Renamed platform family from
connected_mcu/nbutowireless_mcu/nbuPlatform families have now dedicated
fwk_config.h,rpmsg_config.handSecLib_mbedtls_config.h
[Services]:
Moved all framework services in a common directory
services
Zigbee and IEEE 802.15.4
Minor fixes for Zigbee PRO R22 configuration.
Zigbee Pro 2023 Configuration is not supported in this release.