Architect
Introduction
The MCUXpresso Software Development Kit (SDK) provides comprehensive software support for Kinetis and LPC Microcontrollers. The MCUXpresso SDK includes a flexible set of peripheral drivers designed to speed up and simplify development of embedded applications. Along with the peripheral drivers, the MCUXpresso SDK provides an extensive and rich set of example applications covering everything from basic peripheral use case examples to full demo applications. The MCUXpresso SDK contains FreeRTOS, a USB host and device stack, and various other middleware to support rapid development.
The MCUXpresso SDK architecture consists of five key components listed below.
The Arm Cortex Microcontroller Software Interface Standard (CMSIS) CORE compliance device-specific header files, SOC Header, and CMSIS math/DSP libraries.
Peripheral Drivers
Components
Real-time Operating Systems (RTOS)
Stacks and Middleware that integrate with the MCUXpresso SDK
Demo Applications based on the MCUXpresso SDK

CMSIS Support
Along with the SoC header files and peripheral extension header files, the MCUXpresso SDK also includes common CMSIS header files for the Arm Cortex-M core and the math and DSP libraries from the latest CMSIS release. The CMSIS DSP library source code is also included for reference. Content in CMSIS Folder are got from the standard ARM CMSIS Core release.
SoC Support - Header File/Drivers/Startup/Linker…
Each device get a seperate folder to let different devices files can be in same SDK package. For example, MIMXRT1052 is one of the device for RT105X family. It get its only folder inside devices folder.
MCU header files
Each supported MCU device in the MCUXpresso SDK has an overall System-on Chip (SoC) memory-mapped header file. This header file contains the memory map and register base address for each peripheral and the IRQ vector table with associated vector numbers. The overall SoC header file provides a access to the peripheral registers through pointers and predefined bit masks. In addition to the overall SoC memorymapped header file, the MCUXpresso SDK includes a feature header file for each device. The feature header file allows NXP to deliver a single software driver for a given peripheral. The feature file ensures that the driver is properly compiled for the target SOC.
MCU Header files is located in devices/<DEVICE_NAME>/<DEVICE_NAME>.h
The MCU Header files are not hand-written. It is generated from Chip Model data. To add a not supported device in SDK, developer need firstly ensure the Chip Model stuff be prepared/generated.
Feature Header Files
The peripheral drivers are designed to be reusable regardless of the peripheral functional differences from one MCU device to another. An overall Peripheral Feature Header File is provided for the MCUXpresso SDK-supported MCU device to define the features or configuration differences for each sub-family device.
Startup codes, Linker file
Startup codes provide the startup functions, assembly codes to support the SoC to run from the Power-Up to the main() function. The codes usually do with the work like setup stack, configure watchdog, do with global variables and so on. startup codes are devices/<DEVICE_NAME>/system_<DEVICE_NAME>.c/h, devices/<DEVICE_NAME>/<TOOLCHAIN>/startup_<DEVICE_NAME>.s/S files.
Linker file are provided for each toolchain. User can find it from devices/<DEVICE_NAME>/<TOOLCHAIN>/<>.scf. The postfix of the linker file varies from toolchain to toolchain.
Peripheral Drivers
Peripheral Drivers are locatd in devices//<DEVICE_NAME>/drivers.
The MCUXpresso SDK peripheral drivers mainly consist of low-level functional APIs for the MCU product family on-chip peripherals and also of high-level transactional APIs for some bus drivers/DMA driver/eDMA driver to quickly enable the peripherals and perform transfers.
All MCUXpresso SDK peripheral drivers only depend on the CMSIS headers, device feature files, fsl_common.h, and fsl_clock.h files so that users can easily pull selected drivers and their dependencies into projects. With the exception of the clock/power-relevant peripherals, each peripheral has its own driver. Peripheral drivers handle the peripheral clock gating/ungating inside the drivers during initialization and deinitialization respectively.
Low-level functional APIs provide common peripheral functionality, abstracting the hardware peripheral register accesses into a set of stateless basic functional operations. These APIs primarily focus on the control, configuration, and function of basic peripheral operations. The APIs hide the register access details and various MCU peripheral instantiation differences so that the application can be abstracted from the low-level hardware details. The API prototypes are intentionally similar to help ensure easy portability across supported MCUXpresso SDK devices.
Transactional APIs provide a quick method for customers to utilize higher-level functionality of the peripherals. The transactional APIs utilize interrupts and perform asynchronous operations without user intervention. Transactional APIs operate on high-level logic that requires data storage for internal operation context handling. However, the Peripheral Drivers do not allocate this memory space. Rather, the user passes in the memory to the driver for internal driver operation.
Transactional APIs ensure the NVIC is enabled properly inside the drivers. The transactional APIs do not meet all customer needs, but provide a baseline for development of custom user APIs.Note that the transactional drivers never disable an NVIC after use. This is due to the shared nature of interrupt vectors on devices. It is up to the user to ensure that NVIC interrupts are properly disabled after usage is complete.
Interrupt handling for transactional APIs
A double weak mechanism is introduced for drivers with transactional API. The double weak indicates two levels of weak vector entries. See the examples below:
PUBWEAK SPI0_IRQHandler
PUBWEAK SPI0_DriverIRQHandler
SPI0_IRQHandler
LDR R0, =SPI0_DriverIRQHandler
BX R0
The first level of the weak implementation are the functions defined in the vector table. In the devices/<DEVICE_NAME>/<TOOLCHAIN>/startup_<DEVICE_NAME>.s/.S file, the implementation of the first layer weak function calls the second layer of weak function. The implementation of the second layer weak function (ex. SPI0_DriverIRQHandler) jumps to itself (B .). The MCUXpresso SDK drivers with transactional APIs provide the reimplementation of the second layer function inside of the peripheral driver. If the MCUXpresso SDK drivers with transactional APIs are linked into the image, the SPI0_DriverIRQHandler is replaced with the function implemented in the MCUXpresso SDK SPI driver.
The reason for implementing the double weak functions is to provide a better user experience when using the transactional APIs. For drivers with a transactional function, call the transactional APIs and the drivers complete the interrupt-driven flow. Users are not required to redefine the vector entries out of the box. At the same time, if users are not satisfied by the second layer weak function implemented in the MCUXpresso SDK drivers, users can redefine the first layer weak function and implement their own interrupt handler functions to suit their implementation.
The limitation of the double weak mechanism is that it cannot be used for peripherals that share the same vector entry. For this use case, redefine the first layer weak function to enable the desired peripheral interrupt functionality. For example, if the MCU’s UART0 and UART1 share the same vector entry, redefine the UART0_UART1_IRQHandler according to the use case requirements.
RTOS Driver
SDK provide the bus communication driver integrated with native FreeRTOS services. These drivers are called as RTOS driver and provide the sync transfer APIs. User can directly call these APIs in FreeRTOS applications. RTOS drivers are located in same folder of Peripheral Drivers with the freertos in the file name. For example, devices\MIMXRT1052\drivers\fsl_lpi2c_freertos.c/h.
CMSIS Driver
SDK provide CMSIS driver support for all the variants of I2C/UART/SPI peripheral. Different than the way proposed by ARM to configure the PINMUX configuration by passing a set of macros in RTE_Device.h file, SDK CMSIS driver implementation will use the pin mux configuration APIs generated by pinmux tool in pinmux.c files.
Project Template
See description for Project Template in application parts. Comparing to the board level project template, project template in device level are for user scenartio that to create new project with a given device.
Components
SDK provide the components folder in the root directory storing these sensor driver, common software components and so on.
On-Board Device driver
Sensor, PMIC, PHY, Audio Codec which are soldered in the evaluation board will be supported in the SDK. Usually, there drivers can be connected to different variants of the peripheral driver in SoC to make it work. For example, Audio codec can be connected to I2C/LPI2C peripherals.
To ease the porting effort for the same device supporting work with different SoC(Which usually means different variants of peripheral), these device driver will not be implemented bind to specific peripheral like I2C or LPI2C. Instead, it require the application to provide function pointer which is prepared outside of the device driver and device driver can use these APIs to do the data write/read and so on. Device driver don’t care about how these functions pointers are implemented. application can use all variants of way to implement these functions pointer. For example, user can use the CMSIS Driver to implement it or user even can use the raw register read/write to implement it. One important thing to be note here is the initialization/de-initialization of these peripherals will not be done inside the device driver to avoid the race-condition. For example, Audio Codec A and Audio Codec B all use the same I2C. A don’t know the status of B. If A call the de-initialization of I2C, the B’s work may be broken.
Common Software Component
Common software component which are not middleware/stacks will also be placed to this folder. For example, the NAND Flash Component which implement the common NAND flash logic operation. Another example is the application timer. SDK now integrated a lot of stack/middleware inside/outside BL/BU/NXP and some of the middleware/stack provide these kinds of the software components. If certain software component inside these middleware/stack are also requested in other cases, these components will be split out from these middleware/stacks and move to this part if there is no license issue.
Middleware and RTOS
Middle-wares are provided in the directory of middleware folder provided various middleware support.
RTOS are provided in the directory of rtos folder. For FreeRTOS, the bus communication driver are also provided with native FreeRTOS support leveraging services provided by the FreeRTOS. You can find these RTOS drivers from the same location of the peripheral drivers.
RTOS support outside SDK repository
SDK will also support other RTOS but not in the repository of the SDK. Zephyr/Ali-OS/MBED OS are both supported in their community. User can find the support in these public repository.
OSA
SDK don’t provide the unified OSA layers. Middleware needing OSA now get the OSA support inside the middleware.
Application
SDK provide application in boards/<board_name_or_kit_name>/. Board here means the evaluation board created by the NXP avaialbe to customer. Kits here mean a shied board without micro-controller inside. It need work with the evaluation board by connector like Arduino interface. For example, inside the EVKB-IMXRT1050 packages “boards” folder, evkbimxrt1050 is the evaluation board. evkbimxrt1050_agm01 is a shield board which can work with the EVKB-IMXRT1050 board by Arduino connector. AGM01 shield board get multi sensors on the board for user to evaluate NXP sensor product and software.
MCUXpresso SDK board support provides example applications for NXP development and evaluation boards for Arm Cortex-M cores, including Freedom, Tower System, and LPCXpresso boards. Board support packages are found inside of the top level boards folder, and each supported board has its own folder (an MCUXpresso SDK package can support multiple boards). Within each <board_name> folder, there are various sub-folders to classify the type of examples they contain. Except that demo_apps, driver_examples, and cmsis_driver_examples are default for each board, other sub-folders are prepared for each middleware like usb_examples, These include (but are not limited to):
cmsis_driver_examples: Simple applications intended to concisely illustrate how to use CMSIS drivers.
demo_apps: Full-featured applications intended to highlight key functionality and use cases of the target MCU. These applications typically use multiple MCU peripherals and may leverage stacks and middleware.
driver_examples: Simple applications intended to concisely illustrate how to use the MCUXpresso SDK’s peripheral drivers for a single use case. These applications typically only use a single peripheral, but there are cases where multiple are used (for example, SPI conversion using DMA).
emwin_examples: Applications that use the emWin GUI widgets.
rtos_examples: Basic FreeRTOS OS examples showcasing the use of various RTOS objects (semaphores, queues, and so on) and interfacing with the MCUXpresso SDK’s RTOS drivers
usb_examples: Applications that use the USB host/device/OTG stack.
List will be extended with more and more software components integrated into the MCUXpresso SDK
Project Structure
This section describes how the various types of example applications interact with the other components in the MCUXpresso SDK.
Each <board_name> folder in the boards directory contains a comprehensive set of examples that are relevant to that specific piece of hardware. We’ll discuss the hello_world example (part of the demo_apps folder), but the same general rules apply to any type of example in the <board_name> folder.
All files in the application folder are specific to that example, so it is easy to copy and paste an existing example to start developing a custom application based on a project provided in the MCUXpresso SDK.

BOARD specific configuration: board.c/h
board.c/h files are prepared for each board during development. In customer available SDK package, the board.h/c files will be copied to each project. Inside these files, it mainly proivde macros/functions to provide common configuration specific to the board and also that are commonly used by multiple cases. These files are created manually. For example, in the FRDM-K64F board, the UART0 is connected to OPENSDA K20 chips and user can conect to the K20 from PC to get the log input, the board file will debug these UART0 pin connected to OPENSDA K20 as the DEBUG CONSOLE that all cases using debug console needn’t define these macros themselves instead using these macros directly.
Clock configuration : clock_config.c/h
Clock confiugration files are always required to be generated by clock tools in MCUX CFG tools that user can import these files/update files/write back to these files. Clock confiugraiton files provide mutiple clock configuration functions for the application to call. SDK prepare the common clock configuratoin for multiple modes that most of application reuse these files. For some applications with requriement for code size or clock mode, these cases can customize their own clock configuration files accordingly.
PIN configuration: pin_mux.c/h
Pin mux configuration files are always required to be generated by pin tools in MCUX CFG tools that user can import these files/update files/write back to these files. pin mux configuration files are always customized for each applicatiion. pin mux file are create for soc but not for board. If create a pin configuration for a board, a lot of unused functions will be created while it is not needed for specified case.
Project Template
Project template is located in board/<board_name_or_kit_name>/project_template/. Project template are not intented for user’s direct usage. It provide the template for the MCUX CFG tool or CMSIS Pack to create new project as starting point. It provide the basic template of main file, pin mux configuration files, clock configuration files and so on. It existed in board level or soc level. Which file will be used is decided by the request to create proejct for a soc or for a board. There project template need to be updated for each configuration tool update.
boards/<board>/project_tempalate
devices/<soc>/project_template
Documentation
Documents are located in docs folder. Release notes, Getting Start document, API Reference Manual and Change Log document are must have while other document are optional according to content inside SDK package.
Release Notes
Release notes are must have for each MCUXpresso SDK package. It introduce what inside the SDK package and tools set that tested with the package. It also list the known issues for this package and other information information. It is created/maintained/delivered by the documentation team. For detail, please refer to SDK Document.
Getting Start
Getting start document is must have. It describe how to use the SDK package like understanding a typical SDK project, compile, program and debug the application in board. It is created/maintained/delivered by the documentation team.
API Reference Manual and Change Log
APIRM is document describing detail software component API or data structure. The API reference manual are from the doxygen tag in source codes and generated by the SDK Generator. Change Log is documents describing the changes for software components in the package. They are generated from the doxygen information by SDK generator.